커민스, 개인 보호 장비를 위한 핵심 여과 소재 공급 지속

커민스 필터 미디어
현재까지 커민스는 전 세계 마스크 제조업체에 14톤 이상의 여과 매체를 제공해 왔습니다.

In this Q&A, Amy Davis, Vice President of Cummins Filtration, shares an update on the company's progress to provide filter media to mask manufacturers around the globe. 

As the world began to grapple with COVID-19, employees at Cummins were working on innovative solutions to help supply PPE that was in high demand. On April 6, Cummins announced plans to use their filter technology to supply critical materials for N95 respirator masks, an essential piece of personal protective equipment for front-line healthcare workers.

Following the N95 announcement, on April 14, Cummins announced an additional partnership with 3M, which would include the utilization of equipment typically used for producing diesel engine filters to manufacture high-efficiency particulate filters for use in 3M’s powered air purifying respirators (PAPRs).

To date, Cummins has provided more than 14 tons of its filtration media to mask manufacturers across the globe, which has been used to produce more than eight million masks. Amy Davis, Vice President of Cummins Filtration, recently shared an update on the company’s progress to date.

Cummins Filter Media -  Covid - By the Numbers - 1
View the full infographic

Q: First, can you share more about the Cummins Filtration business and your core products?

DAVIS: Our core expertise is designing, manufacturing and selling air, fuel, hydraulic and lube filtration, as well as chemical technology products for diesel and gas-powered equipment around the world. 

Q: How did Cummins Filtration get involved in supplying media for masks?

DAVIS: The need for masks, especially N95 respirator masks, skyrocketed in March and April in response to the COVID-19 pandemic. We learned that many of the world’s leading mask manufacturers needed the critical materials to assemble masks and were struggling to meet demand. We realized that the NanoNet® and NanoForce® Media technology typically found in filtration products for diesel engines could also be used in surgical masks and N95 respirator masks worn by healthcare professionals to help stop the spread of COVID-19. Once we made that connection, we began exploring partnerships to apply the filter material to masks. 

 

Cummins Filter Media - Covid - By the Numbers - 2

Q: How has Cummins been able to partner with 3M in an additional effort to meet the surge in demand for PPE due to the COVID-19 outbreak?

DAVIS: We needed to move fast and saw an opportunity to use our existing workforce at our Neillsville, Wisconsin facility to meet this demand. We acquired, commissioned and tested a new pleater in a matter of weeks and have already produced more than 41,000 filters for 3M’s PAPRs since mid-April. Internally, we talk a lot about employee empowerment and decision making and this project is a testament to our employees’ ability to adapt quickly to fill an important supply void in a totally different market. 

Q: What has the response been like from mask manufacturers?

DAVIS: Demand has been strong – in fact, it’s getting to the point where demand will exceed our capacity. Seeing so many organizations inquire about the media reinforced how critical the need for masks was globally. We’ve talked with Universities, health care systems, other automotive companies and mask manufacturers large and small about our media. To date, we’ve supplied 6 tons of the complete composite multilayer media that can be used in N95 masks, and we’ve shipped 8 tons of a simpler polypropylene media that can be used in surgical masks. 

 

Cummins Filter Media - Covid - By the numbers - 3

Q: Do you plan on selling media for masks long-term, or is this a temporary measure to respond to the COVID-19 pandemic?

DAVIS: We’ve added manufacturing capacity and capability to our plants and plan on continuing to supply media for masks as long as there is demand and a need to protect our communities from COVID-19.  

Q: What has been the most interesting thing about this project for you?

DAVIS: Our employees always want to help, and it wasn’t a surprise when they demonstrated how quickly we could pivot from supplying filters for diesel engines to supplying the media that is critical to manufacturing medical PPE. It only took us one month to go from concept to production on this project! Cummins Filtration employees across the globe have taken immense pride in being part of the solution to help our communities, and the entire initiative is a great example of how Cummins embodies our mission of making people’s lives better by powering a more prosperous world.

커민스 사무실 건물

커민스(Cummins Inc.)

글로벌 전력 기술 리더인 커민스는 광범위한 전력 솔루션 포트폴리오를 설계, 제조, 배포 및 서비스하는 보완 비즈니스 부문의 기업입니다. 이 회사의 제품은 내연, 전기 및 하이브리드 통합 전력 솔루션 및 여과, 후처리, 터보차저, 연료 시스템, 제어 시스템, 공기 처리 시스템, 자동 변속기, 전기 발전 시스템, 마이크로그리드 제어 장치, 배터리, 전해조 및 연료 전지 제품을 포함한 구성품에 이르기까지 다양합니다.

커민스 발전기 판매로 이익을 얻을 수 있는 5가지 비즈니스

가정용 발전기에 대해 상의하는 커민스 딜러

미국 비즈니스의 90%는 중소기업입니다. 수백만 명의 근로자를 고용하는 우리 경제의 진정한 엔진입니다. 많은 업체들이 서비스를 확장하고, 수입을 창출하고, 비즈니스를 성장시킬 새로운 방법을 찾고 있는 가운데, 커민스의 가정용 대기 전력 및 휴대용 발전기는 새로운 수익원이 될 수 있습니다.

어둠의 구름 속의 실버 라이닝

AP 통신에 따르면 지난 2년 동안 악천후로 인한 정전이 두 배로 증가하여 우리나라의 노후화된 전력망에 부담을 줍니다. 이로 인해 정전 빈도와 지속 시간이 증가했습니다. 이러한 빈번한 정전으로 가정 및 기타 기업에 안정적인 백업 전력이 필요합니다. 그리고 진취적인 중소기업에게는 커민스 발전기로 이러한 요구를 충족시키는 것은 엄청난 기회입니다.

커민스 공인 딜러가 됨으로써 가장 많은 혜택을 누릴 수 있는 기업은 무엇일까요? 상위 5개 사항은 다음과 같습니다.

1. 일반 계약업체 - 얼음 폭풍, 허리케인, 강한 바람, 산림 화재 또는 지진과 같은 자연 재해가 발생했을 때 고객이 직면한 유일한 도전은 전력 손실이 아닙니다. 종종 수리해야 하는 재산에 물리적 손상이 있습니다. 고객이 재건을 도울 때 일반 계약업체는 가정 또는 비즈니스의 에너지 요구를 추정하고 Cummins QuietConnect™ 가정용 대기 전력 발전기를 추가할 것을 제안할 기회가 있습니다. 고객이 동의하는 경우, 일반 계약자는 발전기 판매로 이익을 얻는 것뿐만 아니라 발전기 설치를 위한 인건비도 발생합니다.

2. 전기 기사 - 훌륭한 전기 기술자가 신뢰할 수 있는 정보원입니다. 전자 흐름에 대한 전문가는 물론 고객의 특정 전기 설정도 종종 알고 있습니다. 장기간 정전이 있은 후, 많은 사람들이 종종 "다음에 전력이 꺼질 때 전기를 유지하기 위해 할 수 있는 일이 있습니까?" 하고 묻습니다. Cummins QuietConnect 가정용 대기 전력 발전기를 판매 및 설치하는 전기 기사들은 "예, 그렇습니다"라고 말할 수 있습니다. 가정용 대기 전력 발전기 설치는 전기 기사가 제공하는 또 다른 귀중한 서비스가 될 수 있습니다.

3. 난방 및 냉각 계약자 - 정전이 발생했을 때 가정과 사업주가 오프라인으로 전환한 가장 중요한 시스템 중 하나는 중앙 난방 및 냉각 시스템입니다. 오랜 기간 동안 열이나 시원한 공기가 없는 것은 불편할 뿐만 아니라 온도가 극한의 외부에 있다면 위험할 수 있습니다. 따라서 당연히, 일단 전력이 복구되면, 다음 정전 중에 HVAC 시스템을 계속 가동할 방법을 찾는 것이 가장 중요해집니다. 난방 및 냉각 계약자는 가정과 기업에 대규모 시스템을 설치하는 전문가이기 때문에 커민스 QuietConnect 대기 발전기를 가정과 기업에 추가하면 비즈니스에 또 다른 수익 센터를 추가할 수 있는 자연스러운 방법입니다.

4. 온라인 소매업체 - 지금까지 대기 전력 발전기에 대해 논의해 왔습니다. 발전기를 영구 설치하는 것을 전문으로하지 않는 기업의 경우 커민스 휴대용 발전기는 돈을 벌 수 있습니다. 휴대용 발전기는 정전 중에 사용할 수 있지만 휴대성 때문에 더 작은 작업에 더 적합합니다. 따라서 캠핑, 테일게이팅, 건설 작업 현장 등에 이상적입니다. 커민스의 견고하고 믿을 수 있는 평판을 바탕으로 당사의 휴대용 발전기는 이러한 시장 분야에 초점을 맞춘 소매업체에 이상적입니다.

5. 태양광 패널 설치자 - 대부분의 가정용 태양광 패널은 전력망에 직접 연결됩니다. 따라서 전력이 꺼지면 태양 전지판이 전력 공급을 중단합니다. 예비 전력원의 경우, 태양광 패널 설치자는 태양열 배터리 백업을 설치할 수 있습니다. 이 백업 장치는 태양 전지 패널에 의해 충전되거나 가정용 대기 전력 발전기로 충전됩니다. 일반적으로 태양열 배터리 백업은 몇 시간 동안만 가정에 전력을 공급할 수 있으므로 기후 관련 정전이 발생하기 쉬운 경우 Cummins QuietConnect와 같은 가정용 대기 전력 발전기가 더 좋은 선택입니다.

지금이 바로 그 때입니다

그 어느 때보다 많은 사람들이 백업 발전기를 찾고 있는 지금이 커민스 공인 딜러가 되어 회사의 제품을 확장할 수 있는 좋은 시기입니다. 자세한 내용을 보려면 cummins.com/partners/dealers.

커민스 사무실 건물

커민스(Cummins Inc.)

글로벌 전력 기술 리더인 커민스는 광범위한 전력 솔루션 포트폴리오를 설계, 제조, 배포 및 서비스하는 보완 비즈니스 부문의 기업입니다. 이 회사의 제품은 내연, 전기 및 하이브리드 통합 전력 솔루션 및 여과, 후처리, 터보차저, 연료 시스템, 제어 시스템, 공기 처리 시스템, 자동 변속기, 전기 발전 시스템, 마이크로그리드 제어 장치, 배터리, 전해조 및 연료 전지 제품을 포함한 구성품에 이르기까지 다양합니다.

정전을 대비하는 10가지 방법

집의 측면에 장착된 박스를 분리하는 커민스 서비스

전기에 대한 과도한 수요를 야기하는 열파... 수력 발전을 줄이는 가뭄... 활성 산불 근처의 전력망이 안전을 위해 폐쇄되었습니다... 노후화되고 과다한 전력망... 파워라인을 찍는 강한 바람... 이러한 이유로 일부 지역에서는 올해 예정된 정전이 발생할 수 있습니다.

정전이 발생하기 쉬운 지역에 거주하는 경우 가족을 위해 준비하는 데 도움이 되는 몇 가지 팁이 있습니다.

  • 현지 전기 유틸리티에서 알림을 받으려면 등록하세요. 이 서비스가 현지 유틸리티에서 제공되는 경우, 전력이 꺼지기 전에 준비를 시작하도록 경고를 표시할 수 있습니다.
  • 정전 최종 체크리스트를 다운로드하세요. 정전 전후에 무엇을 해야 할지에 대한 심층적인 정보를 제공합니다. 그것은 심지어 의료 필요를 가진 어린이, 애완 동물 및 가족을 위해 무엇을 해야할지 보여줍니다. 여기에서 다운로드할 수 있습니다.
  • 비축할 수 없는 식량과 물 - 매뉴얼도 있어야 합니다. 정전 기간 동안 가족이 수분과 영양을 유지할 수 있도록 모든 사람을 위해 충분한 영양을 공급할 계획입니다.
  • 아이스와 쿨러를 만들거나 구매하세요 - 경고가 충분하면 아이스를 만들거나 구매하여 부패하기 좋은 음식을 냉각기에 담아 보존할 수 있습니다. (냉장고는 내부 온도만 약 4시간, 냉동고는 약 48시간 동안만 유지됩니다.)
  • 손전등 및 추가 배터리 구매 - 정전은 검은색일 수 있습니다. 야간 이동이 필요하지만 아껴서 사용해야 한다면 손전등을 안전을 위해 사용할 수 있습니다. 모든 가족 구성원이 충분해야 합니다.
  • 휴대 전화를 충전하고 가스 탱크를 가득 채움 - 휴대 전화와 차량은 바깥 세상의 생명선입니다. EV가 있는 경우 완전히 충전되었는지 확인하세요.
  • 수동으로 차고 문을 여는 연습 - 어딘가로 운전해야 하는 경우 먼저 차량을 차고에서 꺼낼 수 있어야 합니다.
  • 냉장 보관이 필요한 약물에 대한 계획 - 동력이 돌아올 때까지 냉장 식품과 같은 쿨러에 보관해야 할 수도 있습니다.
  • 가정용 대기 전력 발전기에 투자 - 안심할 수 있도록 Cummins QuietConnect™ 가정용 대기 전력 발전기 중 하나를 고려해 보세요. 정전이 발생하면 발전기가 자동으로 켜지고 집에 동력을 공급합니다.
  • 배터리 백업으로 일산화탄소 감지기를 설치합니다. 일산화탄소가 집에 들어오면 즉시 경고를 받을 수 있도록 모든 층의 중앙 위치에 배치합니다.

롤링 정전이 점점 더 보편화되고 있는 것 같습니다. 다행스럽게도, 미리 계획을 세우고 생명을 완전히 방해하지 않도록 하는 방법이 있습니다. 이러한 계획된 정전 기간 동안 커민스가 가족을 도울 수 있는 다양한 방법을 알아보려면 cummins.com/na/generators/home-standby/whole-house-and-portable 방문하거나 cummins.com/na/generators/home-standby/find-a-dealer 현지 딜러를 찾으세요.

커민스 사무실 건물

커민스(Cummins Inc.)

글로벌 전력 기술 리더인 커민스는 광범위한 전력 솔루션 포트폴리오를 설계, 제조, 배포 및 서비스하는 보완 비즈니스 부문의 기업입니다. 이 회사의 제품은 내연, 전기 및 하이브리드 통합 전력 솔루션 및 여과, 후처리, 터보차저, 연료 시스템, 제어 시스템, 공기 처리 시스템, 자동 변속기, 전기 발전 시스템, 마이크로그리드 제어 장치, 배터리, 전해조 및 연료 전지 제품을 포함한 구성품에 이르기까지 다양합니다.

커민스 터보 테크놀로지스가 8세대 Holset 시리즈 400 가변 용량(VGT) 터보차저 출시 준비

8세대 HE400VGT

배출가스 규정이 더욱 엄격해짐에 따라 커민스 터보 테크놀로지스(CTT)는 혁신적인 새로운 공기 처리 기술을 통해 고객이 배출가스를 줄이고 연비 경제성을 발전시키도록 돕기 위해 최선을 다하고 있습니다.

70년 동안 혁신과 신뢰성을 바탕으로 구축된 CTT와 Holset은 다양한 업계 최고의 공기 처리 기술을 도입했습니다. 2021년 CTT는 7세대 400 시리즈 가변 용량 터보차저(VGT)를 출시하여 엔진 제조사들이 미래의 배출가스 표준을 충족하고 동급 최고의 연비 경제성을 제공할 수 있도록 지원합니다. 커민스는 현재의 기술을 지속적으로 발전시키고 새로운 기술을 개발하면서 혁신이 멈추지 않습니다. 이러한 철학을 염두에 두고 CTT는 이제 8세대 HE400VGT를 소개할 준비를 하고 있습니다. 10-15L 중장비 트럭 시장에서 동급 최고의 성능, 신뢰성, 내구성을 갖도록 특별히 제작된 엔진입니다.

CTT는 최신 세대 제품을 통해 터보차저 성능을 크게 개선했습니다. 8세대 터보차저는 이전의 7세대 터보차저보다 5% 향상된 효율을 제공합니다.

HE400VGT는 엔진 다운사이징 고객을 돕는 향상된 터보차저 효율을 제공하는 것 외에도 더 나은 과도 응답, 향상된 압축기 측 오일 누출 견고성, 공급망 유연성을 위한 주요 컴포넌트에 대한 이중 소싱을 제공합니다.

Holset HE400VGT의 주요 하이라이트는 성능과 과도 응답을 강화하기 위한 새로운 베어링 시스템과 제로에 가까운 여유 공간을 포함합니다. 이러한 개선 사항은 컴프레서 스테이지의 더 엄격한 여유 공간, 터빈 스테이지의 낮은 방사형 움직임, 개선된 표면 마감 및 새로운 에어로 설계를 통해 달성됩니다.

2024년에 출시될 예정인 이 터보차저는 차세대 스마트 전기 액추에이터 및 속도 센서와 최신 칩셋을 통합하여 성능과 내구성을 향상시킵니다. 이중 소싱 전략은 최근에 업계를 악화시켰던 예기치 않은 전자 장치 부족 문제를 줄이는 데 도움이 됩니다.

성능 향상과 함께 최신 세대 터보차저는 상용 중장비 트럭에 동급 최고의 성능을 제공하고 주요 차량 주행 지점에서 연비 경제성을 향상시킵니다.

"CTT는 엔진 고객이 엄격한 배출가스 요건을 충족하고 총 소유 비용을 줄일 수 있도록 최신 HE400VGT에 흥미로운 신기술을 통합했습니다. 고객이 향후 배출가스 규제를 위한 전략을 수립함에 따라 CTT는 성능 저하 없이 고객의 엔진 개발 요구 사항을 충족하는 혁신적인 제품을 제공하기 위해 이전 터보차저 출시의 성공을 계속 구축하고 있습니다.

CTT의 제품 및 기술 혁신에 대해 더 알고 싶으신가요? 오늘 분기별 뉴스레터에 가입하세요.

커민스 사무실 건물

커민스(Cummins Inc.)

글로벌 전력 기술 리더인 커민스는 광범위한 전력 솔루션 포트폴리오를 설계, 제조, 배포 및 서비스하는 보완 비즈니스 부문의 기업입니다. 이 회사의 제품은 내연, 전기 및 하이브리드 통합 전력 솔루션 및 여과, 후처리, 터보차저, 연료 시스템, 제어 시스템, 공기 처리 시스템, 자동 변속기, 전기 발전 시스템, 마이크로그리드 제어 장치, 배터리, 전해조 및 연료 전지 제품을 포함한 구성품에 이르기까지 다양합니다.

재건 성공은 광산 작업자에게 가치가 있습니다

"Cummins 300th QSK60 MCRS Upgrade"라는 텍스트가 있는 벨트 버클

호주와 미국의 커민스 엔지니어들이 마스터 스트로크를 통해 특별 업그레이드 프로그램에 따라 QSK60 엔진을 재건하기로 선택하는 광산 회사들에게 큰 비용 절감과 환경 혜택이 제공되었습니다.

엔지니어들은 초기 세대 QSK60의 재건 가능성과 정밀 검사 시 최신 디젤 기술로 업그레이드할 수 있는 방법에 초점을 두었고, 기본 60리터 V16 설계에는 큰 변화가 없었습니다. 이는 다른 엔진 제조사들을 가로막은 업적이었습니다.

주요 기술 업그레이드는 연료 분사이며, 초기 장치 분사 시스템(HPI)은 현재 커민스의 모든 최신 세대 고마력 엔진에 탑재된 고압 모듈식 커먼레일 시스템(MCRS)으로 대체됩니다.

2700 hp 등급의 300번째 업그레이드 엔진은 최근 브리즈번의 커민스 마스터 재건 센터에서 생산 라인을 끊어 QSK60의 진화를 위한 또 다른 성공적인 단계와 모바일 광산 장비에서 전 세계적으로 가장 높은 마력의 디젤 엔진인 이유를 강조했습니다.

커민스 아시아 태평양 지역 광산 비즈니스 개발 매니저 인 그렉필드(Greg Field)는 "연료 소비 감소와 정밀 검사 시점까지의 수명 연장은 총 소유 비용을 낮추는 열쇠이며, QSK60 업그레이드 프로그램의 엔지니어링을 뒷받침하는 초기 목표였습니다" 라고 말합니다.

"혁신은 커민스의 오랜 역사의 핵심이며, 광산용 고객에게 제공할 수 있는 QSK60 재건 옵션에서 확실히 그 역할을 했습니다."

결론은 인상적입니다: 디젤 분진 배출량은 후처리 없이 실린더 내 연소 기술을 통해 최대 63% 감소합니다. 또한 오일의 그을음 부하가 적어 유지보수를 위한 플러스가 있습니다.

Fuel savings up to 5% are consistently reported in the field for significant greenhouse gas emissions reduction, while life-to-overhaul is extended by 10%, translating to fuel consumption of more than 4.0 million liters before rebuild is required.

1단계 터보차지 기능이 있는 QSK60은 MCRS로의 연료 시스템 업그레이드 외에도 세계에서 가장 엄격한 산업용 배출가스 표준인 티어 4 파이널 및 스테이지 V 배출 규정 준수를 위해 설계된 연소 기술의 다른 혁신 기능도 갖추고 있습니다.

리빌드 업그레이드 패키지는 1785-2700 hp 등급의 1단계 터보차지('Advantage'라고 함)와 2700, 2850 또는 3000 hp로 평가될 수 있는 2단계 터보차저가 있는 QSK60의 두 가지 변형에 적용할 수 있습니다.

300번째 업그레이드된 QSK60은 코마츠 930E 운송 트럭에 설치하기 위해 NSW 거네다 분지의 보가브리 석탄을 방문했습니다. 이 엔진은 호주의 석탄 및 철광석 광산에서 그 가치를 입증했습니다.

노랑 QSK60 엔진

태그
커민스 사무실 건물

커민스(Cummins Inc.)

글로벌 전력 기술 리더인 커민스는 광범위한 전력 솔루션 포트폴리오를 설계, 제조, 배포 및 서비스하는 보완 비즈니스 부문의 기업입니다. 이 회사의 제품은 내연, 전기 및 하이브리드 통합 전력 솔루션 및 여과, 후처리, 터보차저, 연료 시스템, 제어 시스템, 공기 처리 시스템, 자동 변속기, 전기 발전 시스템, 마이크로그리드 제어 장치, 배터리, 전해조 및 연료 전지 제품을 포함한 구성품에 이르기까지 다양합니다.

cummins.com
으로 이동

찾으시는 정보가
cummins.com에 있습니다.

지금 해당 사이트를 열고 있습니다.

감사합니다.