Near zero emission natural gas engine expands reach outside U.S.

The L9N Near Zero emission engine is being tested in Santiago, Chile's capital city.
The L9N Near Zero emission engine is being tested in Santiago, Chile's capital city.

Cummins, the global power leader offering customers a broad portfolio of solutions, is propelling a bus in Chile with the company’s L9N Near Zero emission natural gas engine, the first application for the engine outside the United States.

The L9N, considered one of the world's cleanest internal combustion engines, can significantly reduce particulate matter (PM), nitrogen oxides (NOx) and greenhouse gases (GHGs). The 320-horsepower engine is powering a bus through Santiago, Chile's capital city, on a test basis.

“We are proud to present our Cummins L9N gas engine in Chile, which will significantly contribute to reducing greenhouse gases and decontaminating the

The L9N powered bus in Santiago, Chile
The L9N Near Zero emission natural gas bus is ready to demonstrate its environmental benefits on the streets of Santiago, Chile.

city of Santiago," said Fábio Magrin, General Manager of Cummins Chile. "We endeavor to bring our customers the right power solutions for the work they need to do. The solution found in Chile is in line with our mission to make people's lives better by powering a more prosperous world."

GRABBING ATTENTION

The announcement of the Cummins gas-powered bus was attended by the Chilean Minister of Transport and Telecommunications, Gloria Hutt, and generated interest from the Chilean news media. Much of the coverage highlighted the engine's potential to help improve the environment in the country.

"Natural or renewable gas-powered engines can be incredibly clean and efficient," said Luís Pasquotto, Vice President of Cummins Brazil and the leader of the company's engine business in Latin America. "With increasing gas abundance and a mature technology requiring relatively simple infrastructure investment, these engines are a great solution for many customers and markets, including in Latin America."

A RECORD OF SUCCESS

Cummins delivers natural gas solutions that are reliable, durable and efficient. The 80,000 Cummins natural gas engines currently in use offer dependable, clean and quiet performance, as well as low emissions, high efficiency, low total fuel costs, and reduced dependence on imported oil.

With 100 years of experience and technology leadership, Cummins innovates for a future with energy diversity and will continue to deliver the right technology at the right time for every customer.

The inside of the bus testing the L9N in Chile
The inside of the test bus is ready for customers.


 

Immeuble de bureaux Cummins

Cummins Inc.

Cummins est un chef de file mondial en alimentation qui conçoit, fabrique, vend et entretient des moteurs au diesel et aux carburants de remplacement de 2,8 à 95 litres, des ensembles de génératrices électriques diesel et de remplacement de 2,5 à 3, 500 kW, ainsi que des composants et de la technologie connexes. Cummins dessert ses clients par l’entremise de son réseau de 600 installations de distributeurs indépendantes et détenues par l’entreprise, et de plus de 7 200 concessionnaires répartis dans plus de 190 pays et territoires.

Harbor Harvest : la durabilité et les petites entreprises sur le son

Port de la récolte

Un centre commercial, une entreprise de transport, un constructeur de bateau et un fabricant de moteurs marchent dans un bar... Oh, attendez. Cela devait dire qu’ils ont commencé à expédier des produits d’origine locale partout dans le long Island Sound à l’aide d’un bateau hybride durable unique pour offrir un accès respectueux de l’environnement aux marchandises pendant la pandémie de COVID-19.

Meet Harbor Harvest : la solution novatrice du Connecticut amenant la ferme au port, puis à votre table.

Bob Kunkel vit à Norwalk, dans le Connecticut, depuis 27 ans. Un homme avec un arrière-plan unique qui aimait passer du temps sur l’eau, mais aussi dans la cuisine. Ce duo de passions l’a amené à épouser un marché alimentaire consacré à la vente d’aliments de qualité et à un programme sur la route Marine sur la côte nord-est.

Harbor Harvest hybridePremièrement, qu’est-ce que ce bateau hybride ? Kunkel est président de alternative marine technologies, qui se spécialise dans des projets en dehors de l’histoire de la propulsion normale ou de la conception de navires. En se connectant à BAE Systems (une entreprise de technologie de pointe), les deux organisations ont pensé à convertir le système de bus de véhicules électriques de BAE en un projet maritime. Après avoir travaillé avec un premier fabricant de moteur, m. Kunkel et BAE ont découvert que le système marin entièrement intégré de Cummins Inc. était le dernier élément de leur idée de millions de dollars. Le catamaran diesel-électrique est né à l’aide de deux moteurs QSB 6.7 hybrides prêts à l’emploi et d’un ensemble d’affichage pour surveiller les moteurs, les composants hybrides et le système de stockage d’énergie.

L’hybride transporte environ 28 palettes de produits d’origine locale, dont 10 sont positionnés dans un espace de promenade entièrement réfrigéré et protégé. Le navire fait office de voie de transport pour les fermes familiales et les systèmes agricoles qui amènent leurs produits durables dans la grande ville. Kunkel mentionne que le marché d’une ferme locale n’atteint généralement qu’un rayon de 10 milles. Avec Harbor Harvest, la marine Highway leur permet de prolonger leur portée sans augmenter leurs coûts.

D’un point de vue de la durabilité, les avantages sont clairs. Un voyage que le port de la récolte peut terminer de Norwalk, Connecticut à Huntington, New York en environ une heure emmène leurs homologues du camionnage n’importe où de 6-12 heures pour accomplir. Mais les émissions sur route ne sont pas la seule chose qui sauve la récolte portuaire ; ils améliorent également l’efficacité des agriculteurs locaux. Les fermes familiales n’ont pas à se débarrasser de leur lait ni à jeter leurs produits parce qu’ils ne peuvent pas le faire sur le marché. Harbor Harvest offre à sa nourriture un itinéraire fiable et profitable pour les tables des gens.

Au cours de la pandémie de COVID-19, l’organisation à base de Norwalk a prospéré. Bien que le bateau n’ait couru qu’un ou deux jours par semaine en raison d’une baisse de la demande des restaurants et des détaillants, ils n’ont certainement pas à manquer d’éléments essentiels.

Harbor Harvest 1st location

« Les grandes usines de transformation de la viande ont des problèmes avec les fermetures », a déclaré m. Kunkel. « Nous sommes directement aux fermes et aux abattoirs sur mesure, alors nous n’avons eu aucun problème à fournir de la viande, du poisson et d’autres produits. » Il a ensuite fait en sorte que les vendeurs locaux puissent mieux répondre aux urgences locales, affirmant que cela accentue « ce que «Buy local » et « soutien local » signifie vraiment.»

Harbor Harvest est un parfait orage de la durabilité, de la petite entreprise et de l’innovation. L’amélioration de la relation entre l’agriculteur, le port et le client n’est pas un petit travail, mais Kunkel et ses partenaires corporatifs semblent avoir concocté un fonctionnement impeccable. Harbor Harvest se penche vers l’avenir, espérant qu’il continuera d’élargir ses activités avec d’autres navires hybrides.

Avec un ton décontracté, mais le plus sérieux des intentions, Kunkel conclut, « je pense que nous sommes assez près de changer le monde ».

étiquettes
Katie Yoder-Cummins Inc.

Katie Yoder

Katie Yoder est une spécialiste en communications marketing. Nouveau chez Cummins en 2018, Katie s’est jointe à l’équipe des opérations de commercialisation où elle appuie les initiatives en matière de foires commerciales en Amérique du Nord. En tant qu’ancienne diplômée de l’Université d’Wisconsin, Katie aime observer les sports de blaireau pendant son temps libre.

Que tiendra l’avenir pour les chantiers de construction du monde ?

Chantier du futur

Nous présentons notre série d’articles sur le « worksite of the future », où nous examinons les tendances qui façonneront l’avenir de l’industrie de la construction.

Pour le chantier de construction du futur, les gestionnaires d’équipement et de site pourraient surveiller leurs bulldozers et leurs excavatrices avant de partir. À l’aide d’un tableau de bord sur leur ordinateur portable ou leur téléphone, ils pourraient vérifier quels entretiens ont été effectués pendant la nuit et quels entretiens seront nécessaires pour maximiser la disponibilité au cours des prochains jours. Certains prédisent un moment où les gestionnaires de l’équipement et du site n’auront jamais à quitter leur domicile, ce qui leur permettra d’accomplir leur travail à distance. Leur équipement autonome pourrait également être contrôlé à distance.

Il se peut qu’il y ait un moment avant que tout cela arrive. Mais à mesure que l’industrie de la construction évolue, Cummins Inc. travaillera en partenariat avec les clients de la construction afin de développer des innovations qui leur conviennent. En fait, certaines de ces avancées se trouvent au coin de la rue.

Nous souhaitons partager notre vision du futur chantier, comment nous voyons l’évolution affectant nos clients et ce que nous faisons pour évoluer avec lui. Nous vous apporterons ces renseignements à travers une série d’articles courts au cours des prochaines semaines.

Un point de départ naturel est la compréhension de la force motrice d’un changement de technologie et de la façon dont ces progrès peuvent relever les défis auxquels est confrontée cette industrie cruciale. En décrivant quelques-uns des éléments clés de la modification entourant les groupes motopropulseurs d’équipement, nous explorerons comment nous adaptons la technologie actuelle afin de répondre aux besoins de l’industrie de la construction d’aujourd’hui.

Nous croyons que l’alimentation au diesel de pointe a un long avenir dans l’espace de construction, mais il existe des solutions d’alimentation de rechange qui ont du sens pour certaines applications. Au-delà des progrès technologiques avec le groupe motopropulseur d’équipement, nous pouvons apporter des améliorations de la productivité avec les produits numériques, par l’entremise de l’Internet des objets (IoT) et de l’apprentissage automatique.

Au fur et à mesure que la série progresse, nous explorerons les technologies de la solution d’alimentation du futur et présenterons même certains cas de test actuels. Nous examinerons les tâches précises que chaque application effectue sur le site et comment ce cycle d’utilisation s’aligne sur les forces de certaines technologies futures. Grâce à de nouveaux progrès, le taux d’adoption dépendra de plusieurs facteurs, alors nous discuterons de ces éléments et de la façon dont ils pourraient ajuster la façon dont les projets de construction sont planifiés.

Aujourd’hui, les gestionnaires d’équipement projettent des choses comme la consommation de carburant, les remplacements de filtre et les changements de lubrification. À l’avenir, ces mêmes gestionnaires d’équipement examinaient peut-être la consommation d’électricité, les calendriers de facturation et comment cela pourrait avoir un impact sur le soutien infrastructurel. Par exemple, les modules de recharge portatifs seront-ils obligatoires ou devrait-on installer des pylônes de charge attachés directement au réseau électrique ou à une série de génératrices ?

Comme les solutions d’alimentation utilisées pour déplacer l’équipement de construction évoluent, le soutien sera donc indispensable. Nos outils de service et nos modèles de soutien évolueront avec les technologies émergentes. Les technologies numériques qui surveillent et automatisent les actions de service sur plusieurs chantiers et cycles de vie des produits contribueront à maintenir le fonctionnement efficace des chantiers de construction. Les mêmes technologies de moteur de base qui se présentent sur le site seront également utilisées dans les véhicules de service afin de produire des pièces de rechange et de stockage d’énergie, peut-être en exploitant des algorithmes prédictifs.

Nous sommes ravis de partager cette histoire évolutive, nous espérons que vous vous étiquetez et vous y apprécierez.

Apprenez-en plus et participez à la conversation

Rejoignez la conversation avec #Cummins sur vos plateformes sociales ou visitez https://www.cummins.com/engines/construction pour en savoir plus sur nos solutions de produits actuelles et futures. Nous avons aussi des experts de Cummins partout dans le monde qui sont heureux de répondre à vos questions. Trouvez votre professionnel Cummins le plus près en visitant care.cummins.com ou en téléphonant à 1-800-Cummins.

Immeuble de bureaux Cummins

Cummins Inc.

Cummins est un chef de file mondial en alimentation qui conçoit, fabrique, vend et entretient des moteurs au diesel et aux carburants de remplacement de 2,8 à 95 litres, des ensembles de génératrices électriques diesel et de remplacement de 2,5 à 3, 500 kW, ainsi que des composants et de la technologie connexes. Cummins dessert ses clients par l’entremise de son réseau de 600 installations de distributeurs indépendantes et détenues par l’entreprise, et de plus de 7 200 concessionnaires répartis dans plus de 190 pays et territoires.

Cinq trucs sur la sécurité nautique à retenir avant de prendre l’eau cette saison

Conseils en matière de sécurité nautique

À partir du dépôt d’un plan de bateau pour la planification d’un contrôle de sûreté du bateau, voici cinq astuces pour vous aider à faire en sorte que votre temps sur l’eau soit mémorable pour toutes les bonnes raisons.

L’été se trouve juste au coin de la rue. Beaucoup d’entre nous aspirent aux longues journées, aux temps plus chauds et aux moments passés sur l’eau. Que vous soyez à la tête de votre ponton sur le lac, du bateau de pêche dans le Golfe ou du voilier sur l’océan, une navigation de plaisance sécuritaire commence sur le rivage.

« Chez Cummins, nos vies quotidiennes tournent autour de la sécurité », dit Jennifer McQuilken, qui travaille pour Cummins marine, mais qui est également capitaine de la garde côtière des États-Unis. «De porter un équipement de protection approprié afin de prendre les précautions appropriées lors de l’installation de notre produit dans des applications, garantissant la sécurité des membres de notre équipe et de nos clients est la priorité absolue. C’est pourquoi nous tous chez Cummins marine vous rappellerons quelques choses faciles à faire avant de partir sur l’eau pour la première fois cette saison.»

Sans plus tarder, voici cinq conseils en matière de sécurité nautique à retenir lorsque vous vous préparez à votre voyage.

Portez un gilet de sauvetage

Conseils de sécurité pour bateau et eau – gilets de sauvetage
Selon la U.S. Coast Guard, le port d’un gilet de sauvetage est recommandé pour chaque plaisancier.

Peu importe l’activité que vous avez planifiée sur l’eau, vous devriez toujours avoir un gilet de sauvetage. Il est également important de faire en sorte que votre gilet de sauvetage soit approuvé par la U.S. Coast Guard ou un autre organisme autorisé, soit approprié pour votre activité d’eau et s’adapte correctement. Il existe des styles de gilet de sauvetage disponibles pour presque toutes les aventures – croisière, chasse, pêche, pagayage, sports nautiques, etc.

La sécurité d’abord

Assurez-vous que vous avez l’équipement de sécurité approprié sur votre bateau. Il y a plusieurs articles qui doivent être vérifiés sur n’importe quel bateau, dont certains expirent. L’enregistrement valide, les feux de fonctionnement, les fusées éclairantes et les extincteurs d’incendie approuvés font partie des choses nécessaires pour un voyage en toute sécurité sur l’eau. N’oubliez pas la crème solaire, l’eau et les vêtements appropriés pour les éléments. Vous ne savez pas si vous avez ce qu’il vous faut ? Planifiez un contrôle de sécurité du bateau sans frais avec vos escadrons de la garde côtière des États-Unis ou des États-Unis d’Amérique avant de toucher l’eau.

Déposer un plan de flottaison

Informez une personne que vous avez confiance en votre plan de flottement, qui comprend des détails sur le voyage, le bateau, les personnes, le véhicule tracteur, l’équipement de communication et les contacts d’urgence. Si vous n’êtes pas de retour ou de check-in tel que prévu, un plan de flottaison permettra à quelqu’un d’avoir les renseignements dont il a besoin pour vous aider. En savoir plus sur http://floatplancentral.cgaux.org/.

Suivez les règles de navigation

Adhérer à ces règles, c’est comme suivre les lois sur la circulation. En tant qu’opérateur, vous êtes responsable de la sécurité de votre bateau et de vos passagers. Il est essentiel de savoir quoi faire dans des situations comme la réunion en tête, le dépassement d’un autre bateau et la compréhension des aides à la navigation (signes, bouées, etc.) pour un fonctionnement sécuritaire de votre bateau. Soyez conscient de votre entourage et voyagez toujours à une vitesse appropriée pour l’environnement.

Connaissez vos lois locales en matière de navigation

Les règles et les lois peuvent différer selon l’état , la région ou le pays. Les infractions peuvent entraîner des contraventions, des amendes ou une peine de prison. L’âge de l’utilisateur minimal, les restrictions de remorquage, les permis de navigation et les assurances varient. Assurez-vous de vous enregistrer avec vos directives locales avant de heurter l’eau.

« Être sur l’eau est un moyen amusant de communiquer avec vos amis et votre famille », dit le capitaine McQuilken.

« Des activités actives comme la pêche et les tuyaux, pour se détendre sur un voilier ou faire une croisière autour, nous voulons que vous ayez du plaisir, une journée sûre sur l’océan ou le lac. »

Peu importe que vous soyez un plaisancier expérimenté, ou simplement que vos pieds soient humides, il y a des ressources pour vous aider, votre famille ou vos amis en apprendre plus sur la sécurité sur l’eau. Considérez en train de suivre un cours de navigation en toute sécurité , en personne ou en ligne.

« On se voit là-bas ! »

Katie Yoder-Cummins Inc.

Katie Yoder

Katie Yoder est une spécialiste en communications marketing. Nouveau chez Cummins en 2018, Katie s’est jointe à l’équipe des opérations de commercialisation où elle appuie les initiatives en matière de foires commerciales en Amérique du Nord. En tant qu’ancienne diplômée de l’Université d’Wisconsin, Katie aime observer les sports de blaireau pendant son temps libre.

En compétition pour le titre : le plus grand et le plus baddest de Bristol Bay

Le F/V Emory James est un système de Gillnetter à double jet Bristol Bay à moteur Cummins

Vous profitez d’un côté de chaos avec votre pêche au saumon ? Bienvenue dans la pêche de la baie de Bristol.

Chaos absolu. Des centaines de bateaux se claquent les uns dans les autres. Filets de pêche jetés les uns sur les autres. Les marées montent et tombent à l’heure. Les patrouilleurs, les avions et les hélicoptères surveillent les coordonnées GPS toutes les minutes de chaque jour pour s’assurer que personne ne traverse la frontière. And if you do? At best, you're looking at a $5,000 fine.

Bienvenue dans la pêche de la baie de Bristol, qui abrite la plus grande course de saumons rouges sauvages au monde.

La saison de quatre semaines débute à la mi-juin, alors que le saumon 50 millions se rend jusqu’aux frayères aux amont des quatre districts fluviaux principaux ; Naknek/Kvichak, Nushagak, Egegik et Ugashik. During this time, 1,500 boats will voyage to southwestern Alaska to partake in their most thrilling yet exhausting month of the year. Chaque bateau transportera entre quatre et six pêcheurs qui endureront des jours de 20 heures sur l’eau pendant un mois entier, sans vous aventurer en arrière sur les terres. De nombreux participants feront la vie de toute l’année en leur temps dans la baie de Bristol, ce qui rend la construction de nouveaux bateaux de pêche commerciaux phénoménaux en valent la peine.

F/V non coupable
Une paire de moteurs Cummins QSC 8.3 générant chacun 600 HP à 2800 tr/min puissance F/V non coupable (photo).

The competition at Bristol Bay is at an all-time high with the run exceeding 50 million for five years straight; a historical best in 2018 at 62.4 million. Ce niveau de succès a permis aux pêcheurs de s’assurer que leurs bateaux sont les plus grands et les plus puissants de l’eau. Afin de battre l’autre gars, vous avez obtenu d’avoir le meilleur. C’est pourquoi de nombreux constructeurs de bateaux font appel aux moteurs de série B, C et M de Cummins. Le QSC 8.3 est le plus populaire grâce à sa structure légère et puissante. Atteignant 600 HP et une puissance commerciale légère, ce moteur a une longueur d’avance sur le marché de la pêche dans la baie de Bristol.

Jeff Johnson, de bateaux pèlerins, affirme que « Cummins est très favorable à l’allumette d’un moteur avec l’application de notre jet afin d’obtenir les meilleures performances possible dans un bateau de baie. » Jeff a construit une poignée de bateaux Cummins pour ses clients, mais possède également deux navires commerciaux plus gros lui-même.

«En ce qui me concerne, il n’y a pas de meilleur moteur. La correspondance et le service de Cummins se démarque, je ne le ferai pas... recommander tout autre... pour mon application.»

En plus des qualités déjà mentionnées, la baie de Bristol est également unique en raison de son emplacement éloigné. Il n’y a que deux façons d’y arriver : en avion ou en bateau. C’est pourquoi deux attributs principaux ont mis Cummins à part leurs homologues pendant la saison de pêche commerciale.

Tout d’abord, c’est un service local. Cummins marine pilotera deux techniciens au sud-ouest de l’Alaska pendant l’été pour aider nos clients à pêcher la baie. Dans un environnement aussi concurrentiel et si bref d’une saison, il est crucial de disposer d’un soutien technique 24h/24. Même une heure de temps d’arrêt n’est qu’une occasion perdue.

La disponibilité des pièces est le deuxième atout essentiel. Les produits Cummins sont fabriqués aux États-Unis et facilement accessibles dans un court laps de temps. Cela rend notre produit beaucoup plus commode lorsque des solutions sont nécessaires rapidement.

Au cours de l’année prochaine, 10 nouveaux bateaux de 1200 HP seront touchés par la flotte commerciale de Bristol Bay, , le tout propulsé par des moteurs Cummins Twin . Ces bateaux rejoindront le combat rempli d’adrénaline pour le titre le plus rapide et le plus puissant de la baie de Bristol. Bientôt, leur teint brillant et leur extérieur lustré seront battus par des contusions résultant de pousser le bateau et l’équipage vers leurs limites ultimes. Mais ils apprécieront le chaos absolu et total qui ne peut se caractériser que par les quatre courtes semaines par an passées à la pêche de la baie de Bristol.

Katie Yoder-Cummins Inc.

Katie Yoder

Katie Yoder est une spécialiste en communications marketing. Nouveau chez Cummins en 2018, Katie s’est jointe à l’équipe des opérations de commercialisation où elle appuie les initiatives en matière de foires commerciales en Amérique du Nord. En tant qu’ancienne diplômée de l’Université d’Wisconsin, Katie aime observer les sports de blaireau pendant son temps libre.

Redirection vers
cummins.com

L'information que vous cherchez se trouve à cet endroit :
cummins.com

Nous lançons ce site pour vous maintenant.

Merci.