Energy IQ : trois tendances qui changeront l’avenir de l’infrastructure de soins de santé

What does the future of health care look like? An increasingly connected, less centralized and more resilient infrastructure lies ahead.

As we continue to look at the changing infrastructure of health care, we expect changes in three specific areas over the next decade. 

Trend No. 1: A more connected health care infrastructure

Today - A combination of consumers accessing health care differently and the increased adoption of technology, ranging from Internet of Things (IoT) to artificial intelligence (AI), will lead to a more connected health care infrastructure.

Healthcare IoT
IoT is used in healthcare for varying purposes by different stakeholders. 

As consumers increasingly use virtual visits, the health care industry will need to build facilities that can host tele-doctors and tele-nurses; and these facilities will need to be equipped with reliable connectivity to operate efficiently. Additionally, as consumers and the industry adopt IoT devices for tasks ranging from patient monitoring to imaging devices, there will be an increasing need to build the infrastructure supporting the technology.

Future - IoT devices will make more tasks dependent on electrical power while improving the facilities’ productivity. Facilities will seek a higher quality electricity supply for their sensitive IoT devices and be more critically dependent on reliable power sources to stay always on.   

Opportunity – Health care companies balancing reliability and efficiency as they consume power could lead others in customer satisfaction and physician productivity. A power outage at a health care facility is already catastrophic today and it will get more damaging as the health care infrastructure gets more connected. Increased use of IoT devices in more medical tasks and facilities will make more patients vulnerable to power outages. Increasing virtual visits mean more medical staff at risk of losing productivity if the power is out. 

Trend No. 2: A less centralized health care infrastructure

Today – Two factors are driving trends towards a less centralized health care infrastructure.

First is the advancement in clinical procedures. Thanks to less invasive procedures and technologies such as robotics, procedures once needing long inpatient stays can now be outpatient procedures that are conducted in hospitals, or they can be procedures conducted in other health care facilities1. This advancement fuels the growth in urgent care clinics, medical office buildings and ambulatory facilities2.

The second factor is the various mergers and acquisitions that occur within the health care eco-system. These mergers and acquisitions result in health care companies acquiring each other's assets including various type of facilities. When a merger and acquisition is focused on vertical integration, the resulting company ends up with more diversified facilities.

Future - We expect the health care infrastructure to feature a more diverse range of facilities and be more geographically spread out; "hub and spoke" is the term commonly used for this future growth. 

Opportunity – Companies in the health care industry can generate a competitive advantage by perfecting their capabilities in managing their diversified and geographically spread facilities.

"Mastering the facilities management in the next decade will be a key enabler of 'better care at a lower price' objective," said Wissam Balshe, Director of Systems and Controls Segment at Cummins Power Systems. "To help our partners in the industry, we are investing in the advancement of our remote monitoring capabilities. This includes everything from remote diagnostics to advanced condition-based maintenance and prognostics."

Trend No. 3: A more resilient health care infrastructure

We too often read about health care facilities losing power and the catastrophic outcomes. Severe weather continues to be the top cause of power outages, and as changing weather patterns put increasing strain on the electricity grid, we expect there will be more focus in incorporating reliable back-up power systems in health care facilities. We will take a closer look at how increasing frequency of power outages shape the future of health care infrastructure in our upcoming "How increasing instances of severe weather events impact health care infrastructure" article.

In summary, the decade ahead will bring out a more connected health care infrastructure with the increasing use of IoT devices and virtual visits. The evolving health care infrastructure will also feature a more diversified range of facilities that are geographically more spread out. Health care companies that master facilities management and include not only reliable but also efficient power systems in their infrastructure will lead others in consumer satisfaction and financials.

To learn more about trends in health care industry follow Cummins on Facebook and LinkedIn. To learn more about power solutions for health care industry, visit our web page. To learn more about how Cummins is powering a world that's "Always On," visit our web page.

Pensez-vous que vos amis et collègues aimeraient ce contenu ? Partagez sur LinkedIn et Facebook.

Références:
1 2019 Global health care outlook, Deloitte [PDF file]. (2019). Ce document provient de https://www2.deloitte.com.
2 Avis E. & Morgan J. (2019). 2019 Hospital Construction Survey [Web Post]. Retrieved from https://www.hfmmagazine.com/

 

Augmentez votre énergie IQ

Développez professionnellement avec les tendances énergétiques et les idées fournies dans votre boîte de réception. Apprenez-en plus sur les technologies et les tendances énergétiques sur notre Energy IQ hub .

Aytek Yuksel-Cummins Inc

Aytek Yuksel

Aytek Yuksel est le responsable du marketing de contenu de Cummins Inc., en se concentrant sur les marchés des systèmes d’alimentation. Aytek s’est joint à l’entreprise en 2008. Depuis, il a occupé plusieurs postes de marketing et vous offre maintenant les enseignements tirés de nos marchés clés, allant des marchés industriels au secteur résidentiel. Aytek vit à Minneapolis, au Minnesota, avec sa femme et ses deux enfants.

Q&A : sensibilisation à la sécurité thermique

While summer typically brings plenty of fun in the sun, it also means families need to be prepared for the dangers of extreme heat. 

On July 10, 1913, the United States experienced the hottest temperature ever recorded at 134.1°F in Death Valley, California. While most of us will never experience a temperature that high in our lifetimes, extreme heat still calls for vital safety measures during the summer. At Cummins, we want you to have the information available to stay safe all season long.

What are the dangers of extreme heat?

Heat Exhaustion Symptoms

  • Sweating, clammy, pale skin
  • Weak, rapid pulse
  • Headache, muscle cramps
  • Weakness, fatigue, dizziness
  • Nausea or vomiting

Actions to take: 

  • Move to a cool place with A/C
  • Lie down and rest with feet elevated
  • Stay hydrated with water
  • Cool your body with cold, wet cloths
  • Loosen clothing
  • Seek medical help if vomiting occurs or symptoms worsen

Heat Stroke Symptoms:

  • Fever of 103 or higher
  • Dry, red and hot skin with no sweating
  • Fast, strong pulse
  • Dizziness, nausea, throbbing headache
  • Loss of consciousness or seizure

Actions to take: 

  • Call 911 immediately
  • Move person to a cool place
  • Lower person's body temperature with cold water, wet cloths and fanning
  • Place ice packs on neck, arm pits and groin
  • Death is possible if untreated

What are some safety tips during a heat wave?

  • Do not leave children or pets alone in hot vehicles
  • Stay inside during the hottest part of the day (10 a.m. - 4 p.m.) and limit time outside in the sun
  • If A/C is not available, stay indoors on the lowest floor in a well-ventilated area with fans
  • Keep shades and blinds closed
  • Stay hydrated with plenty of water
  • Avoid alcohol and soda as they make dehydration worse
  • Limit strenuous activity and postpone outdoor games and events
  • Apply sunscreen frequently, wear a hat and light-colored clothing
  • Entertain yourself at air-conditioned public spaces such as malls, movie theaters or libraries
  • Check on family and friends with special needs, those who may not have A/C or live alone
  • Keep your pets indoors and ensure they are in a cool space and have plenty of water
  • Listen for weather updates from the National Weather Service on a NOAA weather radio
  • Allez à un refuge public désigné si votre maison perd de la puissance pendant les périodes de chaleur extrême. Text SHELTER + your ZIP Code to 43362 (4FEMA) pour trouver l’abri le plus près de votre région (par exemple : Shelter 12345) et écouter vos fonctionnaires locaux pour les emplacements d’abris.

Génératrice d’urgence pour la maison de CumminsHow should I prepare for extreme heat?

  • Consider a home standby generator that will keep your home cool in the event of an outage
  • Properly install window air conditioners (sealing any cracks) and insulate if necessary
  • Check A/C ducts for proper insulation and clean filters
  • Install awnings, blinds or light-colored drapes to keep sunlight and heat out
  • Upgrade your windows and weather-stripe door to keep heat out and cool air in
  • Get trained in first aid and CPR

How can a generator keep me safe during a heat wave?

  • Home generators will keep your essential functions – like air conditioning – operating in the event of an outage
  • An automatic transfer switch will ensure your generator starts immediately once your power goes out, so you don’t have to go outside or leave your home
  • Portable generators can provide power to smaller items, like a window A/C unit to keep you cool when experiencing extreme heat

Get your free in-home assessment now or find a local dealer.

Cheryl Nelson, météorologue de radiodiffusion certifié

Cheryl Nelson

Cheryl Nelson est une météorologue, animateur de télévision, instructeur certifié FEMA et conseiller en météorologie et en préparation pour Cummins. Vous pouvez visiter le site Web de Cheryl à www.PrepareWithCher.com et suivez-la sur Twitter et Facebook @CherylNelsonTV.

Les puissances marines de Cummins aventuristes autour de la grande boucle

Bill et Amy Denison
Bill and Amy Denison complete the 6,500-mile journey around the Great Loop

Beaucoup de marins ont la grande boucle sur leur liste de seau, mais seulement quelques-uns sont assez chanceux pour accomplir la tâche. Bill et Amy Denison font partie de ces quelques-uns. With great pride, they were able to complete the 6,500-mile journey down the east coast, up the inland rivers and back across the great lakes.

Leur voyage a commencé dans les eaux du Maine et de la Nouvelle-Écosse. Bill et Amy se sont bordés le long de la côte pour visiter les îles éloignées de leur bateau, Mar-Kat, une back Cove 41 portant le nom de leurs filles, Margaret et Kathleen. Ils ont décidé qu’ils voulaient s’aventurer plus loin et se sont joints à l’American Great Loop Cruising Association (AGLCA).

Après six mois de recherche et de planification, le couple a dit adieu à ses amis et à sa famille pour s’être mis en route pour s’attaquer à la grande boucle. Partant le 15 juin 2018, d’Albemarle Sound en Caroline du Nord, ils se dirigent vers le Sud. Mar-Kat est propulsé par un moteur diesel marine Cummins de 710 chevaux et une génératrice marine Cummins Onan de 9 kW.Bateau motorisé Cummins marine

Au cours de son voyage, Bill et Amy ont voyagé dans 13 États et dans la province de l’Ontario, passant par 100 écluses et ayant accumulé près de 500 heures de bateau. En complétant la boucle dans le sens anti-horaire, ils ont pu tirer parti des courants de la rivière SWIFT.

Bill a déclaré : « le moteur Cummins QSM11 a fonctionné sans faille tout au long du voyage et n’a besoin que de quelques changements d’huile. » Lorsque l’entretien du service était indispensable, le couple est entré en contact avec son distributeur local et « a reçu un bon soutien de la part de l’équipe de Cummins Virginia ».

Avec des éléments de conception robustes uniques, les petits moteurs diesel de Cummins ont une durée de vie utile du moteur et offrent des performances d’accélération et de couple éprouvées. Ce moteur marin fiable à quatre soupapes par cylindre est approuvé par des centaines de fabricants et se trouve dans les salles de moteur des bateaux de plaisance partout dans le monde. De plus, avec plus de 8 000 concessionnaires et distributeurs, le produit Cummins offre aux clients la tranquillité d’esprit dont ils ont besoin, peu importe où leur voyage les emmène.

Après avoir terminé avec succès la grande boucle en 10 mois, Bill et Amy préparent maintenant leur prochaine aventure avec Mar-Kat, peut-être en explorant la Floride ou les Bahamas du Sud. Peu importe où ils se dirigent ensuite, Cummins fournira la puissance, l’innovation et la fiabilité pour conduire son voyage.

Découvrez la gamme de produits marins Cummins au cummins.com/marine pour voir comment nos groupes moteurs et nos génératrices peuvent alimenter vos voyages, sur la mer ou sur terre.

Vous avez besoin d’aide pour choisir la bonne solution pour votre bateau ? Trouvez votre représentant Cummins local

Immeuble de bureaux Cummins

Cummins Inc.

Cummins est un chef de file mondial en alimentation qui conçoit, fabrique, vend et entretient des moteurs au diesel et aux carburants de remplacement de 2,8 à 95 litres, des ensembles de génératrices électriques diesel et de remplacement de 2,5 à 3, 500 kW, ainsi que des composants et de la technologie connexes. Cummins dessert ses clients par l’entremise de son réseau de 600 installations de distributeurs indépendantes et détenues par l’entreprise, et de plus de 7 200 concessionnaires répartis dans plus de 190 pays et territoires.

Microgrille historique hybride d’énergie renouvelable de l’Australie complétée par une production d’électricité thermique de Cummins Power Generation

La génératrice à essence Cummins QSV91G et les groupes moteurs diesel QSK60 appuient la microgrille d’énergie renouvelable de la mine d’or Agnew.
La génératrice à essence Cummins QSV91G et les groupes moteurs diesel QSK60 appuient la microgrille d’énergie renouvelable de la mine d’or Agnew.

Avec une capacité installée de 56 MW, la nouvelle centrale hybride renouvelable d’Agnew est devenue la plus grande microgrille d’énergie renouvelable hybride de l’Australie, et la première à utiliser la production éolienne dans une mine. L’énergie produite équivaut à alimenter 11 500 maisons et à consommer 46 et 400 tonnes de dioxyde de carbone la première année seulement.

Station d’alimentation renouvelable hybride Agnew, AustralieAvec une capacité installée de 56 MW, la nouvelle centrale hybride renouvelable d’Agnew est devenue la plus grande microgrille d’énergie renouvelable hybride de l’Australie, et la première à utiliser la production éolienne dans une mine. L’énergie produite équivaut à alimenter 11 500 maisons et à consommer 46 et 400 tonnes de dioxyde de carbone la première année seulement.

«Les technologies de l’énergie renouvelable de la nouvelle centrale hybride renouvelable de l’EDL sont complétées par la production thermique des génératrices à essence et au diesel de Cummins, a déclaré Jason Dickfos, directeur de la croissance de l’EDL. « Nous sommes heureux de travailler avec Cummins pour réaliser ce projet historique, qui fournira la mine d’or Agnew avec plus de 50% d’énergie renouvelable à long terme, sans compromettre la qualité de l’alimentation ni la fiabilité. »

La solution hybride d’énergie renouvelable de la mine de gisements aurifères en Australie-occidentale se compose d’une nouvelle centrale électrique hors réseau de 23 MW incorporant du gaz, du solaire photovoltaïque et de la production d’électricité diesel, suivie d’une génération de vent de 18 MW, d’une batterie de 13 MW et d’un système de commande de de de pointe. Une exigence cruciale était que les génératrices devaient offrir une alimentation fiable et continue à des températures allant jusqu’à 45 ° c. Le modèle de génératrice à essence Cummins QSV91G a été choisi en raison de sa capacité à fonctionner dans des conditions ambiantes élevées, en plus d’offrir des charges d’étape à impact élevé et des débits de rampe rapides tout en conservant la qualité de l’alimentation, tandis que les unités diesel Cummins QSK60 fournissent une alimentation supplémentaire pendant les périodes de pointe de la demande et disposent de capacités de démarrage noir en cas de panne

En savoir plus sur l’Agnew de dans cette étude de cas .

Angela Papageorgiou

Angela Papageorgiou est la spécialiste principale en communications marketing pour le secteur de la gestion de l’énergie de Cummins Inc. avant de se joindre à Cummins en 2014, elle a travaillé pour des organismes de communication en marketing soutenant l’élaboration et l’exécution de projets de campagne B2C et B2B. [email protected]

Energy IQ : trois situations qui maximisent les avantages des applications de cogénération

Trois situations qui maximisent les avantages des applications de cogénération
Trois situations qui maximisent les avantages des applications de cogénération

Les serres, les hôpitaux, les fabricants industriels et les propriétaires de bâtiments commerciaux sont quelques-uns des nombreux se tournant vers la cogénération, également connue sous le nom de Combined Heat and Power (CHP). Ils bénéficient d’avantages allant de l’amélioration de la performance financière à la réduction de l’empreinte environnementale. Le rendement élevé des applications de cogénération dans la conversion de l’énergie du carburant d’origine en énergie utile est le fondement de ces avantages.

Ces avantages des applications de cogénération sont encore plus amplifiés dans certaines situations. Couvrons ces situations et les exemples associés d’applications de cogénération.

No. 1 : certains aspects de votre entreprise fonctionnent 24/7

Les systèmes de cogénération les plus rentables fonctionnent à pleine puissance 24/7.

Cela ne signifie pas que votre entreprise a besoin d’exécuter 24/7. Au lieu de cela, vous pouvez identifier les aspects de votre entreprise qui gèrent le 24/7, et les alimenter avec un système de cogénération. Entre-temps, vous pouvez toujours avoir la connexion de services publics et les chaudières sur place. Ces derniers sont utiles pour alimenter le reste de vos activités commerciales et pour gérer les pics potentiels de la demande en électricité ou en énergie thermique. Un autre avantage de l’utilisation d’une combinaison de la cogénération et de l’alimentation des services publics est autour des événements d’entretien. Cette combinaison vous permet d’effectuer l’entretien et le service de votre système de cogénération sans interrompre l’accès à l’électricité pour votre entreprise.

Les hôpitaux sont un bon exemple d’applications de cogénération pour ce scénario. Le contrôle de la température, la gestion de la qualité de l’air, le maintien de l’équipement médical et de nombreuses autres activités requièrent de l’électricité et de l’énergie thermique tout au long de la journée.

N ° 2 : le besoin d’énergie thermique est cohérent ; Il est également simultané avec le besoin d’électricité plusieurs mois de l’année

De nombreuses installations exploitent des applications de cogénération avec une popularité croissante au fil des années.
De nombreuses installations exploitent des applications de cogénération avec une popularité croissante au fil des années.

La vente ou le stockage de l’excédent d’énergie thermique n’est souvent pas pratique. L’excès de chaleur est généralement rejeté comme chaleur de rebut, réduisant ainsi l’efficacité globale et les gains financiers de l’application de cogénération. L’efficacité d’un système de cogénération augmente lorsque les besoins thermiques (vapeur, eau chaude ou eau réfrigérée) demeurent à un niveau constant. La même chose ne s’applique pas autant aux besoins en électricité, puisque l’excès d’électricité pourrait souvent être revendu à l’utilitaire électrique.

Plus le besoin simultané d’électricité et d’énergie thermique est long, plus une application de cogénération est avantageuse. En fait, une bonne orientation est de considérer les applications de cogénération si votre entreprise a des besoins simultanés en électricité et en chauffage/refroidissement environ la moitié de l’année ou plus 1 . Il y a des exceptions à cela, et certaines applications sont réalisables même lorsque le besoin simultané est de 2, 000 heures par an, environ trois mois.

La fabrication industrielle est un bon exemple d’une application de cogénération pour ce scénario. L’énergie thermique nécessaire dans le traitement industriel tend à être cohérente tout au long de l’exploitation de l’usine. De plus, l’énergie thermique et l’électricité sont généralement nécessaires en même temps tout au long de l’année dans ces installations.

N ° 3 : les prix de l’électricité sont élevés par rapport au coût du gaz naturel

Vous vous améliorez financièrement si la production d’électricité sur place est moins coûteuse que l’achat d’électricité à partir de l’utilitaire. De nombreux systèmes de cogénération produisant de l’électricité sur place utilisent le gaz naturel comme carburant, et c’est là que la propagation de l’étincelle entre en jeu.

La propagation à l’étincelle est une mesure permettant d’estimer la rentabilité des génératrices électriques alimentées au gaz naturel. C’est la différence entre le prix de l’électricité et le coût du gaz naturel nécessaire pour produire cette électricité 2 . À mesure que la propagation de l’étincelle augmente, les économies fournies par un système de cogénération augmentent également. La propagation des étincelles est un indicateur de viabilité financière, mais ce n’est pas une mesure exacte de la rentabilité.

Les installations où le coût de l’électricité est élevé et que le gaz naturel comme carburant sont offerts sont de bons exemples d’applications de cogénération pour ce scénario.

Au-delà des facteurs ci-dessus, le évaluant la cogénération pour votre installation le livre blanc décrit d’autres aspects à considérer lorsque vous explorez la cogénération en option.

Inscrivez-vous ci-dessous pour Energy IQ afin de recevoir des renseignements axés sur l’énergie sur les marchés allant des centres informatiques aux établissements de soins de santé aux installations de fabrication, et tout cela au-delà. Pour en savoir plus sur les offres de cogénération et de Trigeneration Power solutions de Cummins Inc., visitez notre page Web .

Pensez-vous que vos amis et collègues aimeraient ce contenu ? Partagez sur LinkedIn et Facebook.

Références:
1 Hamilton, J. (n.d.). Evaluer la cogénération pour votre établissement [bulletin]. Cummins Inc. ce document provient de https://www.cummins.com.
2 U.S. Energy administration Office (2013 février). Introduction aux écarts d’allumage. Ce document provient de https://www.eia.gov/.
 

Augmentez votre énergie IQ

Développez professionnellement avec les tendances énergétiques et les idées fournies dans votre boîte de réception. Apprenez-en plus sur les technologies et les tendances énergétiques sur notre Energy IQ hub .

Aytek Yuksel-Cummins Inc

Aytek Yuksel

Aytek Yuksel est le responsable du marketing de contenu de Cummins Inc., en se concentrant sur les marchés des systèmes d’alimentation. Aytek s’est joint à l’entreprise en 2008. Depuis, il a occupé plusieurs postes de marketing et vous offre maintenant les enseignements tirés de nos marchés clés, allant des marchés industriels au secteur résidentiel. Aytek vit à Minneapolis, au Minnesota, avec sa femme et ses deux enfants.

Redirection vers
cummins.com

L'information que vous cherchez se trouve à cet endroit :
cummins.com

Nous lançons ce site pour vous maintenant.

Merci.