Cummins comienza a probar el motor de combustión interna alimentada por hidrógeno

- Cummins began testing a hydrogen-fueled internal combustion engine.
- Following the proof-of-concept testing, the company plans to evaluate the engine in a variety of on- and off-highway applications.
Cummins Inc. (NYSE: CMI) has taken another step forward in advancing zero carbon technology as the company began testing a hydrogen-fueled internal combustion engine. La prueba de prueba de concepto se basa en el liderazgo tecnológico existente de Cummins en aplicaciones de combustible gaseoso y liderazgo del tren motriz para crear nuevas soluciones de energía que ayuden a los clientes a satisfacer las necesidades energéticas y ambientales del futuro.
"Cummins is thrilled about the potential of the hydrogen engine to reduce emissions and provide power and performance for customers," said Srikanth Padmanabhan, President of the Engine Segment. "We are using all new engine platforms equipped with the latest technologies to improve power density, reduce friction and improve thermal efficiency, allowing us to avoid the typical performance limitations and efficiency compromises associated with converting diesel or natural gas engines over to hydrogen fuel. We have made significant technological advancements and will continue moving forward. We are optimistic about bringing this solution to market."
Following the proof-of-concept testing, the company plans to evaluate the engine in a variety of on- and off-highway applications, supporting the company’s efforts to accelerate the decarbonization of commercial vehicles.
“The hydrogen engine program can potentially expand the technology options available to achieve a more sustainable transport sector, complementing our capabilities in hydrogen fuel cell, battery electric and renewable natural gas powertrains,” said Jonathon White, Vice-President of Engine Business Engineering.
Hydrogen engines offer OEMs and end-users the benefit of adaptability by continuing to use familiar mechanical drivelines with vehicle and equipment integration mirroring that of current powertrains while continuing to provide the power and capability for meeting application needs.
The hydrogen engines can use green hydrogen fuel, produced by Cummins-manufactured electrolyzers, emitting near zero CO2 emissions through the tailpipe and near zero levels of NOx. La inversión proyectada en la producción de hidrógeno renovable a nivel mundial brindará una oportunidad cada vez mayor para el despliegue de flotas con motor de hidrógeno que utilizan la energía de la célula de combustible de Cummins o la de los motores.
Integrating Hydrogen Technology
Cummins is investing across a range of technologies to support hydrogen-based transportation including hydrogen engines, fuel cells, electrolyzers and storage tanks.
The high energy density of hydrogen enables easily integrated on-board gas storage without compromising either the vehicle payload or operating range. Cummins' joint venture partnership with hydrogen storage specialist NPROXX adds the ability to integrate the fuel cell or hydrogen engine with the high-pressure gas cylinder tanks and supply lines on the vehicle. NPROXX is also a leading supplier of containerized storage vessels, enabling fast hydrogen refueling for end users.
Cummins' pivotal role in expanding the hydrogen ecosphere goes beyond fuel cells and storage solutions to the manufacture of decarbonized renewable hydrogen, with the experience of more than 600 electrolyzer installations across the globe. The modular scalability of our electrolyzers are ideally suited for a range of applications, from the localized supply of truck and bus fleets to utility-scale electrolysis. Cummins has unique hydrogen capabilities extending from fuel production to storage and vehicle power.
Cummins Inc., líder mundial en tecnología de energía, es una corporación de segmentos de negocios complementarios que diseñan, fabrican, distribuyen y servicio una amplia cartera de soluciones de energía. Los productos de la compañía abarcan desde combustión interna, soluciones eléctricas e híbridas integradas de energía y componentes, incluyendo filtración, postratamiento, turbocompresores, sistemas de combustible, sistemas de control, sistemas de control de aire, transmisiones automatizadas, sistemas de generación de energía eléctrica, controles de microred, baterías, electrolitos y productos de células de combustible. Con sede en Columbus, Indiana (EE. UU.), desde su fundación en 1919, Cummins emplea aproximadamente a 59,900 personas comprometidas con impulsar un mundo más próspero a través de tres prioridades de responsabilidad corporativa global fundamental para comunidades saludables: educación, medio ambiente e igualdad de oportunidades. Cummins atiende a sus clientes en línea, a través de una red de ubicaciones de distribuidores independientes y propiedad de la compañía, y a través de miles de ubicaciones de distribuidores en todo el mundo y ganó alrededor de $2,1 mil millones en ventas de $24 mil millones en 2021. Más información en cummins.com .