Cummins utiliza tecnología de hidrógeno para que los servicios públicos de Washington puedan usar tecnología renovable con el electrolizador PEM más grande de los Estados Unidos

Douglas County, Washington (USA)
Wells Dam - Estado de Washington - Cummins

Global technology and power solutions leader Cummins Inc. (NYSE: CMI) will provide its 5-megawatt PEM electrolyzer to enable renewable energy for the Douglas County Public Utility District (Douglas County PUD) in Washington state. El electrógeno Cummins se dedicará a producir hidrógeno a partir de energías renovables y será el más grande, y el primero de su tipo, en uso por parte de una compañía de servicios públicos, en los Estados Unidos.

Expected to be operational in 2021, the new renewable hydrogen facility allows the Douglas County PUD to manufacture commercial hydrogen using electrolysis to harvest hydrogen from water from Wells Dam on the Columbia River. The PEM electrolyzer system, which stands for proton exchange membrane, takes the excess renewable energy and through a chemical reaction splits water into hydrogen and oxygen. El hidrógeno actúa como un portador de energía y el oxígeno se libera al aire. Luego, el hidrógeno se puede almacenar en estado gaseoso o líquido para utilizarlo en una multitud de aplicaciones, incluida la movilidad eléctrica de pilas de combustible. The electrolyzer is powered by clean hydroelectricity, so the production of hydrogen does not generate any carbon emissions.

“At Cummins, we believe that scaling hydrogen technologies will continue to grow low-carbon solutions,” said Amy Davis, Cummins Vice President and President of New Power, the company’s alternative power business.

"It takes enterprises, governments and utilities working together, like what we have done with Douglas County PUD, to make alternative power a reality and promote a more sustainable world. Douglas County PUD is just one example of how Cummins is expanding the energy market and driving new power solutions for our customers."

The electrolyzer technology provides a means to address one of the largest dilemmas in the renewable energy industry, which is how to store the energy when it's not in demand. Cummins' PEM electrolyzers, like Douglas County PUD's electrolyzer plant, enables utilities to store the excess energy that they would typically sell off to the market at a financial loss, or not harness at all, and instead store that energy to sell into a new green hydrogen market. Additionally, it creates a way for utilities to engage in new market opportunities outside of their typical service area, removing growth barriers often faced in the industry.

Cummins hydrogen electrolyzer

"Douglas County PUD is excited to work with Cummins' Fuel Cell and Hydrogen Technologies on our 5-megawatt hydrogen electrolyzer project. This hydrogen plant will create efficiencies for our Wells Hydroelectric Project and create a new renewable hydrogen gas resource for our community," said Gary Ivory, General Manager of Douglas County PUD. "As the first renewable hydrogen production plant in Washington State, we understand the importance of great partners, and we believe Cummins' will help us build a successful project."

This electrolyzer project is a part of an initial 5-megawatt project made possible by the passage of Senate Bill 5588 in Washington state last year, which authorized public utility districts to make and sell hydrogen. It will be built in the Baker Flats Industrial Park, which is located outside East Wenatchee and will use surplus hydropower from the Wells Dam Facility to produce renewable hydrogen.

"This project is a watershed, a first step into the huge economic and environmental opportunity that our growing use of clean power offers," said Ken Dragoon, Executive Director of the Renewable Hydrogen Alliance. "For the first time, the Northwest will produce clean fuels from renewable electricity-and the Douglas County PUD's innovative plan will use their electrolyzer's flexibility to free up valuable capacity on their dam."

Already a leader in advanced diesel, natural gas and battery technologies, Cummins is rapidly growing its hydrogen capabilities and the company continues to deepen its expertise in fuel cell technologies. Cummins uses fuel cell and hydrogen technologies to power a variety of applications, including transit buses, semi-trucksdelivery trucks, refuse trucks and passenger trains,and has made several announcements in the past year related to hydrogen and fuel cell technologies. These include the acquisition of Hydrogenics Corporation in September 2019, providing Cummins with both PEM, alkaline fuel cells, and electrolyzers used to generate hydrogen. Cummins has also invested in LOOP Energy, signed a memo of understanding with Hyundai Motor Company, entered an agreement to form a joint venture with NPROXX>, and invested in the development of solid oxide fuel cells.

For more examples of how Cummins has supported new firsts in the fuel cell and hydrogen industry and for more information about Cummins Fuel Cell and Hydrogen Technologies, please visit www.cummins.com/new-power.

Acerca de Cummins Inc.

Cummins Inc., líder mundial en tecnología de energía, es una corporación de segmentos de negocios complementarios que diseñan, fabrican, distribuyen y servicio una amplia cartera de soluciones de energía. Los productos de la compañía abarcan desde combustión interna, soluciones eléctricas e híbridas integradas de energía y componentes, incluyendo filtración, postratamiento, turbocompresores, sistemas de combustible, sistemas de control, sistemas de control de aire, transmisiones automatizadas, sistemas de generación de energía eléctrica, controles de microred, baterías, electrolitos y productos de células de combustible. Con sede en Columbus, Indiana (EE. UU.), desde su fundación en 1919, Cummins emplea aproximadamente a 59,900 personas comprometidas con impulsar un mundo más próspero a través de tres prioridades de responsabilidad corporativa global fundamental para comunidades saludables: educación, medio ambiente e igualdad de oportunidades. Cummins atiende a sus clientes en línea, a través de una red de ubicaciones de distribuidores independientes y propiedad de la compañía, y a través de miles de ubicaciones de distribuidores en todo el mundo y ganó alrededor de $2,1 mil millones en ventas de $24 mil millones en 2021.

Contacto de medios
Imágenes de la historia
Redirigiendo a
cummins.com

La información que busca está en
cummins.com

Ahora estamos iniciando ese sitio para usted.

Gracias.