La energía integrada de Cummins ofrece una opción para clientes para un mundo que está siempre en funcionamiento

Atlanta, Georgia
""

Cummins Integrated Power™ makes a debut at the Technology and Maintenance Council (TMC) Annual Meeting in Atlanta, Georgia

Cummins Inc. (NYSE: CMI), a global power leader, presents Cummins Integrated Power™, delivering choice to customers through a broad portfolio of solutions. With proven, reliable technologies, the Cummins Integrated Power portfolio features expertly paired engines and transmissions, componentry, advanced electronic engine features and connected technologies, bringing unmatched performance to the industry.

"As a global, independent supplier, Cummins is uniquely positioned to work with a variety of partners and suppliers to provide the broadest portfolio of integrated power to our customers," said Srikanth Padmanabhan, President of Cummins Engine Business. "Our expanding portfolio of diesel, natural gas, hybrid and electrified power is a testament to our dedication to delivering the right technology at the right time."

Integrated Diesel Power from Cummins
At TMC, Cummins will showcase the X12™ and the X15™ engine platforms, both paired with Eaton Cummins Automated Transmission Technologies Endurant™ transmissions, representing two integrated diesel power solutions from the Cummins Integrated Power portfolio. 

"Technology integration plays a huge role in how effective a customer's operations can be," said Mike Taylor, General Manager - Global Powertrain Integration. "Cummins has the knowledge and experience that allows us to optimize key technologies to deliver the power our customers expect."

In the medium-bore space, an integrated X12 powertrain will offer customers the lightest solution on the market today. With hundreds of pounds shed, the integrated X12 powertrain allows the customer to carry more freight on the vehicle, helping to make operations more efficient. The X12, with an innovative sculpted block design, weighs in at just 2,050lbs while maintaining rigidity and performance. With a peak rating of up to 500 hp (372 kW), the X12 has the highest power-to-weight ratio of any heavy-duty engine from 10 liters to 16 liters in size. Further weight reduction is achieved when the X12 is paired with the Endurant transmission, which is the lightest, most efficient 1,850 ft. lb. of torque capable transmission in the industry. And, when the Single Module™ aftertreatment system from Cummins Emission Solutions is applied, up to 40 percent more weight is saved when compared to earlier emissions systems.

In the big-bore space, an integrated X15 powertrain is designed with total cost of ownership in mind. With less maintenance to worry about, customers can put more focus on the job at hand. The X15 engine features reduced maintenance over prior 15L models from Cummins, with a 50,000 mile oil drain interval, but can reach up to an 80,000 mile interval through the Cummins OilGuard™ program. Additional maintenance reduction is achieved when using the Endurant, which offers the longest transmission oil change intervals for line haul applications at 750,000 miles and uses half as much oil as competitive automated transmissions. The Single Module aftertreatment takes total cost of ownership improvements a step further for the integrated X15 powertrain, offering longer ash cleaning intervals for many customer applications.

With each of these integrated diesel powertrains harnessing the power of the ADEPT™ suite from Cummins, customers can achieve even greater fuel economy gains with no impact to productivity, harnessing the electronic capabilities of the engine and transmission to make powertrain control decisions in real time. With each element of the Integrated Power portfolio further connected, customers can achieve more than ever.

At TMC (booth 2321) Cummins will also display the ISX12N™ from the natural gas power portfolio, which Cummins can pair with the right powertrain technologies to provide the performance our customers expect. Also on display from Cummins in TMC's Advanced Technology Pavilion (booth 1343) will be the AEOS concept vehicle to demonstrate Cummins' commitment to delivering choice to customers through the Cummins Integrated Power portfolio.

“Cummins has a long history of delivering reliable power and service to our customers, and our commitment to a growing Cummins Integrated Power portfolio will only enhance our offerings,” concluded Taylor.  

Acerca de Cummins Inc.

Cummins Inc., líder mundial en tecnología de energía, es una corporación de segmentos de negocios complementarios que diseñan, fabrican, distribuyen y brindan mantenimiento a una amplia cartera de soluciones energéticas. Los productos de la compañía abarcan desde soluciones de energía integrada de combustión interna, eléctrica e híbrida hasta componentes que incluyen filtración, postratamiento, turbocompresores, sistemas de combustible, sistemas de control, sistemas de control de aire, transmisiones automatizadas, sistemas de generación de energía eléctrica, controles de microrredes, baterías, electrolizadores y pilas de combustible. Con sede en Columbus, Indiana (EE. UU.), desde su fundación en 1919, Cummins emplea aproximadamente a 73,600 personas comprometidas con impulsar un mundo más próspero a través de tres prioridades de responsabilidad corporativa global fundamental para comunidades saludables: educación, medio ambiente e igualdad de oportunidades. Cummins atiende a sus clientes en línea, a través de una red de ubicaciones de distribuidores independientes y de propiedad de la empresa, y a través de miles de ubicaciones de distribuidores en todo el mundo, y ganó alrededor de $2.2 mil millones en ventas de $28.1 mil millones en 2022.

Contacto de medios
Molly Yedinak
Especialista en comunicaciones de marketing sénior
1-812-603-9955
Redirigiendo a
cummins.com

La información que busca está en
cummins.com

Ahora estamos iniciando ese sitio para usted.

Gracias.