CUMMINS ANUNCIA COMPATIBILIDAD CON COMBUSTIBLES DIÉSEL RENOVABLES SELECCIONADOS PARA MOTORES B6.7 Y L9

Cummins Inc. (NYSE: CMI) today announced that the B4.5, B6.7 and L9 engine platforms are compatible with paraffinic renewable diesel fuels meeting the EN 15940 specification. Both On-Highway and Off-Highway versions of the B6.7 and L9 platforms and all vintages are approved to use paraffinic diesel fuels in North America.
Cummins Inc. (NYSE: CMI) today announced that the B4.5, B6.7 and L9 engine platforms are compatible with paraffinic renewable diesel fuels meeting the EN 15940 specification. Both On-Highway and Off-Highway versions of the B6.7 and L9 platforms and all vintages are approved to use paraffinic diesel fuels in North America.
As with our announcement in September on our Euro VI platforms, this helps further reduce the carbon footprint of Cummins-powered bus, truck, agricultural and construction fleets operating around the world. Compared with conventional fossil-based diesel, paraffinic diesel fuels offer the potential to reduce greenhouse gas (GHG) emissions by 40 percent to 90 percent over the total life cycle of the vehicle.
Paraffinic diesel fuels can be used as a 100 percent substitute for standard EN 590 or ASTM D975 Ultra-Low Sulfur Diesel (ULSD) without requiring any change to the Cummins engine. No additional engine maintenance is required when using paraffinic fuels meeting the EN 15940 specification, and the same fuel filters are retained. Paraffinic diesel can easily be blended with standard diesel at varying percentages, including winter-grade fuels, and has the same stability and cold properties as conventional diesel, which means it can be used and stored in the same ways.
Cummins led an 18-month field trial running 100 percent paraffinic diesel fuel in order to understand changes in engine performance, aftertreatment effects and fuel system durability. Engine performance remained stable and consistent while using the paraffinic fuel, and customers should not expect to see any differences. Depending on the application and the engine duty cycle, a fuel economy detriment of 0 percent to 6 percent is expected due to the lower density of paraffinic fuels compared with regular diesel fuel.
A thorough analysis of the aftertreatment system showed that each subsystem - the Diesel Oxidation Catalyst (DOC), Diesel Particulate Filter (DPF) and Selective Catalytic Reduction (SCR) - remained stable throughout the test with performance similar to that of regular diesel fuel. The materials in the fuel system equipment (O-rings, injectors and pumps) are all compatible with EN 15940 diesel fuels.
"Focused on energy diversity and enabling the power of choice, Cummins has provided another approved fuel option to help the continued reduction of emissions. The use of paraffinic diesel allows customers to minimize their emissions-based footprints without additional capital investment. Plus, they have the comfort of knowing that Cummins conducted a thorough analysis prior to approval," said Jim Fier, Cummins - Vice President - Engineering.
Cummins approval for the use of renewable diesel with B6.7 and L9 engines aligns with
the recent introduction of EN 15940, a final European CEN specification for paraffinic diesel fuels, including hydrotreated vegetable oil (HVO), gas-to-liquids (GTL) and biomass-to-liquids (BTL). Operators of Cummins-powered trucks and buses are required to source all paraffinic fuels from high-purity suppliers meeting EN 15940, as this ensures that the fuel contains the necessary lubricity additive for use in a diesel engine.
Other light-duty, heavy-duty and high-horsepower platforms are currently undergoing a similar validation plan on 100 percent paraffinic fuels, and Cummins will be announcing the results of the studies throughout 2017.
Acerca de Cummins Inc.
Cummins Inc., a global power leader, is a corporation of complementary business units that design, manufacture, distribute and service diesel and natural gas engines and related technologies, including fuel systems, controls, air handling, filtration, emission solutions and electrical power generation systems. Headquartered in Columbus, Indiana (USA), Cummins currently employs approximately 55,400 people worldwide and serves customers in approximately 190 countries and territories through a network of approximately 600 company-owned and independent distributor locations and approximately 7,400 dealer locations. Cummins earned $1.39 billion on sales of $17.5 billion in 2016. Press releases can be found on the Web at www.cummins.com/news. Follow Cummins on Twitter at www.twittter.com/cumminsengines and on YouTube at www.youtube.com/cumminsengines.