Bundu Khan restaurant and bakery expands with Cummins standby power

The Cummins power systems at the bakeries provide 55 kVA of power to back up the main utility.
The Cummins power systems at the bakeries provide 55 kVA of power to back up the main utility.

Bundu Khan is an old venture in the Pakistani food industry that has become a household brand for barbeque cuisine. As a sole proprietor with its first bakery opening on Mall Road in Lahore in 1991, today Bundu Khan operates bakeries and restaurants in Lahore, Multan and now in Murree.

Bundu KhanCummins was selected as the backup power provider for Bundu Khan several years ago for the main office building. The customer recently added Cummins generators to the production plant and at each of the 11 branch locations. Authorized Cummins distributor Orient Energy Systems installed each of the units, comprising one Cummins C140D5, two C66D5 and 11 C55D5 generator sets. The power systems at the bakeries provide 55 kVA of power to back up the main utility. Tailor-made enclosures provide sound levels of 85 dBA at 1 meter.

OES was instrumental in providing exceptional service, often with short delivery lead times. While the customer plans to open a certain number of branches annually, unexpected delays in the planning phases can mean tight delivery deadlines to be ready for shop openings, which are also coordinated with annual festivals, explained OES Sales Manager Muzaffar Iqbal. To meet delivery lead times, OES is equipped with a stocking plan to meet the customer's unexpected needs as well.

"The customer has many options for backup power generation available in the local market, but due to OES' and Cummins' brand reputation for customer service, he is inclined toward Cummins," Iqbal said. "OES always strives for the best possible services and backup support."

For more information on standby power systems for commercial and business applications, visit cummins.com
 

Anisha George

Como especialista en comunicaciones de comercialización, Anisha respalda el marketing, las comunicaciones y la gestión de eventos para África y las regiones de Oriente Medio. Antes de incorporarse a Cummins en 2011, adquirió experiencia en la industria trabajando en el campo de la gestión de eventos. [email protegido] 

Q&A: conciencia de seguridad contra el calor

Mientras que el verano generalmente trae mucha diversión al sol, también significa que las familias deben estar preparadas para los peligros del calor extremo.

El 10 de julio de 1913, Estados Unidos experimentó la temperatura más caliente jamás registrada en 134.1 ° f en Death Valley, California. Si bien la mayoría de nosotros nunca experimentaremos una temperatura tan alta en nuestra vida, el calor extremo aún requiere medidas de seguridad vitales durante el verano. En Cummins, queremos que tenga la información disponible para mantenerse segura durante toda la temporada.

¿Cuáles son los peligros del calor extremo?

Síntomas de agotamiento por calor

  • Sudoración, pegajosa, piel pálida
  • Pulso débil y rápido
  • Dolor de cabeza, calambres musculares
  • Debilidad, fatiga, mareos
  • Náuseas o vómitos

Medidas a tomar:

  • Muévase a un lugar fresco con a/C
  • Recuéstese y descanse con los pies elevados
  • Manténgase hidratado con agua
  • Enfríe su cuerpo con paños fríos y mojados
  • Aflojar la ropa
  • Busque ayuda médica si ocurre vómitos o si los síntomas empeoran

Síntomas de la carrera de calor:

  • Fiebre de 103 o más
  • Piel seca, roja y caliente sin sudoración
  • Pulso rápido y fuerte
  • Mareos, náuseas, dolor de cabeza palpitante
  • Pérdida de consciencia o convulsiones

Medidas a tomar:

  • Llame al 911 inmediatamente
  • Mueva a la persona a un lugar fresco
  • Temperatura corporal de la persona más baja con agua fría, paños húmedos y Fanning
  • Coloque bolsas de hielo en el cuello, las axilas y la ingle
  • La muerte es posible si no se trata

¿Cuáles son algunos consejos de seguridad durante una ola de calor?

  • No deje niños o mascotas solos en vehículos calientes
  • Permanezca dentro durante la parte más caliente del día (10 a.m.-4 p.m.) y limite el tiempo al aire libre en el sol
  • Si el A/C no está disponible, permanezca en el interior del piso más bajo en una zona bien ventilada con ventiladores
  • Mantenga las persianas cerradas
  • Manténgase hidratado con abundante agua
  • Evite el alcohol y las gaseosas ya que empeoran la deshidratación
  • Limite la actividad extenuante y posponga juegos y eventos al aire libre
  • Aplique protector solar con frecuencia, use un sombrero y ropa de color claro
  • Entretenerse en espacios públicos con aire acondicionado como centros comerciales, cines o bibliotecas
  • Revise A su familia y amigos con necesidades especiales, aquellos que no pueden tener A/C o vivir solos
  • Mantenga a sus mascotas en el interior y asegúrese de que estén en un lugar fresco y que tengan mucha agua
  • Escuche las actualizaciones meteorológicas del Servicio Meteorológico Nacional en una radio meteorológica de NOAA
  • Vaya a un refugio público designado si su hogar pierde energía durante períodos de calor extremo. Texto SHELTER + su código postal a 43362 (4FEMA) para encontrar el refugio más cercano en su área (ejemplo: Refugio 12345) y escuchar a sus funcionarios locales para buscar ubicaciones de refugio.

Generador de reserva para el hogar Cummins¿Cómo debo prepararme para el calor extremo?

  • Considere un generador de reserva para el hogar que mantendrá su hogar fresco en caso de un corte de energía
  • Instale adecuadamente los acondicionadores de aire de la ventana (sellado de las grietas) y aíbase si es necesario
  • Revise los conductos de A/C para un aislamiento adecuado y filtros limpios
  • Instale toldos, persianas o cortinas de color claro para mantener la luz solar y el calor fuera
  • Actualice sus ventanas y la puerta con franjas de clima para mantener el calor fuera y el aire fresco en
  • Obtenga capacitación en primeros auxilios y RCP

¿Cómo puede un generador mantenerme a salvo durante una ola de calor?

  • Los generadores para el hogar mantendrán sus funciones esenciales, como el aire acondicionado, funcionando en caso de una interrupción
  • Un conmutador de transferencia automática garantizará que su generador se inicie inmediatamente después de que se apague la energía, para que no tenga que salir o salir de su casa
  • generadores portátiles pueden suministrar energía a artículos más pequeños, como una unidad de aire acondicionado de ventana para mantenerlo fresco cuando experimenta calor extremo

Obtenga su evaluación en el hogar gratis ahora o busque un distribuidor local.

Cheryl Nelson, meteoróloga de broadcast certificada

Cheryl Nelson

Cheryl Nelson es una galardonada meteoróloga de broadcast, nominada a los premios Emmy, presentadora de televisión, instructora certificada por la FEMA y asesora meteorológica y de preparación para Cummins. Puede visitar el sitio web de Cheryl en www.PrepareWithCher.com y síguela en Twitter y Facebook @CherylNelsonTV.

Cummins Marine impulsa a los aventureros alrededor del gran circuito

Bill y Amy Denison
Bill and Amy Denison complete the 6,500-mile journey around the Great Loop

Muchos marineros tienen el gran lazo en su lista de cubos pero solo unos pocos son lo suficientemente afortunados como para cumplir con la tarea. Bill y Amy Denison son uno de esos pocos. With great pride, they were able to complete the 6,500-mile journey down the east coast, up the inland rivers and back across the great lakes.

Su viaje comenzó en las aguas de Maine y Nueva Escocia. Bill y Amy navegaron a lo largo de la costa y visitaron islas remotas en su barco, mar-Kat-a Back Cove 41 con el nombre de sus hijas, Margaret y Kathleen. Decidieron que querían aventurarse más y se unieron a la Asociación Americana de cruceros de gran lazo (AGLCA).

Luego de seis meses de investigación y planificación, la pareja se despidió de sus amigos y familiares para emprender su viaje para hacer frente al gran lazo. Saliendo el 15 de junio de 2018, desde Albemarle Sound en Carolina del norte, se dirigieron al sur. Mar-Kat impulsado por un motor de diésel marino Cummins de 710 caballos de fuerza y un generador marino Cummins Onan de 9 kW.Embarcación con motor marino Cummins

Durante el transcurso de su viaje, Bill y Amy viajaron a través de 13 Estados y la provincia de Ontario, pasando por 100 cerraduras y acumulando casi 500 horas en su bote. Al completar el bucle en sentido contrario a las agujas del reloj, pudieron aprovechar las veloces corrientes fluviales.

Bill dijo: "el motor Cummins QSM11 funcionó sin problemas durante todo el viaje y solo requirió algunos cambios de aceite". Cuando se requería mantenimiento del servicio, la pareja se puso en contacto con su distribuidor local y "recibió un buen respaldo del equipo de Cummins Virginia".

Con elementos de diseño exclusivos para trabajo pesado, los pequeños motores de diésel de Cummins tienen una vida útil extendida del motor y ofrecen una aceleración y un desempeño de torsión comprobados. Cientos de fabricantes confían en este motor marino confiable de cuatro válvulas por cilindro, que se puede encontrar en las salas de motores de embarcaciones de recreo en todo el mundo. Además, con más de 8, 000 distribuidores y distribuidores, el producto Cummins le brinda a los clientes la tranquilidad que necesitan, sin importar dónde los lleve su viaje.

Luego de completar exitosamente el Great Loop en 10 meses, Bill y Amy ahora están planeando su próxima aventura con mar-Kat, tal vez explorando Florida o el sur de las Bahamas. Independientemente de dónde se dirigen a continuación, Cummins proporcionará la energía, la innovación y la confiabilidad para impulsar su viaje.

Descubra la gama Cummins Marine en cummins.com/marine , para ver cómo nuestros motores y generadores pueden alimentar sus viajes, en el mar o por tierra.

¿Necesita ayuda para elegir la solución adecuada para su embarcación? Busque su representante de Cummins local

Edificio de oficinas de Cummins

Cummins Inc.

Cummins es un líder mundial en energía que diseña, fabrica, vende y ofrece servicios de diésel y motores de combustible alternativo de 2,8 a 95 litros, diésel y grupos electrógenos eléctricos con combustibles alternativos de 2,5 a 3, 500 kW, además de componentes y tecnología relacionados. Cummins atiende a sus clientes a través de su red de 600 instalaciones de distribuidores independientes y propiedad de la compañía y más de 7, 200 centros de distribuidores en más de 190 países y territorios.

La emblemática microred de energía renovable híbrida de Australia se complementa con la generación de energía térmica de la generación de energía de Cummins

Las unidades de generador de gas y diésel QSK60 de Cummins QSV91G respaldan la microred de energía renovable de la mina de oro Agnew.
Las unidades de generador de gas y diésel QSK60 de Cummins QSV91G respaldan la microred de energía renovable de la mina de oro Agnew.

Con una capacidad instalada de 56MW, la central de energía renovable de Agnew se convirtió en la microred de energía renovable híbrida más grande de Australia, y la primera en utilizar generación de viento en una mina. La energía producida equivale a alimentar 11, 500 hogares y solo abusará de las 46, 400 toneladas de dióxido de carbono en el primer año.

Agnew híbrido Renewable Power Station, AustraliaCon una capacidad instalada de 56MW, la central de energía renovable de Agnew se convirtió en la microred de energía renovable híbrida más grande de Australia, y la primera en utilizar generación de viento en una mina. La energía producida equivale a alimentar 11, 500 hogares y solo abusará de las 46, 400 toneladas de dióxido de carbono en el primer año.

"Las tecnologías de energía renovable de la estación de energía renovable híbrida Agnew de EDL se complementan con la generación térmica de los generadores de diésel y gas de Cummins", dijo Jason Dickfos, jefe de crecimiento de EDL. "Estamos encantados de trabajar con Cummins para ofrecer este proyecto emblemático, el cual proporcionará a la mina de oro Agnew con más de un 50% de energía renovable a largo plazo, sin comprometer la calidad ni la confiabilidad de la energía."

La solución de energía renovable híbrida en la mina Gold Fields en Australia occidental consiste en una nueva estación de energía de 23MW fuera de la red que incorpora gas, energía solar fotovoltaica y generación de potencia diésel, seguida de la generación eólica de 18 MW, una batería de 13MW y un sistema de control de microred avanzado. Un requisito crucial era que los generadores tuvieran que suministrar energía continua y confiable a temperaturas de hasta 45 ° c. El modelo de generador de gas Cummins QSV91G fue seleccionado debido a su capacidad para operar en condiciones ambientales altas, además de proporcionar cargas de paso de alto impacto y velocidades de rampa rápidas a la vez que mantiene la calidad de energía, mientras que las unidades de diésel QSK60 de Cummins brindan energía adicional durante los períodos de máxima demanda y tienen capacidades de arranque en negro en caso de un corte de energía.

Lea más acerca de la Agnew energía en este de estudio de casos .

Angela Papageorgiou

Angela Papageorgiou es la especialista Senior en comunicaciones de marketing para el segmento de gestión de energía de Cummins Inc. antes de incorporarse a Cummins en 2014, Angela trabajó en agencias de comunicaciones de comercialización apoyando el desarrollo y la ejecución de proyectos de campaña B2C y B2B. [email protegido]

Energy IQ: tres situaciones que maximizan las ventajas de las aplicaciones de cogeneración

Tres situaciones que maximizan las ventajas de las aplicaciones de cogeneración
Tres situaciones que maximizan las ventajas de las aplicaciones de cogeneración

Los invernaderos, los hospitales, los fabricantes industriales y los propietarios de edificios comerciales son algunos de los muchos que recurren a la cogeneración, también conocida como combinación de calor y energía (CHP). Gozan de beneficios que van desde un mejor desempeño financiero hasta una menor huella ambiental. La gran eficiencia de las aplicaciones de cogeneración en convertir la energía en el combustible original en energía útil es la base de estas ventajas.

Estos beneficios de las aplicaciones de cogeneración se amplifican en ciertas situaciones. Vamos a cubrir estas situaciones y ejemplos asociados de aplicaciones de cogeneración.

Núm. 1: ciertos aspectos de su negocio operan 24/7

Los sistemas de cogeneración más rentables funcionan a la potencia total 24/7.

Esto no significa que todo su negocio necesite ejecutar 24/7. En cambio, puede identificar aspectos de su negocio que ejecuten 24/7 y suministrar energía a estos con un sistema de cogeneración. Mientras tanto, aún puede tener la conexión de servicio público y las calderas en el lugar. Estos son útiles para impulsar el resto de sus operaciones comerciales y para administrar picos potenciales en la demanda de energía eléctrica o térmica. Otra ventaja de usar una combinación de cogeneración y energía de servicio público es alrededor de los eventos de mantenimiento. Esta combinación le permite llevar a cabo mantenimiento y servicio en su sistema de cogeneración sin interrumpir el acceso a la electricidad para su negocio.

Los hospitales son un buen ejemplo de las aplicaciones de cogeneración para este escenario. Controlar la temperatura, controlar la calidad del aire, mantener el funcionamiento del equipo médico y muchas otras actividades requieren electricidad y energía térmica durante todo el día.

Núm. 2: la necesidad de energía térmica es consistente; también es simultáneo con la necesidad de electricidad varios meses del año

Muchas instalaciones aprovechan las aplicaciones de cogeneración con mayor popularidad a lo largo de los años
Muchas instalaciones aprovechan las aplicaciones de cogeneración con mayor popularidad a lo largo de los años

Vender o almacenar exceso de energía térmica a menudo no es práctico. El calor excesivo se libera comúnmente como calor residual, lo que disminuye la eficiencia general y las ganancias financieras de la aplicación de cogeneración. La eficiencia de un sistema de cogeneración aumenta cuando las necesidades térmicas (vapor, agua caliente o agua refrigerada) permanecen en un nivel consistente. Lo mismo no se aplica tanto a las necesidades de electricidad, ya que el exceso de electricidad a menudo podría ser vendido de vuelta a la compañía eléctrica.

Cuanto más larga sea la necesidad simultánea de electricidad y energía térmica, más ventajosa es una aplicación de cogeneración. De hecho, una buena guía es considerar las aplicaciones de cogeneración si su negocio tiene necesidades simultáneas de electricidad y calefacción/enfriamiento alrededor de la mitad del año o más 1 . Hay excepciones a esto, y algunas aplicaciones son factibles incluso cuando la necesidad simultánea es de 2, 000 horas al año, unos tres meses.

La fabricación industrial es un buen ejemplo de una aplicación de cogeneración para este escenario. La energía térmica necesaria en el procesamiento industrial tiende a ser consistente durante todo el funcionamiento de la instalación. Además, la energía térmica y la electricidad suelen ser necesarias simultáneamente durante todo el año en estas instalaciones.

Núm. 3: los precios de la electricidad son altos en comparación con el costo del gas natural

Usted está financieramente mejor si la producción de electricidad en el lugar es más barata que la compra de electricidad de la compañía de servicios públicos. Muchos sistemas de cogeneración que producen electricidad en el lugar usan gas natural como combustible, y aquí es donde entra en juego la propagación de la chispa.

La propagación de la chispa es una métrica para estimar la rentabilidad de los generadores eléctricos a gas natural. Es la diferencia entre el precio de la electricidad y el costo del gas natural necesario para producir esa electricidad 2 . A medida que aumenta la propagación de la chispa, también aumenta el ahorro que ofrece un sistema de cogeneración. La propagación de la chispa es un indicador de la viabilidad financiera, pero no es una medida exacta de la rentabilidad.

Los centros donde el costo de la electricidad es alto y el gas natural como combustible está disponible son buenos ejemplos de las aplicaciones de cogeneración para este escenario.

Más allá de los factores anteriores, el que evalúa la cogeneración para su instalación el informe describe otros aspectos a considerar a medida que explora la cogeneración como una opción.

Suscríbase a continuación para obtener información centrada en la energía en mercados que abarcan desde centros de datos e instalaciones de atención médica hasta instalaciones de fabricación y todo lo demás. Para obtener más información sobre las ofertas de cogeneración y trigeneration Power Solutions de Cummins Inc., visite nuestra página web .

¿Cree que a sus amigos y colegas les gustaría este contenido? Compartir en LinkedIn y Facebook.

Referencias:
1 Hamilton, J. (n.d.). Evaluar la cogeneración para su instalación [Boletín]. Cummins Inc. se recuperó de https://www.cummins.com
2 Oficina de administración de energía de EE. UU. (2013 de febrero). Una introducción a los diferenciales de chispa. Obtenido de https://www.eia.gov/
 

Aumente su coeficiente de energía

Crezca profesionalmente con las tendencias energéticas y las estadísticas que se le proporcionan a su bandeja de entrada. Lea acerca de las tendencias y tecnologías energéticas en nuestro Energy IQ Hub .

Aytek Yuksel-Cummins Inc

Aytek Yuksel

Aytek Yuksel es el líder en marketing de contenidos para Cummins Inc., con un enfoque en los mercados de sistemas de energía. Aytek se unió a la compañía en 2008. Desde entonces, ha trabajado en varios puestos de marketing y ahora le ofrece los aprendizajes de nuestros mercados clave, que van desde los mercados industriales hasta los residenciales. Aytek vive en Minneapolis, Minnesota con su esposa y sus dos hijos.

Redirigiendo a
cummins.com

La información que busca está en
cummins.com

Ahora estamos iniciando ese sitio para usted.

Gracias.