Filtration in DEF Manufacturing and Delivery

The particles and contaminants that we are trying to filter out are far smaller than can be seen with the naked eye, magnifying glass or even a low powered telescope.

What is a Micron?

The unwanted particles found in today’s DEF are measured in microns (μ). A micron is a unit of linear measure in the metric system used to measure distance from one point to another. A micron rating for DEF filtration is a generalized way of quantifying the ability of a filter’s media to remove contaminants of a particular size.

For example, a filter with a micron rating of “7” will filter out contaminants of 7 microns or larger and a filter with a micron rating of “3” will filter out contaminants of 3 microns or larger. Filter efficiency refers to a measurement of the filter’s retention efficiency. The measurement is typically the number of particles retained by a filter compared to the number of particles present in the DEF that will pass through the filter. A 7 micron filter with 98.7% efficiency rating removes 98.7% of the particles at or above the 7 micron size.

Proper Storage and Filtration of DEF is Critical

As the graphic below illustrates, the wide variance in filtration throughout the manufacturing and delivery process of DEF makes awareness of proper storage and filtration an essential part of your Selective Catalytic Reduction (SCR) aftertreatment system’s reliability and performance.

def process illustration

Case Study Actions

Goldacres Sprayers - Cummins Powered Since 1999

View

Cummins Powers Global Growth in Almond Production

View

Cummins Tier 4 Final power for the Apache sprayer range

View

Cummins helps build the Australian cotton industry

View

Cummins power units are the pick of the crop

View

Cutting edge efficiency

View

Cummins Performance Series Enables Engine Downsizing for Bandit Industries Whole Tree Chipper

View

Cummins steps in to provide power and reliability for Kubota's biggest tractor ever

View

Increase fuel efficiency and save money: a farmer’s guide

View

Cummins powers GUSS - the world's first autonomous orchard sprayer

View


To view all case studies, click here.
Redirecting to
cummins.com

The information you are looking for is on
cummins.com

We are launching that site for you now.

Thank you.