Russia Generator Projects

Cummins Inc. - A partner you can trust to deliver.

Cummins generator project Russia

Whatever your plans or challenges in gas fueled power, it pays to choose an expert partner you can trust to deliver. Whether it’s solving a specific problem, delivering a turnkey solution or providing support, Cummins Power Generation Energy Solutions Business (ESB) has the total capability you need, whatever your application, wherever you are in the world.

When you work with Cummins ESB you get one company with vast experience and resources behind you, delivering the skills and services you need expertly, efficiently and reliably. We work in partnership with you, utilizing Cummins Power Generation gas and diesel fueled technology and providing a complete range of services, whether it’s for a peaking or standby power site or a cogeneration or waste-to-energy project. Complex problems call for specialist, customized solutions. Challenging environments require robust technologies. Demanding schedules need committed teams. With Cummins ESB, you get them all and more through one global project partner. We shape our services around your goals. Our expert teams can provide everything from turnkey solutions to rental packages to fit your plans and business.

Flexible solutions

Whether you’re planning to self-generate your power on single or multiple sites or want to supply power to other users, you can call on Cummins ESB to help. Our services encompass turnkey solutions to give you an entire on-site power plant from scratch. Plus, we can offer rental solution, supplying power for sale to other customers. Whichever way you want your power, we have the experience and resources to make it happen.

Working as partners

Whatever the project, we work in partnership with you. We start by listening to your needs and forming a clear understanding of your objectives, before delivering fresh insights and identifying the most effective route forward for your business. We then get to work, bringing together our teams and specialist providers when required and providing a tailored solution through a single point of contact, and one centrally managed resource. And throughout, we think and act like an extension of your business, treating your goals as our own.

Skilled and dedicated people

When you work with Cummins Power Generation, you get a unique advantage: the skills and dedication of Cummins people. No matter what the challenge, our experienced project managers and skilled technicians will bring your plans to fruition, whether it’s designing a customized power system, installing equipment or delivering expert O&M support. Part of one of the biggest power generation teams in the world, they’re committed to providing the personal consultation and top-flight expertise you expect from an industry leader.


Gas Projects

Zvezda-Energetika project

Bovanenkovo-Ukhta gas pipeline
Customer: GAZPROM

Project: Delivery of 9 power stations on the basis of Cummins QSK60/QSV91 gas powered electrical generators with the total capacity of 93 MW for compressor stations of Bovanenkovo-Ukhta gas pipeline, part of North-stream pipeline infrastructural project. Gas engine power plants satisfy all power requirements of compressor stations. Each power plant consists of 5-7 Cummins QSK60/QSV91 gas engine units rated at 1,1-1,5 MW each and stand-by Cummins diesel power plants with the capacity of 0.6-1 MW each.

NG-Energo project

Western Sakhalin field
Customer: JSC Surgutneftegaz

Project: “Energo-P6160/6.3KN30” gas engine generator plant on the basis of Cummins QSV91G gas powered electrical generators with overall capacity of 6.16 MW, generator voltage – 6.3 kV. The power station is intended for power supply of oil production and associated petroleum gas disposal on the oil field. In order to ensure operation of gas powered electrical generators the site was equipped with a system of fuel gas preparation which provides elimination of additives, moisture, drops of liquid from the associated gas and ensure maintenance of necessary pressure and temperature. Mode of operation – continuous, in parallel with the power system or independent in case of emergencies in the power system.

OOO “Cummins” project

BELAZ production facility cogeneration power supply
Customer: ОАО «BELAZ»

Project: Delivery of 3 power stations on the basis of Cummins QSK60 gas powered electrical generators with the total capacity of 3.3 MW for heat and power supply of production line of BELAZ, largest HHP mining dump trucks manufacturer in CIS, based in Zhodino, Belarus. Provided solution is more cost effective both in terms of heat and power generation and allows to significantly reduce relevant costs of production. Power plant consists of 3 Cummins QSK60 gas engine units rated at 1,1 MW each.

OOO “Cummins” project

Prime power supply for Siboil company oil field
Customer: Siboil company

Project: Delivery of 8 gas generating sets on the basis of Cummins QSV91 gas engines with the total capacity of 12,3MW for autonomous energy and heat supply on flare gas fuel. This project included existing generating sets overhaul and renovation, including containerization. Equipment provides steady and reliable energy supply in remote oil field with harsh weather conditions and absence of central power supply.


Diesel Projects

NG Energo project

Customer: Gazpromburenie LLC

Project: Delivery of 44 diesel power stations 1 MW each and 11 ones 320 kW each. Power stations together with 6.3 kV switchgear and operator room are manufactured according to the project that was developed by JSC NG-Energo and operate as part of new “Catherine” boring installations (manufactured by “Uralmashboring equipment”). Power stations are operated on oil fields in Orenburg region and on the territory of Yamalo-Nenetsky Autonomous District. Service maintenance is performed by Service department specialists.

Zvezda Energetika project

Customer: SP Sakhalin Energy

Project: One of the biggest projects of “Zvezda-Energetika” is the power station in Prigorodnoe village at Sakhalin, that was a turn-key construction in 2004 for Sakhalin-2 project for ZAO IC “Transstroy”. The power station consists of 12 containerized C2250D5 diesel gensets 1600kW each , an 8 MW boiler station, HV switchgear, Automatic Control System, Fuel Storage, Administrative Building. Possible seismic intensity up to grade 9 was considered during constructional design. The power station is under supervision of “Zvezda- Energetika” technical specialist with a constant presence at the site.

Redirecting to
cummins.com

The information you are looking for is on
cummins.com

We are launching that site for you now.

Thank you.