CUMMINS BRINGS EURO 6 SMART EFFICIENCY TO FIAA SHOW
At the FIAA show, Cummins Europe will display the latest generation of Smart Efficiency B4.5 and B6.7 bus engines with a 112 kW to 224 kW (150-300 hp) ratings range to meet Euro 6 Phase-C regulations which took effect on January 1, 2017. This latest evolution of the B Series carries forward the best-in-class attributes of the current engines, but now with 10 percent higher peak torque, extended service intervals and a unique, fully integrated Stop-Start option capable of delivering fuel savings of up to 8 percent. The B Series will be joined by the L9 bus engine on the Cummins display at FIAA, taking the power range up to 276 kW (370 hp).
Madrid, Spain