Cummins Case Studies

We’re in it for the long haul. We build lasting partnerships that lead to smarter innovations for our customers. These customer stories demonstrate our commitment and success in providing customers like you with improved power solutions through world-class innovation in a number of industries.

Filter Case Studies

Located on Valentia Island, in County Kerry, near the extreme southwest corner of Ireland, Murphy Marine, builds boats designed and proven on the extrema Atlantic waters. The well-known yard builds  a range of boats from 24 to 44 feet. While the hull designs are proven and set, the upper portions of the vessel include a variety of different configurations. The Cygnus Cyclone 30 with its co

“We got 59,115 hours on those engines, without ever removing a head,” marvels Seaspan International’s Port Engineer Kevin Tweedy, “and they were still running so, at 5,000 to 5,500 hours per year, we could easily have done 60,000 hours.” But the company schedule worked to do a like-for-like repower. The pair of 850-hp, tier 1, Cummins KTA38 diesels were pulled out and a brand-new set of 850 hp, ti

For nearly a century, the rugged coast and islands of Scotland were served by the handy little steam freight boats known as Puffers. They carried manufactured goods out to villages and farm produce back to the mainland. The recent delivery of the 27-by-9.7-meter Havara shows just how dramatically small coasters have developed over the past two generations. In fact, apart from that their role as a

Since the days of wooden hulls and human power, lifeboat crews have put to sea through dangerous surf to save the lives of their fellow seamen. The first engine-powered boats allowed decks and cabins that afforded a greater level of safety. When the US Coast Guard developed their 47-foot surf boat in the late 1990s, it set a whole new standard for lifeboats. Designated 47-foot MLBs, these all

Ocean science is in high demand by scientists studying ocean acidification, wave energy, seabed composition, changing water temperatures, fish populations and dozens of other research projects. The Oregon State University (OSU) has a proud history in the field. The wide variety of research project require a variety of vessels. One boat that has made large contributions to research is the 54

Successful fishermen have long demonstrated a respect for tradition and a willingness to test new water and new technologies. Mr. Richard Hards and Mr. George Jacks, of Pecheurs Eccosse Limited in Inverness, Scotland, demonstrate that balance with their new catamaran vessel, the Sharon Anne. With a 5.5-meter beam, the 11.95-meter catamaran has more fishing power than its length would suggest. I

Calling all farmers! We know that efficiencies help keep your business successful, so we’ve developed ten tips to help increase your fuel economy and save money.  Watch the video to find out more about how our top tips can help ensure you’re getting the most out of your engine, while minimizing operational costs. Cummins Performance Series is our most powerful and productive agriculture

Joey Rodriguez has seen the ups and downs of the boat building business at his Rodriguez Shipbuilding in Coden Alabama. For a time, there was huge demand for big steel Gulf Shrimp boats and then the oil industry ramped up and kept him busy with a variety of tugboats. Then came the crash in oil prices and the crash in demand for towboats. Joey shuttered his yard for a year and a half. “I didn’t

Founded in 1958 as an extension of the Stradiotti family businesses, North Arm Transportation has grown to be a significant fuel company on the BC coast. Over the years, the company fleet has expanded and evolved. With tugs in a range of size and power, as well as cargo and fuel barges, the company services the coast out of its headquarters in Vancouver on the North Arm of the Fraser River. They a

Bunkering ports around the world have long used a variety of small tankers or tug and barge combinations to deliver fuel to visiting ships. Mostly this was heavy oil, but recently a new breed of bunkering vessels is emerging to deliver clean burning LNG to modern ships with dual-fuel capabilities. The fall of 2020 will see a fine new addition to this fleet servicing cruise ships in Florida and

It has been said that if you want a versatile, practical, and safe boat, go to an islander. With multiple generations on the Isle of Škoj in the Adriatic off the Croatian city of Split, Luka, the youngest of the Colnago family, is a noted designer and builder. His latest work, the Colnago 45 Pilot, is one of his most versatile yet. A lot of Luka’s boats are high-end, high-speed, pleasure and to

Like many fishermen, Justin Yager is interested in the responsible harvesting or marine resources. “We don’t need to be fishing the crabs right up into their molt stages,” he said recently. Similarly, he saw the common sense of rebuilding the Gulf Shrimper B.J. Thomas when the boat had a serious fire at Newport, Oregon. Built in 1976 at Marine Builders in Mobile, Alabama the boat found its way

Overview Challenge: Red Cross Hospital in Cordoba, Spain needed to replace an older outdated backup genset with a new genset that provided 220 kva. In addition, the removal of the old genset and installation of the new backup genset needed to take place within a 24-hour period without leaving the hospital at risk during an outage. Solution: The

In 2020, Kubota unveiled its largest tractor to date – the 19,510 lb. / 8550 kg M8. Its big features – power, reliability, comfort and value. Power comes in the form of a 180 hp (134 kW) or 200 hp (149kW) Cummins B6.7 Performance Series engine. As Cummins’ most popular product, with over 15 million B Series engines built since its introduction, the B6.7 represents next generation engine technol

Overview Challenge: Provide cogeneration solution to Varegro, a horticultural company in Ootrozebeke, West Flanders. Solution: Install Cummins C2000N5CD 2MW HSK78G gas generator to provide additional power along-side vast cost and energy savings. Result: A range of energy needs were met in addition to converting remaining waste

Overview Challenge: Supply Belgian tomato grower Desmet with combined heat and power system delivering on agreed level of electrical and thermal energy. Solution: Design, build and provide Desmet with an energy service contract. Result: Reduced heating costs and emissions without increasing cash-flow and incurring the costs of i

With a beautiful design, the Back Cove 37 is long-range cruiser for extended voyages that's also great for day-tripping with friends, representing excellent value and fuel economy for every boating lifestyle. By Lisa Overing Photos by Billy Black   If you’ve ever dreamed of crossing an ocean, your quest for exploration is strong. The Back Cove 37, a usable cruising boat with a midle