Cummins Case Studies

We’re in it for the long haul. We build lasting partnerships that lead to smarter innovations for our customers. These customer stories demonstrate our commitment and success in providing customers like you with improved power solutions through world-class innovation in a number of industries.

Filter Case Studies

“Builders choose Onan generators because of the ease of using Onan, and it is backed by Cummins, so the supply chain should be better, too." Fishermen appreciate quiet Onan gensets Custom-built pleasure crafts represent the ultimate vessel in luxury design, naval architecture and craftsmanship. As the epitome and vision of a discriminating, private yacht owner, one-off dreamboats demand pr

Challenge:  Digea required standby power for more than 45 digital television broadcast sites around the country, which was essential to keep the sheltered equipment running, and transmissions on-air, in the event of a grid failure. Solution: Cummins distributor Ergotrak supplied back-up systems for the 45 plus sites, deploying three types of Cummins g

"The Cummins KTA19s provide the perfect amount of power to do our job." — Brennan Templet, mate and pilot of Richard B Scream all you want in the swamp, no one will ever hear you - or help you. Down on the bayou, autonomy and self-preservation is key, because in a remote area, you’re on your own, in the elements. Having an engine like the Cummins KTA19 with torque, power and maneuverabi

Challenge:  To install a reliable critical protection power system for Digital Realty to meet stringent Tier 3 certification requirements, as defined by Uptime Institute. Solution: Cummins Power Generation delivered six roof mounted C2250D5 diesel generator sets powered by QSK60-G4 engines, together with custom-built acoustic enclosures and fuel syste

Challenge:  To install a reliable standby power system for the LG CNS Busan Global Data Center, ensuring service continuity and preventing data loss in the event of a power failure. Solution: Cummins delivered a comprehensive power system comprising 12 units of C2250D6A diesel generator sets to provide a total of 27MW of standby power. Res

Challenge:  Cummins was entrusted to supply the Twin Arrows Navajo Casino Resort in a rural location with emergency standby power. The critical need for standby as a gaming operation is so the resort wouldn’t lose power to the gaming floor or the gaming slot systems to maintain play on the floor. Cummins Power Generation was selected to supply diesel generators for critic

Challenge:  Design a backup power system tailored to meet NEXTDC’s criticality level requirements and install it in an unconventional environment, but also meet the customer’s rapid time to market demand without comprising the integrity of the work and equipment. Solution: 5.4 MW of standby power comprising of three C2250 QSK60 Generator Sets of CPG g

Challenge:  To reduce reliance on National Grid by upgrading the university’s 32 years old cogeneration solution. Using technology that complies with environmental regulations and can run continuously on a 24/7 basis, while being able to fit into a limited allocated space. Solution: A new cogeneration solution with Cummins C2000N6C, QSV91G singe turbo

Cummins power solution for KBC Bank   Challenge:  KBC Bank and its Hungarian subsidiary K&H selected Cummins for standby power at two of the bank’s mirrored data center sites in Hungary. Solution: Each of the mirrored sites were equipped with two C3000 D5 generator sets per site, both with QSK78 engines and PCC 3.3 controls.

Cummins Data Center Continuous Solution is Top Choice for Turkcell   Challenge:  To become the main provider of continuous power to Turkcell’s Datacenter. Solution: Cummins installed ten C1675 D5A generator sets plus two C1100 D5B units and a single C700 D5 in the basement of a three-story building.  Cummins also won a contract to supp

Challenge:  CalBank, one of Ghana’s leading banks, needed a standby power solution for its Head Office in Accra. Cummins Ghana were tasked with providing a standby power system that the head office buildings, including a banking hall and data center, could rely on to provide uninterrupted, efficient service and solutions to its customers, even during power outages.

"Up here, near Cape Cod, there’s a lot of support [from Cummins]. The Dunham dealership is open all the time. I also have Cummins X15’s in all my work and pickup trucks for my excavation company." — Capt. Anthony Belculfine  Smart diesel QSC8.3 600 gets out in front of the fleet The shocking combination of horsepower with efficiency is just one benefit of finding the perfect boat and

Overview Challenge: Provide power systems technologies for a completely off-grid microgrid solution that has the capacity to provide continuous reliable power in high ambient conditions, for a gold mining company.  Solution: A hybrid renewable energy solution with nine C2000N5CB QSV91G gas generator sets, two C2250D5 QSK60 diesel generator

What: Four 1250 kW at 13.8kV AC generator sets with on-board autonomous microprocessor-based PowerCommand® Control for paralleling and protection. The PowerCommand® DMC 8000 which is a state-of-the-art system level control. Arc-Resistance switchgear rated at 15kV, and the PowerCommand Cloud™ for real-time monitoring. The system runs in an extended parallel operation with the utilit

Liveaboard, Spanish-inspired llaut loaded with style, creature comforts Wrapped in luxury amid the waves gently lapping the hull of the Menorquin 68 is a sensual experience at sea. Three lovely staterooms with four berths encourage sleeping in just a little bit longer. Upon awakening, stepping up the companionway into the well-appointed salon's open entryway brings the sunlight in with the sea

“The whisper-quiet genset, proven reliability, ease of maintenance and longevity are prime reasons why Nordhavn’s long range vessels are built standard with Onan marine generators.” - Jim Leishman, Vice President & Co-owner, Nordhavn Yachts Nordhavn 41 fuel-miser boasts a small carbon footprint The Nordhavn 40 set the world record for a production boat under 70 feet, circumnaviga

“Loaded with creature comforts, the audio in an Azimut is like a night club with an amazing sound system.” - Peter Kurki, Sales Executive, Allied Marine   Semi-displacement hull for smooth sailing in Azimut style Azimut, the world’s leading builder of seductive, fast-planing flybridge yachts, now builds vessels for long-range cruising. The 43 navetta-style yacht is the fourth m

As progressive nations worldwide commit to reducing greenhouse gases, a fishing vessel is built to do its share with Cummins marine propulsion. Designed by Norway’s Skipsteknisk and Selvåg AS, the Selvåg Senior is under construction at Cemre Shipyard for Sorheim Holding and is truly a remarkable concept. Capable of both trawling and purse seining, the 79.5 by 16.2-meter vessel with have a molde