""
Marine

Guangzhou Hangtong Shipbuilding: Accommodation & Construction Boat

by Alan Haig-Brown

Cummins Vessel Reference #763

One of the two accommodation boats built at Guangzhou Mangtong Shipbuilding.photo: courtesy of Guangzhou Mangtong Shipbuilding.

In recent years, a number of shipyards in southern China have grown, not only in size, but also in the sophistication of the vessels that they are building. At the Guangzhou Hangtong Shipbuilding this is well illustrated by the 83.6 by 22-meter construction and accommodation design that they are building. With one of these big boats already delivered to a contract in Mexico, they were, in mid-March, putting the finishing touches on a sister ship.

Fifi pump mounted to front of Cummins QSK60-M.photo Haig-Brown/Cummins

Fitted with a four way mooring system, a hefty deck crane, a large clear after deck and a variety of other attributes, the vessel is well outfitted for marine construction work. The large exhaust stack for all engines, main and auxiliary, is mounted on the port side to allow for ease of crane work over the starboard side. This also allows space on the starboard side for a Zhejiang Hengxin Ship Equipment (HXN) rescue boat and davit. A pair of large HXN enclosed lifeboats are also mounted port and starboard.

 

The bridge on the 83 by 22-meter accommodation ship.photo Haig-Brown/Cummins

The multi-decked superstructure is located well forward and provides accommodation in a variety of rooms for up to 200 people. A mess hall and galley suitable for this number is also located in the deckhouse.

The aft controls with a clear view over the working deck.photo Haig-Brown/Cummins

The bridge is outfitted with all the latest in controls to provide operational status on the two Cummins QSK60-M main engines as well as the three Cummins KTA38-DM-powered electrical generators. The wheelhouse also has an extensive suite of navigational instruments. In addition to the forward console, an aft set of controls allows for safe use of the cranes and other construction utilities while giving the operator a clear view of the after working deck.

 

A galley large enough to cook for 200 people. photo Haig-Brown/Cummins

The large engine room space is located midships in the 7.2-meter deep hull. The three Cummins-powered 590 kW generator sets provide for the extensive electrical needs of the accommodation block as well as the deck cranes, bow thrusters and active stabalizers designed for the comfort of personnel. The twin Cummins QSK60-M main engines each produce 2200 horsepower at 1800 RPM and turn fixed-pitch propellers through Twin Disc MGX5600 gears with 5.76:1 reduction. One of the two main engines has a fire pump linked to the front of the engine with a power take-off.

 

Chairs in the mess area are attached by chain to the deck. photo Haig-Brown/Cummins
 
Massive positioning anchors rest on the stern deck. photo Haig-Brown/Cummins

For further information:


Qin Juan
Purchasing Dept. Manager
Guangzhou Mangtong Shipbuilding and Shipping Co. Ltd.
16 Zhenxing Street, Haizhu District
Guangzhou, 510290, China
Moblie: 86 18998 155437
E-mail: [email protected]

Linda Zhang
Manager: Southern China
Cummins Inc., East Asia Marine
Phone: 86 20 3998 2999
Mobile: 86 136 0004 0695
E-mail: [email protected]

Weney Lee ???
Customer Support
Cummins Dealer
Yinpeng Group
No.5, Yihengxi Road,
Dongsha, Panyu,
Guangzhou,
Guangdong China
Phone: 86 20 84872872
Mobile:
1371 940 5000
URL: www.yinpeng.com
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...