Wiederverwendung von Methan aus Mülldeponien für eine nachhaltigere Entsorgung

""

Es ist kein Geheimnis, dass lkw-Märkte auf der ganzen Welt sauberere Kraftstoffalternativen fordern. In 2018, the United States Environmental Protection Agency (EPA) launched the Clean Trucking Initiative to "ensure emissions reductions occur in the real world in all types of truck operation."

With a specific reference to heavy-duty trucks and their impact on the environment, the refuse market has a unique opportunity to increase their use of renewable resources. How? By capturing and reusing landfill gases.

Landfills are an extreme threat to the ozone and are responsible for emitting raw methane gases. Raw methane gas is 40 times more potent than tail pipe exhaust and will remain trapped in the atmosphere for hundreds of years. But on the flip side, methane emissions from landfills also represent an undervalued opportunity to seize and repurpose a significant energy resource.

Once methane is produced, it can go through three different levels of treatments in order to repurpose the gas in a productive manner. The primary and secondary treatments remove moisture and impurities, respectively. If these two steps are completed, the gas can be used to generate electricity in power generation plants. If the methane undergoes a third treatment to remove CO2, N2, O2, and VOCs (as needed), it can be reused for vehicle fuel as renewable natural gas (RNG).

Renewable Natural Gas landfill process

This process creates the opportunity for a full life cycle of natural gas landfills. Waste companies, like Waste Management, are sending RNG-powered trucks to your neighborhood to collect waste and recycling. The material collected is then deposited into landfills and over time produces methane. That methane becomes a RNG through the cleansing process and then fuel to power the natural gas powered trucks that collect the waste. Cummins’ natural gas engine line already produces emissions 90% lower than EPA requirements; adding this fuel type further reduces Waste Management’s vehicles to net sub-zero emissions! 

On a larger scale, there are also opportunities for waste companies to funnel their RNG from landfills into the national natural gas pipeline network. The U.S. natural gas pipeline system totals over three million miles of pipeline across the country, providing natural gas to factories, hotels, city-owned facilities, convention sites, airports, commercial ship and motorized vehicle refueling sites, and finally into residential homes across the country.

While both RNG and fossil natural gas share the same pipeline, the year-over-year expansion of injecting RNG into the pipeline will continue to reduce our dependence on fossil fuels. To further encourage the growth and use of RNG in the United States, the EPA established the Renewable Identification Number program (or RIN). Fleets who contract the purchases and use RNG from authorized brokers receive full Greenhouse Gas reduction credits when pulling natural gas off the pipeline.

It seems like a perfect solution. Is that because it is? Landfills, dairy farms, livestock farms and sewerage treatment plants all produce raw methane naturally. Capturing this abundant energy source and converting it to a very affordable energy source, then coupling it with Cummins' renewable natural gas engine delivers net sub-zero emissions goods movement today.

Next question, please. 

Learn more about Cummins natural gas solutions.  

Quellen
Environmental Protection Agency: https://www.epa.gov/lmop/basic-information-about-landfill-gas 

Tags:

Bleiben Sie immer auf dem neuesten Stand

Bleiben Sie mit den neuesten Technologien, Produkten, Branchentrends und Neuigkeiten auf dem Laufenden.

Senden Sie mir die neuesten Nachrichten in (alle zutreffenden Optionen auswählen):
Bürogebäude von Cummins

Cummins Inc.

Cummins, ein weltweit führendes Unternehmen in der Energietechnik, ist ein Konzern mit sich ergänzenden Geschäftsbereichen, die ein breites Portfolio an Stromversorgungslösungen entwickeln, herstellen, vertreiben und warten. Die Produkte des Unternehmens reichen von integrierten Verbrennungs-, Elektro- und Hybridantriebslösungen bis hin zu Komponenten wie Filtration, Abgasnachbehandlung, Turbolader, Kraftstoffsysteme, Steuerungssysteme, Luftaufbereitungssysteme, automatisierte Getriebe, Stromerzeugungssysteme, Microgrid-Steuerungen, Batterien, Elektrolyseure und Brennstoffzellenprodukte.

Einblicke in unsere neuesten Erdgasgeneratoren

Generator-Rendering

Cummins Inc. freut sich, unseren Kunden zwei neue Erdgasgeneratoren, den C175N6B und C200N6B, vorzustellen. Diese Ergänzungen verwenden die gleiche QSJ8.9G-Motorplattform wie die Erdgasgeneratoren C125N6 und C150N6, die bei verschiedenen industriellen Anwendungen beliebt sind. In Nordamerika hat der Markt für Erdgasgeneratoren in den letzten Jahren immer mehr zugenommen. Umweltauflagen und der Komfort des einfachen Nachfüllens von Kraftstoff sind einige der Gründe, warum Kunden Erdgasgeneratoren anderen Kraftstoffarten vorziehen.

Wir haben Vijay Jayaprakash, Cummins Product Manager für <1MW Gas Generator Sets & G-Drive, eingeladen, um seine Erfahrungen bei Cummins zu besprechen und die beiden neuen Produkte vorzustellen.
 

1. Was war Ihre Rolle bei der Entwicklung von C175N6B und C200N6B?

Als Produktmanager habe ich umfangreiche Forschungen darüber durchgeführt, was die Bedürfnisse von Kunden und der Branche sind und wie Cummins diese Anforderungen erfüllen kann, indem ich enge Beziehungen zu den Kunden und dem Vertriebsteam aufgebaut habe. Unser Team hat viel Zeit und Mühe in die Erforschung und Entwicklung der richtigen Generatoren investiert, um die Leistung unseres bewährten und auf dem Markt anerkannten QSJ8.9G-Motors zu steigern. Mit diesen beiden neuen Produkten reicht die Produktpalette der QSJ8.9G-Motorgeneratoren von 125 kW bis 200 kW.

Headshot

2. Wo sehen Sie die Verwendung dieser beiden neuen Produkte?

Ähnlich wie C125N6 und C150N6 werden C175N6B und C200N6B in Regierungsgebäuden, Wasserkläranlagen, Gesundheitseinrichtungen, Gewerbegebäuden, öffentlicher Infrastruktur und vielen mehr verwendet. Diese Produkte sind auch eine großartige Ergänzung für alle Bereiche, in denen eine Parallelschaltung von bereits bestehenden Stromsystemen erforderlich ist. Um mehr über Parallelisierung zu erfahren, klicken Sie hier.

Mit dem QSJ8.9G-Motor können C175N6B und C200N6B mit Erdgas betrieben werden, was sie für bevölkerungsreiche Gebiete und Städte besser geeignet macht. Weitere Informationen zu den Vorteilen von Erdgasgeneratoren finden Sie hier.

3. Was haben Sie bei der Arbeit an diesen neuen Produkten während der COVID-19-Pandemie in Ihrem Team gesehen, das dies möglich und erfolgreich gemacht hat?

Die Teamarbeit und das Engagement, das Produkt schneller auf den Markt zu bringen, haben dieses Projekt möglich gemacht. Obwohl es auf dem Weg dorthin einige Schwierigkeiten gab, bin ich wirklich dankbar, dass sich alle in den verschiedenen Teams im Werk, in der Technik, im Marketing und in vielen anderen Bereichen engagiert haben. Die Teammitglieder waren bereit, für Beta-Builds und Produkttests ins Büro/Werk zu kommen und flexibel zu arbeiten, um dieses Produkt erfolgreich für unsere Kunden zu liefern. Teamwork ist einer der Werte von Cummins, und unser Team hat darüber hinaus gezeigt, was Teamwork leisten kann. Immer aktiv.

4. Mit welchem Wort würden Sie die neuen 175 und 200 kW-Generatoranlagen beschreiben?

Leistung. C175N6B und C200N6B sind mit seinem 8,9-Liter-Motor die marktführenden Erdgasgeneratorprodukte in Bezug auf die Leistungsdichte. Bislang ist kein anderes Produkt in der Lage, diese Leistung auf kleinerem Raum zu erbringen, einschließlich des Schallpegels im 2 Gehäuse (73.6 (175kW) und 74.4 (200kW) dbA). Wir glauben, dass der C175N6B und der C200N6B den Markt verändern und unseren Kunden zuverlässige Energie liefern werden.


Cummins C175N6B und C200N6B verwenden einen 8,9-Liter-QSJ8.9G-Motor mit Erdgas als Kraftstoff. Mit diesen beiden Knotenpunkten bietet der QSJ8.9G die höchste Leistungsdichte unter den Erdgasgeneratoranlagenprodukten der Branche. Cummins setzt sich mit unserer führenden Technologie, unserem Fachwissen und unserem Engagement dafür ein, die Anforderungen unserer Kunden zu erfüllen.

Bürogebäude von Cummins

Cummins Inc.

Cummins, ein weltweit führendes Unternehmen in der Energietechnik, ist ein Konzern mit sich ergänzenden Geschäftsbereichen, die ein breites Portfolio an Stromversorgungslösungen entwickeln, herstellen, vertreiben und warten. Die Produkte des Unternehmens reichen von integrierten Verbrennungs-, Elektro- und Hybridantriebslösungen bis hin zu Komponenten wie Filtration, Abgasnachbehandlung, Turbolader, Kraftstoffsysteme, Steuerungssysteme, Luftaufbereitungssysteme, automatisierte Getriebe, Stromerzeugungssysteme, Microgrid-Steuerungen, Batterien, Elektrolyseure und Brennstoffzellenprodukte.

Weniger Abfall, derselbe legendäre Pick-up-Truck

Mitarbeiter vor der Tür

Ob Leistung, Zuverlässigkeit oder Langlebigkeit – 75 % aller Besitzer von RAM-Schwerlast-Pick-ups der Klassen 2500 und 2500 entscheiden sich für den optionalen Cummins Inc. 6,7-l-Turbo-Diesel. Die Herstellung dieses legendären Motors wird jeden Tag sauberer.

Im April 2022 führten Sven Creutz, Indirect Materials Manager bei Columbus Mid-Range Engine Plant (CMEP), und Clayton Johnson, Continuous Improvement Leader, ein Recyclingprogramm für Nitrilhandschuhe ein, um Abfälle von den Mülldeponien fernzuhalten. Aber was sind Nitril-Schmiermittel und was hat das Plants-Programm bisher bewirkt?

Was sind Nitril-Schutzmittel?

Wahrscheinlich haben Sie die leuchtend violetten, orangefarbenen oder blauen Handschuhe schon in Ihrer Arztpraxis, Apotheke oder in der örtlichen Autowerkstatt gesehen. Nitrilhandschuhe sind eine Standard-PSA-Praxis in vielen Lebensmittel-, Industrie- und Chemielaborbereichen. Diese synthetischen Gummihandschuhe werden aus der Verbindung Nitril hergestellt und sind aufgrund ihrer Chemikalien- und Abriebbeständigkeit besonders beliebt. Sie sind wasser-, fett- und ölabweisend, was sie oft zur ersten Wahl bei Handschuhen für Berufe macht, in denen lange gearbeitet wird und die mit schädlichen Substanzen in Berührung kommen (z. B. Latex).

Wie werden Nitrilhandschuhe bei CMEP verwendet?

Für die Mitarbeiter des Werks dienen Nitrilhandschuhe als zweite Barriere, um die Mitarbeiter von Cummins bei der Inspektion des 6,7-Liter-Dieselmotors vor dem Kontakt mit schädlichen Chemikalien und Verletzungen zu schützen. Die Mitarbeiter tragen die Nitrilhandschuhe in der Regel als Basisschicht unter einem dickeren Paar Handschuhe, die der Sicherheit dienen.

Außerdem schützen sie die Mitarbeiter davor, Produkte zu verunreinigen.

Um die strengen Produktqualitätsstandards einzuhalten, müssen die Mitarbeiter jede Stunde ihre Handschuhe wechseln. Während die Verwendung der Schutzhandschuhe sowohl Mitarbeiter als auch Produkte von Cummins schützt, kann der erzeugte Abfall groß sein. Nitrilhandschuhe sind eine Einweg-PSA; nach dem ersten Gebrauch können sie zum Schutz vor schädlichen Substanzen, die möglicherweise auf der Oberfläche zurückbleiben, nicht erneut getragen werden.

Nitrilhandschuhe gelten als weniger biologisch abbaubar als ihre Gegenstücke aus Latex und werden oft nicht recycelt, da sie in Einrichtungen verwendet werden, in denen sie kontaminiert werden könnten, und daher als zu gefährlich für eine Wiederverwendung gelten.

In einem Jahr können die 800 Mitarbeiter des Cummins Mid-Range Engine Plant über 530 Kisten mit Nitrilhandschuhen verbrauchen, was ungefähr 875.000 Handschuhen entspricht.

Die Auswirkungen des Nitrilhandschuh-Recyclingprogramms

Kimberly-Clark Professional, ein weltweit tätiges Unternehmen, das sich der Herstellung von Produkten für die Sicherheit, Gesundheit und Hygiene von Verbrauchern und Unternehmen verschrieben hat und einer der ersten Hersteller ist, der ein Recyclingprogramm für ungefährliche PEE anbietet, hat sich mit dem Werk zusammengetan, um seine biologisch abbaubaren Nitrilhandschuhe zu recyceln und wiederzuverwenden.

Das Werk füllt alle zwei Wochen Gaylords mit Nitrilhandschuhen und versendet sie zur Sortierung an eine gemeinnützige Organisation in West Virginia, Rightcycle, die Arbeitsplätze für behinderte und benachteiligte Arbeitnehmer bietet. Die gebrauchten, nicht kontaminierten Handschuhe werden dann zu Kunststoffgranulat verarbeitet und zu neuen Produkten wie Aufbewahrungsbehältern, Regalen und Gartenstühlen verarbeitet. Letztendlich hat die Columbus Mid-Range Engine Plant einen Lebenszyklus für Nitrilhandschuhe geschaffen und gleichzeitig Arbeitsplätze geschaffen, erklärte Creutz.

Seit Beginn des Programms hat das Werk eine Tonne Handschuhe gesammelt und an die Rightcycle-Anlage geliefert. Wenn das Werk weiterhin durchschnittlich 530 Kisten Handschuhe pro Jahr verbraucht, könnte es damit rechnen, jedes Jahr fast 3,75 Tonnen Abfall von der Mülldeponie fernzuhalten.

Das Columbus Mid-Range Engine Plant ist in der Lage, wichtige 2030 Ziele der PLANET 2050-Strategie von Cummins zu erreichen, indem es einen kreisförmigen Lebenszyklus für Materialien schafft und durch das Recyclingprogramm weniger Abfall in den Anlagen und Betrieben erzeugt. Für Besitzer, die nach nachhaltig hergestellten Motoren suchen, setzt das Columbus Mid-Range Engine Plant den Standard.


Klicken Sie hier, um mehr über wichtige Initiativen zur Nachhaltigkeit bei CMEP zu erfahren.

Bürogebäude von Cummins

Cummins Inc.

Cummins, ein weltweit führendes Unternehmen in der Energietechnik, ist ein Konzern mit sich ergänzenden Geschäftsbereichen, die ein breites Portfolio an Stromversorgungslösungen entwickeln, herstellen, vertreiben und warten. Die Produkte des Unternehmens reichen von integrierten Verbrennungs-, Elektro- und Hybridantriebslösungen bis hin zu Komponenten wie Filtration, Abgasnachbehandlung, Turbolader, Kraftstoffsysteme, Steuerungssysteme, Luftaufbereitungssysteme, automatisierte Getriebe, Stromerzeugungssysteme, Microgrid-Steuerungen, Batterien, Elektrolyseure und Brennstoffzellenprodukte.

Solarfachleute in New Mexico machen einen Unterschied während einer Zeit potenzieller Versorgungsengpässe

Heimgenerator

Die meisten Menschen kennen New Mexico möglicherweise nur wegen seiner Hitze und der hohen Bergwüsten. New Mexico ist jedoch die Heimat der Eigentümer von NM Solar Professionals, LLC, deren Eigentümer Elaine Silva (Gründer und CFO) und Albert Silva (Mitgründer und CEO) sind. Die in New Mexico geborenen Silvas bieten seit jeher Back-up-Stromversorgungssysteme für Haushalte und Unternehmen in ihrer Gemeinde an, die der Hitze und großen Höhen in New Mexico standhalten. Die Silvas verfügen über integrierte Home-Standby-Generatoren mit Solar für sichere, erschwingliche Notstromversorgung.

Die New Mexico Solar Professionals, LLC (NM Solar Pro) wurde 2016 in New Mexico gegründet. Dieses Unternehmen ist einzigartig auf dem Markt für Energieerzeugung positioniert (Planung, Installation und Integration von Stromerzeugung durch Erdgas, Flüssiggas und andere Stromerzeuger). Dieses lokale Familienunternehmen hat seine Stromerzeugungsprojekte integriert und sich Cummins als Händlernetzwerk für Stromerzeugungsanlagen für Privathaushalte und kleine Unternehmen angeschlossen. Mit der Erfahrung im Baugewerbe und der Lizenz als Generalunternehmer und Elektroinstallateur ist es ein großer Vorteil, den Kunden die bestmöglichen Installationen zu bieten.

NM Solar Professionals-Logo

Der Name des Unternehmens lässt natürlich nicht vermuten, dass es Cummins-Stromerzeuger für Privathaushalte und kleine Unternehmen verkauft. Angesichts des Rekordwachstums der Solarbranche war es jedoch naheliegend, ähnliche kostengünstige Erdgas-/Primärenergiesysteme in Betracht zu ziehen, die den Kunden bei der Deckung des täglichen Bedarfs helfen könnten. Ein Geschäftszug, der sich als Erfolg für die Silvas erwiesen hat. Sie haben festgestellt, dass die meisten Hausbesitzer nicht wissen, dass ein Solarexperte benötigt wird, um ihr bestehendes Solarsystem mit ihrem zusätzlichen Stromerzeugungssystem zu kombinieren; ein entscheidender Vorteil, den NM Solar Pros erfüllen kann.

Da es in New Mexico nicht viele Händler gibt, die über eine ähnliche Ausbildung, Lizenzierung und einen ähnlichen Hintergrund wie Silva verfügen, wird der tägliche Bedarf an Notstromversorgung immer häufiger. Ein wichtiger Grund dafür ist die kürzliche Abschaltung der San Juan Generating Station, einem lokalen Kohlekraftwerk, das nach den Prognosen der Silvas etwa ~20% des lokalen Strommarktes vom Netz nehmen wird. Leider gibt es von der örtlichen Regierung keine Anzeichen für eine Aufrüstung oder den Bau neuer Anlagen, so dass eine Lösung dringend erforderlich ist. NM Solar Pros möchte weiterhin eine wichtige Quelle der Hoffnung für die Gemeinschaft sein.

Für die Silvas ist dies ein entscheidender Moment für die Installation von Cummins-Generatoren. In Erwartung eines 10-stündigen Stromausfalls an einem unvorhersehbaren Tag haben die Silvas begonnen, mit der Gemeinde an kosteneffizienten Investitionen in die Cummins-Generatoren der Quiet-Series für Privathaushalte mit einer Leistung von 20kw zu arbeiten. Sie gehen davon aus, dass die Kunden mit einem Cummins Home-Standby-Generator etwa 50 % weniger ausgeben und 50 % mehr Strom erhalten als mit einer Backup-Batterieoption.

Als Cummins-Händler konnten sie ihre Gemeinde auf mehr als eine Weise unterstützen.

Die Silvas sagen, dass sie am meisten Freude daran haben, ihre Kunden in der Nutzung der Systeme zu schulen und zu wissen, dass sie über Energiefreiheit verfügen, die lang- und kurzfristige Ausfälle zu allen Jahreszeiten überdauern kann. Es erfüllt sie mit großem Stolz, dass die Kunden wissen, dass sie ein sicheres und erschwingliches Backup-System für ihr Haus haben, selbst wenn ihr örtliches Versorgungsunternehmen keine Sicherheit bietet.

NM Solar Pros hat eine glänzende Zukunft vor sich, das Unternehmen wächst Monat für Monat mit der Unterstützung der Gemeinde. 2023 hat es sich NM Solar Pros mit Cummins zur Aufgabe gemacht, Familien dabei zu helfen, die Stromversorgung für ihre Häuser und Unternehmen zu sichern.

Arbeiten an Generatoren

Bürogebäude von Cummins

Cummins Inc.

Cummins, ein weltweit führendes Unternehmen in der Energietechnik, ist ein Konzern mit sich ergänzenden Geschäftsbereichen, die ein breites Portfolio an Stromversorgungslösungen entwickeln, herstellen, vertreiben und warten. Die Produkte des Unternehmens reichen von integrierten Verbrennungs-, Elektro- und Hybridantriebslösungen bis hin zu Komponenten wie Filtration, Abgasnachbehandlung, Turbolader, Kraftstoffsysteme, Steuerungssysteme, Luftaufbereitungssysteme, automatisierte Getriebe, Stromerzeugungssysteme, Microgrid-Steuerungen, Batterien, Elektrolyseure und Brennstoffzellenprodukte.

Cummins kündigt neue Entwässerungspumpen an

Entwässerungspumpe

Cummins Inc. (NYSE: CMI) gab die Verfügbarkeit von zwei neuen Entwässerungspumpenlösungen für den Einsatz im Bauwesen, in der Öl- und Gasindustrie, in der Landwirtschaft, im Bergbau sowie in der Wasser- und Abwasserwirtschaft bekannt. Der QSF4X4 und der QSF6X6 bieten Kunden eine vollständig fertige Pumpe für den Einsatz in ihrem Betrieb, der vom QSF2.8-Motor von Cummins angetrieben wird.

„Die neuen Pumpen sind das Ergebnis vieler Stunden an Kundenforschung. Produktzuverlässigkeit und Betriebszeit sind für sie sehr wichtig, daher haben wir ein robustes Paket entwickelt, das von Cummins starkem Support-Netzwerk unterstützt wird“, sagte Greg Totin, Cummins' Industrial Sales Director.

Diese Pumpen bestehen aus einer hochbelastbaren Gusseisenkonstruktion und werden auf einem vollständig abschleppbaren Anhänger hergestellt, um den Transport zu erleichtern. Sie sind in der Lage, sich selbst zu entlüften, wenn sie mit Wasser gefüllt sind und entlüften sich automatisch wieder. Die Cummins QSF6X6 ist für moderate Fördermengen bis zu 1,430 gpm ausgelegt und kann Förderhöhen bis zu 104 Fuß bewältigen. Der Cummins QSF4X4 unterstützt Durchflussmengen bis zu 1,350 gpm und kann Förderhöhen bis zu 135 Fuß bewältigen.

Der Cummins QSF2.8-Motor, der die Pumpen antreibt, ist für industrielle Anwendungen mit 74 PS in kompakter Baugröße erhältlich. Er nutzt die bewährte Cummins-Kraftstoffeinspritzung, die Turboaufladung und die elektronische Steuerungstechnologie, um ein Spitzendrehmoment von 221 lb-ft zu liefern und gleichzeitig die Abgasnorm Tier 4 Final-Emissionen zu erfüllen. Der geformte Gusseisenblock verleiht dem 2,8-Liter-Motor eine Langlebigkeit bei einem geringen Gewicht von 507 lb.

„Die neuen Pumpen sind mit unseren Telematikdiensten kompatibel, um die Verfügbarkeit und Effizienz zu maximieren und gleichzeitig die Ausfallzeiten zu minimieren“, fügt Totin hinzu.

Die QSF6X6 und QSF4X4 sind in ganz Nordamerika erhältlich und werden auf der ARA-Messe im Februar am Cummins-Stand mit der Nummer 5056 und im März auf der ConExpo am Stand S84615 zu sehen sein. Interessierte Kunden sollten sich für weitere Informationen an ihren örtlichen Händler wenden.


Über Cummins

Cummins Inc. ist ein weltweit führendes Unternehmen mit komplementären Geschäftseinheiten, die ein breites Portfolio an Antriebslösungen entwerfen, herstellen, vertreiben und warten. Die Produkte des Unternehmens reichen von integrierten Verbrennungs-, Elektro- und Hybridantriebslösungen bis hin zu Komponenten wie Filtration, Abgasnachbehandlung, Turbolader, Kraftstoffsysteme, Steuerungssysteme, Luftaufbereitungssysteme, automatisierte Getriebe, Stromerzeugungssysteme, Microgrid-Steuerungen, Batterien, Elektrolyseure und Brennstoffzellenprodukte. Cummins hat seinen Hauptsitz in Columbus, Indiana (USA), und beschäftigt seit seiner Gründung im Jahr 1919 ca. 59.900 Menschen, die sich für eine bessere Welt einsetzen. Dies geschieht durch die Priorisierung der Unternehmensverantwortung mit drei globalen Anliegen, die für gesunde Gemeinschaften entscheidend sind: Bildung, Umwelt und Chancengleichheit. Über ein Netzwerk firmeneigener und unabhängiger Vertriebsstandorte sowie über Tausende Händlerstandorte weltweit bedient Cummins Kunden online. Im Jahr 2021 betrug der Gewinn bei einem Umsatz von 2,1 Milliarden US-Dollar rund 24 Milliarden US-Dollar.

Bürogebäude von Cummins

Cummins Inc.

Cummins, ein weltweit führendes Unternehmen in der Energietechnik, ist ein Konzern mit sich ergänzenden Geschäftsbereichen, die ein breites Portfolio an Stromversorgungslösungen entwickeln, herstellen, vertreiben und warten. Die Produkte des Unternehmens reichen von integrierten Verbrennungs-, Elektro- und Hybridantriebslösungen bis hin zu Komponenten wie Filtration, Abgasnachbehandlung, Turbolader, Kraftstoffsysteme, Steuerungssysteme, Luftaufbereitungssysteme, automatisierte Getriebe, Stromerzeugungssysteme, Microgrid-Steuerungen, Batterien, Elektrolyseure und Brennstoffzellenprodukte.

Weiterleitung zu
cummins.com

Die von Ihnen gesuchten Informationen befinden sich auf
cummins.com

Wir öffnen nun diese Website für Sie.

Vielen Dank.