Von den Energiekosten bis zur Resilienz: die drei wichtigsten Themen für Fachleute in Gesundheitseinrichtungen

""

Die Mehrzahl der erfolgreichen Unternehmen verfügt über eine Marketing-, Produkt- oder Lieferkettenstrategie, doch es gibt noch einen weiteren wichtigen Bereich, den es zu berücksichtigen gilt, wenn man seinen Gewinn maximieren will: eine Energiemanagementstrategie. Heutzutage kann eine gut geplante Energiemanagementstrategie Gesundheitseinrichtungen dabei helfen, ihre Finanzlage zu verbessern. Darüber hinaus helfen die richtigen Energieentscheidungen den Unternehmen, die Zuverlässigkeit ihres Betriebs zu verbessern und ihre Bemühungen um Nachhaltigkeit voranzutreiben.

Given the importance of energy in health care, let’s cover three top of mind topics associated with energy for health care professionals. 

No. 1: Cost of energy continues to be a critical lever to deliver superior financials for health care facilities

Today’s modern health care facilities are not only tech marvels, but intense users of energy. In fact, hospitals are identified as the type of building with the second highest energy use intensity (EUI) by Energy Star1. A median size hospital would use over 12 times more energy than an average size office building. 

Healthcare - Cost of energy to resiliency
Health care facilities such as hospitals and medical offices have high energy use intensity. 

With this, it is no surprise the top two topics C-suite executives are most interested to learn about are cost control and expense reduction, according to Becker Hospital Review2. As this trend on cost control continues, health care facility leaders will increasingly be rewarded in their efforts to cut down energy costs. 

Typically, a health care facility acquires energy in the form of electricity from the power grid and separately burns natural gas to produce heat or steam. Purchasing electricity from the grid brings the advantage of convenience but at a significant cost for the health care facility. This cost is due to the inefficiencies in centrally producing the electricity and distributing it through large geographies.

Healthcare - Inefficiencies in energy waste
Inefficiencies and energy waste in centralized generation result in higher energy costs for customers.

In comparison, on-site combined heat and power (CHP) applications can offer 70% to 90% efficiency while delivering electricity and heat to the facility. This heat and steam are commonly used for sterilizing medical instruments, keeping patients and staff at a comfortable temperature and maintaining facilities’ humidity level. Some facilities, such as Royal Children’s Hospital in Melbourne, Australia, also pursue tri-generation to further improve energy efficiency. Tri-generation systems produce cooling in addition to heating and electricity offered by CHP applications.

This increase in efficiency could translate into an energy savings up to 35% for the health care facility, depending upon size and facility structure. Health care facilities with access to natural gas can take advantage of CHP applications with lean-burn engine generators that use natural gas as the fuel to produce electricity, heat and steam. These systems could be as small as 300 kilowatts or as large as several megawatts. For instance, a Sydney hospital partnered with Cummins on a cogeneration plant providing 4 megawatts electric of base load power to improve energy efficiency and to meet emission targets.

No. 2: Health care facilities can improve financial performance and resiliency with emerging power system technologies such as microgrids

Did you know that average U.S. electricity customer disruption was over seven hours in 2017, almost doubling the average disruption in 20163? Take a look at how changing weather patterns impact our grid and cause more power outages. Most health care facilities are legally required to have emergency back-up power systems. These systems provide peace of mind and security for the facility and its patrons but are also costly assets that might sit idle for most of the time. 

Facility leaders that aim to have superior financial performance are leveraging microgrids to monetize their energy assets, including existing emergency back-up power systems. A microgrid is a local energy grid with control capability, which means it can disconnect from the traditional grid and operate autonomously4. Microgrids commonly feature advanced control systems and software to track electricity prices and usage at the facility, and they decide whether to buy electricity from the grid or to produce it on-site through the microgrid assets. In summary, micro-grids convert the existing on-site power generation systems into financial enablers for the facility leaders. 

Facility leaders can also leverage microgrids for resiliency purposes. Microgrids take the resiliency of traditional emergency back-up power systems to the next level by integrating additional energy assets to the existing back-up power system. These additional energy assets could be electricity sources, such as solar photovoltaics and CHP generators, storage assets such as batteries, and control systems and software. Integration of additional assets creates redundancy in electricity generation and increases the resiliency of the system.

No. 3: Health care facility leaders leverage digitization of power systems to manage their facilities

There is substantial news coverage on penetration of digitization in health care with respect to patient experience. On the other hand, not everybody sees the impact of digitization in health care with respect to facility management.

While building management systems (BMS) have been around for decades, today’s BMS are ever more digitized as sub-systems ranging from heating and ventilation equipment to power systems being digitized. 

Digitization is also changing how health care facility professionals do their jobs; being more focused on preventative actions driven by rich analytics to avoid potential future issues. They are also increasingly partnering with vendors beyond a purchase transaction or service event.

Let's take health care power systems as an example. Modern remote monitoring systems such as Cummins PowerCommand Cloud help facility teams reduce downtime by providing teams remote access to make decisions and act on them quickly. Moreover, facility teams can partner with a local Cummins distributor, which can handle routine issues remotely and mitigate potentially serious situations by scheduling proactive service calls based on the data they see.

In summary, health care facility leaders focused on financial gains could explore CHP applications to cut their energy costs, and microgrids to monetize their on-site power generation assets. Facility leaders focused on resiliency should also learn more about health care microgrid applications.

To learn more about trends in the health care industry follow Cummins on Facebook and connect on LinkedIn. To learn more about power solutions for the health care industry, visit our web page. To learn more about how Cummins is powering a world that’s “Always On,” visit our web page.

Think your friends and colleagues would like this content? Share on LinkedIn and Facebook.

Verweise:
1 EnergyStar Portfolio Manager Energy Use Benchmarking. [PDF file]. n.d. (2012, October). Retrieved August 18th, 2019 from https://www.energystar.gov/
2 Lazerow, R. (2018, July 11). What 146 C-suite executives told Advisory Board about their shift in priorities this year. Retrieved from https://www.beckershospitalreview.com/
3 n.d. (2019, July 31). Annual Electric Power Industry Report, Form EIA-861. Retrieved from https://www.eia.gov/
4 Lantero, A. (2014, June 17). How Microgrids Work. Retrieved from https://www.energy.gov/

 

Aytek Yuksel – Cummins Inc

Aytek Yuksel

Aytek Yuksel ist der Content Marketing Leader bei Cummins Inc. mit schwerpunkt auf den Märkten für Power Systems. Aytek ist dem Unternehmen 2008 beigetreten. Seitdem war er in mehreren Marketingpositionen tätig und bringt Ihnen jetzt die Erkenntnisse aus unseren wichtigsten Märkten, von der Industrie bis zum Wohnbereich, ein. Aytek lebt mit seiner Frau und seinen zwei Kindern in Minneapolis im US-Bundesstaat Minnesota.

Hurrikan Sally ist kein Problem für ein Ehepaar aus Florida und ihren Notstromgenerator zu Hause

Familie mit Hund neben einem Cummins Notstromaggregat stehend

Drei Monate. So wenig Zeit hatten Macy und Sherry Summers zwischen der Installation ihres neuen Cummins QuietConnect-Standby-Generators™ für Haushalte und dem ersten großen Test: der Ankunft des Hurrikans Sally.

Der Hurrikan der Kategorie-2 wüte im September 2020 fast 12 Stunden lang über dem Gebiet von Pensateroperabilität im Bundesstaat Fla. und verursachte Winde von 110 meilen/h, starken Regen und größere Stromausfälle. Während sich viele ihrer Nachbarn während des Sturms überfluteten, waren die Sommer sicher, da sie wussten, dass ihr Cummins-Generator ihnen helfen würde, sie durchzuziehen.

"Ich war sehr beschämt darüber, dass, wenn zu viel Wasser in der Nähe des Haus ankam, es dazu kommen könnte", sagte Macy. "Ohne Strom konnten wir unsere Pumpen nicht betreiben, wir konnten das Wasser nicht von unserem Gewässer entfernen. Das war die große Angst um mich."

Der neue Cummins-Generator kam immer wieder durch, treibt während des Sturms seine Heim- und drei Sump-Pumpen an und betrieb fast 90 Stunden mit einer Unterbrechung für einen Ölwechsel, bevor die Stromversorgung wieder hergestellt wurde.

Seine Leistung war keine Überraschung für Macy, einen ehemaligen Lockheed Martin-Ingenieur. Nachdem er 2019 dauerhaft ins Haus zog, nutzte er seinen Forschungssinn, um den besten Weg zu finden, ihr Haus durch einen Sturm anzutreiben. Nach 18 Monaten entschied er sich aufgrund des guten Rufs, der Qualität und des Supports für einen Standby-Generator für den Heimbetrieb von Cummins.

"Die Marke war für uns wirklich wichtig. Wir wollten ein gutes Support-System von einem großen Unternehmen, von dem wir wussten, dass es da sein würde, wenn wir es brauchen. Es stellte sich heraus, dass Cummins der richtige für uns war", sagte Macy.

"Ich würde Cummins sicherlich gegenüber den Marken empfehlen, von denen die meisten Menschen schon einmal gehört haben. Cummins ist eine stärkere Lösung für alle, die diese Zuverlässigkeit wollen."

Für die Installation bestellten die Summers Notstromaggregate, ihren örtlichen Cummins-Händler im nahegelegenen Fort Walton Beach, der ebenfalls den Generator für sie wartet und wartet.

Raul Perez, der die Generatorinstallationen für die Notstromversorgung beaufsichtigt, sagt: "Wir versuchen, mit einem Produkt zusammen zu arbeiten, von dem wir wissen, dass wir eine komfortable Wartung haben, dass wir es mit der Installation bequem haben und dass wir komfortabel hinten stehen. Das bedeutet viel. Wir arbeiten gerne mit Cummins zusammen, denn wenn wir anrufen und Unterstützung brauchen, sind sie immer da."

Sherry sagt, dass der QuietConnect-Generator seinem Namen gerecht wird. "Es ist unglaublich, dass wir, wenn wir es hören, immer sagen werden: 'Oh, da ist der Generator. Die Leistung muss ausgeschaltet sein." Wir machen einfach weiter, was wir auch tun", sagte sie.

Nach dem Hurrikan haben die Summer volles Vertrauen in ihren Cummins-Generator. Sherry sagt, dass sie sich nicht mehr darum kümmern will, dass das Haus kühl ist und die Lachpumpen am Laufen bleiben.

Macy fügt hinzu: "Wenn ein Hurrikan kommt, kann ich mich wirklich um diese Systeme kümmern, die wir zum Schutz unseres Heims eingesetzt haben. Sie haben jetzt eine konstante Leistung, die vom Generator aktiviert wird."

Besuchen Sie den Cummins Generatorgrößenrechner, um den perfekten Generator für Ihr Zuhause zu finden.


Um zu hören, wie die Summers ihre eigene Geschichte erzählen, sehen Sie sich das folgende Video von ihnen an.
https://www.youtube.com/watch?v=Lv9jxX7PFGU

Bürogebäude von Cummins

Cummins Inc.

Cummins, ein weltweit führendes Unternehmen in der Energietechnik, ist ein Unternehmen mit sich ergänzenden Geschäftsbereichen, die ein breites Portfolio an Stromversorgungslösungen entwickeln, herstellen, vertreiben und warten. Die Produktpalette des Unternehmens reicht von Verbrennungs-, Elektro- und Hybrid-Integrated-Power-Lösungen und -Komponenten wie Filtration, Abgasnachbehandlung, Turbolader, Kraftstoffsysteme, Steuerungssysteme, Luftbehandlungssysteme, automatisierte Getriebe, elektrische Stromerzeugungssysteme, Mikronetz-Steuerungen, Batterien, Elektrolyseure und Brennstoffzellenprodukte.

Cummins bringt neues Twinpack-Dieselstromaggregat zur Miete auf den Markt

Logo von Cummins am Eingang des Werks in Fridley

Cummins Inc. (NYSE: CMI) hat einen neuen 1 MW Twinpack-Mietgenerator, den C1000D6RE, eingeführt, der eine wettbewerbsfähige Mietstromlösung für eine vielfältige Palette von Anwendungen in ganz Nordamerika bietet. Das neue Modell C1000D6RE wird von Cummins hergestellt, einem Unternehmen, das seit 1919 für Technologie, Zuverlässigkeit und Service steht.

Als Doppelpack kombiniert der C1000D6RE zwei Cummins 15-l-Generatoren mit 500 kW zu einem einzigen, 40 Fuß großen Stromversorgungsgerät mit Abgasnachbehandlung. Dies ermöglicht es dem C1000D6RE, die Endgültigen Emissionsvorschriften von Tier 4 zu erfüllen und gleichzeitig eine zuverlässige, hohe Leistung zu liefern. Der Generator kann parallel zu anderen Mietstromlösungen eingesetzt werden und ist in der Lage, den Lastbedarf ohne Meister zu bewältigen.

Der C1000D6RE bietet eine Nennleistung von 1000 kW gemäß ISO 8528 und wird von 2 x US Tier 4 Final zertifizierten QSX15 Cummins-Motoren angetrieben. Der QSX15-Motor erfüllt die strengen EPA-Normen ohne den Einsatz eines Dieselpartikelfilters (DPF), der eine einfache Wartung, geringere Emissionen und eine höhere Leistung bietet.

Ein neues Schwerlast-Anhänger- und Zugdesign sorgt für noch mehr Zuverlässigkeit für robuste mobile Stromversorgungsanwendungen. Der Behälter des Generators hält extremen Wetterbedingungen stand, während ein vollständiges Schalldämpfungspaket den Geräuschpegel des Generators minimiert. Für schnellere und sauberere Ölwechsel ist auch eine Option für das Ölwechselsystem "Quick Fit" verfügbar.

Der C1000D6RE bringt 69.000 Pfund Kraftstoff auf die Waage und ist mit einem Front-End-Dämpfer und einem mobilen Air-Ride ausgestattet, um die Auswirkungen von Reisestrecken zu reduzieren und mögliche Ausfallzeiten zu minimieren.

Der C1000D6RE ist für den Einsatz in einer Vielzahl von großen Branchen geeignet, die Mietgeräte benötigen, einschließlich: Baustellen, Notstromversorgung, Großereignisse, Industriegebäude und Versorgungsunternehmen in entlegenen Standorten oder städtischen Gebieten.

John Gebenbons, Direktor für Mietgerätemärkte bei Cummins, sagte: "Wir haben unseren Kunden zugehört und den C1000DR6RE speziell entwickelt, um ihre Anforderungen zu erfüllen. Wir wollten auch der Produktion eines Generators Priorität ein geben, der unabhängig vom Klima, dem Standort oder der Branche weiterhin zuverlässige Stromversorgungslösungen bereitstellt. Wir sind davon überzeugt, dass dieses Produkt den Märkten mehr Zuverlässigkeit, verbesserte Leistung und größere Flexibilität bieten wird."

Das 1MW Twinpack-Modell kann für eine Vielzahl von Branchen eingesetzt werden, die mobile Stromversorgung benötigen; Von Baustellen, Industriegebäuden und Versorgungsunternehmen in abgelegenen Standorten oder städtischen Gebieten. Die Fernstart- und Stopp-Kontaktfunktion ermöglicht es, den Generator auf Abruf ein- und auszuschalten, ohne dass lokale Wartungsunterstützung erforderlich ist. Infolgedessen können Kunden mehr Stabilität, längere Betriebszeit und niedrigere Arbeitskosten erwarten, die zu niedrigeren Gesamtbetriebskosten führen.

Um eine kontinuierliche Leistung zu gewährleisten, bietet Cummins seinen Kunden Wartung und Wartung seiner mobilen Stromaggregate an. Die Ersatzteilmarkt-Kapazitäten von Cummins werden über ein Netzwerk von über 200 lokalen Vertriebs- und Servicestandorten in ganz Nordamerika bereitgestellt; unterstützt von einem globalen System von Servicetechnikern, Ingenieuren und Teile-Vertriebszentren, das erfahrungskundig darin ist, mobile Stromversorgungslösungen für jeden Strombedarf anzubieten.

Bürogebäude von Cummins

Cummins Inc.

Cummins, ein weltweit führendes Unternehmen in der Energietechnik, ist ein Unternehmen mit sich ergänzenden Geschäftsbereichen, die ein breites Portfolio an Stromversorgungslösungen entwickeln, herstellen, vertreiben und warten. Die Produktpalette des Unternehmens reicht von Verbrennungs-, Elektro- und Hybrid-Integrated-Power-Lösungen und -Komponenten wie Filtration, Abgasnachbehandlung, Turbolader, Kraftstoffsysteme, Steuerungssysteme, Luftbehandlungssysteme, automatisierte Getriebe, elektrische Stromerzeugungssysteme, Mikronetz-Steuerungen, Batterien, Elektrolyseure und Brennstoffzellenprodukte.

Euro 7/VII – das fehlende Puzzlestück zur Verbesserung der Luftqualität in Europa

Euro 7/VII – das fehlende Puzzlestück zur Verbesserung der Luftqualität in Europa

Das Umfeld befindet sich in einer kriselndem Umfeld, und wir müssen jetzt handeln, indem wir die Emissionen reduzieren, um eine unzureichende Luftqualität anzugehen und den Klimawandel zu stoppen. Politik, Industrie, Wissenschaft und Vordenker müssen gemeinsam an der Neutralisierung dieser Drohungen arbeiten. Der demnächst vorgelegte Verordnungsantrag gemäß Euro 7/VII hat, wenn auch ehrgeizig, das Potenzial, einen bedeutenden Unterschied zu machen.

Melina Kennedy, Vizepräsidentin Produktkonformität und regulatorische Angelegenheiten bei Cummins Inc.
Melina Kennedy, Vizepräsidentin Produktkonformität und regulatorische Angelegenheiten bei Cummins Inc.

Die EU ist ein Wegbereiter in der Klimarichtlinie und hat durch den ehrgeizigen europäischen Grünen Deal klare Ambitionen gesetzt, bis 2050 klimaneutral zu sein. Das Paket "Fit für 55" war eine ausgezeichnete Reihe von Maßnahmen, um den Übergang voranzutreiben, und der RepowerEU-Plan wird nun wohl als Katalysator fungieren, der erforderlich ist, um noch schneller Veränderungen zu bewirken. Das Rätsel, das noch fehlt, um den Übergang zu beschleunigen, sind die vorgeschlagenen Vorschriften für Euro 7/VII für Autos, Lieferwagen und Schwerlastfahrzeuge.

Wir bei Cummins sind bestrebt, mit unserer Destination ZeroTM-Strategie null Emissionen zu erreichen. Wir unterstützen voll und ganz eine strenge, klare, durchsetzbare Euro-VII-Regelung, die uns den Wettbewerb unter fairen Wettbewerbsbedingungen ermöglicht und der Umwelt echte Vorteile bringt. Unsere technischen Experten sind sicher, dass wir die ehrgeizigen Ziele erreichen können. Wir hoffen, dass der Verordnungsantrag diese Ambitionen bei der Veröffentlichung widerspiegelt.

Die Europäische Green Deal-Strategie spiegelt unseren eigenen Planet 2050-Plan bei Cummins wieder, in dem wir Ambitionen haben, dass alle unsere Anlagen, Betriebe und Produkte bis 2050 klimaneutral werden. Cummins ist ein weltweit führender Anbieter von Technologien, um die weltweiten Herausforderungen im Bereich Nachhaltigkeit zu meistern. Wir sind seit weit über 100 Jahren innovativ und haben einen starken Fußabdruck in Europa, wo wir ein breites Portfolio an Energielösungen für Transport- und Energieanwendungen entwickeln, herstellen, verkaufen und warten.

Auf diesem Weg in eine null-emissionsfreie Zukunft kann die Einführung sauberer Technologien wie erdgasbetriebener Produkte und Diesel mit nahezu Null-Emissionen bereits vor der allgemeinen Kommerzialisierung von Null-Emissions-Technologien für alle Märkte sofort positive Auswirkungen haben. Die Euro-VII-Verordnung und ihr Zusammenspiel mit der CO2-Verordnung für Schwerlastfahrzeuge sind daher entscheidend für die Reduzierung von Emissionen und die Verbesserung der Luftqualität am Anfang dieser Reise in eine emissionsfreie Zukunft. Dieser kurzfristige Schritt ist für den Schwerlastsektor entscheidend, der aufgrund seiner typischen Nutzungsanforderungen und ihres Gewichts aus Luftqualitäts- und Emissionssicht viel schwieriger zu reduzieren ist als andere Branchen.

Damit die Industrie innovativ sein kann, brauchen wir einen klaren Zeitplan und eine klare Anleitung von den politischen Entscheidungsstellen darüber, welche Vorschriften in den kommenden Jahren anstehen. Als weltweit größter unabhängiger Motorenhersteller im Schwerlastbereich ist es für unser Geschäft und die unserer Kunden von maßgeblicher Bedeutung, die Euro-VII-Vorschriften im Detail zu kennen und zu verstehen.

Der Zeitpunkt der Regelung bestimmt unsere Produktplanung, Technologieentwicklung, Investitionsentscheidungen und unseren Weg zu null Emissionen. Eine weitere Verzögerung der vorgeschlagenen Veröffentlichung des Euro-VII-Verordnungsantrags im Juli ist für diejenigen in der Branche sehr schwierig, die Zeit benötigen, um Produkte zu entwickeln, zu entwickeln und einzuführen. Wir hoffen, dass die Euro-VII-Verordnung weiterhin auf dem neuesten Aktualisierten Zeitplan steht, da für die Bereitstellung einer neuen Motortechnologieplattform ein hohes Maß an Komplexität und entsprechendem Zeitaufwand erforderlich ist. Cummins ist bereit, die Anforderungen einer strengen Verordnung zu erfüllen, aber es würde eine neue Basismotorhardware, neue Software, neue Architekturen und Komponenten für die Abgasnachbehandlung erfordern, um nur einige zu sein. Und wir wollen sicherstellen, dass die Vorlaufzeit angemessen ist, damit die notwendigen Innovationen stattfinden können, um der Umwelt, unseren Kunden und Endverbrauchern mit neuen und zuverlässigen Technologien zugute zu kommen.

Für den Schwerlastsektor auf dem Weg zu emissionsfreien Emissionen gibt es kein Wundermittel. Um die Anforderungen von Euro VII zu erfüllen und die im Europäischen Green Deal festgelegten Ziele null zu erreichen, ist eine Reihe verschiedener Stromversorgungslösungen erforderlich. Richtlinienanträge, die einen technologieneutralen Ansatz verfolgen, sind entscheidend für die Innovation und werden sicherstellen, dass der Euro-VII-Vorschlag erfolgreich sein wird. Auf unserer Innovationsreise für den Schwerlastsektor hat Cummins die branchenweit erste kraftstoff-aggnostische Verbrennungsmotorplattform vorgestellt, die so ausgelegt sein kann, dass sie mit verschiedenen Kraftstoffen optimal betrieben werden kann, einschließlich Diesel, erneuerbarem Erdgas oder Wasserstoff. Diese Technologien können es unseren Kunden und Endanwendern ermöglichen, weg von fossilen Brennstoffen zu gehen und die Anforderungen von Euro VII erschwinglich zu erfüllen.

Cummins investiert stark in emissionsfreie Technologien und gibt jedes Jahr über 1.07 Milliarden USD (1 Milliarden EURO) für Forschung und Technologie aus. Cummins ist heute weltweit führend in der Batterie- und Wasserstofftechnologie, wobei ein Großteil dieser Arbeit in Europa stattfindet. Cummins verfügt über ein Brennstoffzellen-Produktionswerk in Herten, Deutschland, das Stromversorgungslösungen für Züge und Lkw bereitstellt. Cummins ist einer der weltweit größten Hersteller von Elektrolyseuren für die Produktion von grünem Wasserstoff. Er verfügt über Standorte in Belgien und ein zukünftiges Werk in Spanien. Und wir haben ein Joint Venture mit NPROXX zur Herstellung kritischer Wasserstofftanks für die Lagerung und den Transport in Deutschland. All dies sind Technologien, die für die Schaffung einer Wasserstoffwirtschaft hier in Europa und für den Erfolg des europäischen Green Deal unerlässlich sind.

Die Schwerlastmotor- und Fahrzeugindustrie in Europa stand in den letzten drei Jahren vor größeren Herausforderungen als in erinnerung. Austritt aus Großbritannien, Covid, erhebliche Knappheit in der Lieferkette und jetzt die Krise in Großbritannien. Eine phase der regulatorischen Gewissheit mit klaren Leistungen und gleichzeitig die Bewältigung der im Europäischen Green Deal festgelegten Herausforderung wird entscheidend für den Erfolg des Sektors sein. Wir verlangen, dass der anstehende Vorschlag für eine Verordnung nach Euro VII in seinem Ansatz zeitnah, klar, ehrgeizig und technologisch neutral ist. In diesem Falle würde er ein fehlendes Rätsel auf dem Weg in die Ecke für den Sektor und für eine nachhaltigere und wohlhabendere Zukunft in Europa lösen.

Melina Kennedy

Melina Kennedy ist Vizepräsidentin für Produktkonformität und regulatorische Angelegenheiten bei Cummins Inc. Zuvor war sie als Direktorin für Executive Communications bei Cummins Inc. tätig. Dort entwickelte und implementierte sie Strategien auf hohem Niveau, um die wichtigsten Kommunikationsanforderungen unserer Führungskräfte zu erfüllen. Melina ist eine ehemalige Kandidatin für die Bürgermeisterin von Indianapolis und Rechtsberaterin bei Baker and Daniels. Zuvor war sie als Direktorin für Wirtschaftsentwicklung bei dem früheren Bürgermeister von Indianapolis Bart Peterson tätig, wo sie ihr Talent als Führungskraft und Communicator nutzte.

Generator Onan SD20 treibt mobiles Verkaufsgeschäft in Richmond, Va. an

Mehrfarbiger mobiler Verkaufswagen mit SD20-Generatorantrieb

Das Unternehmen befindet sich in Virginia, The Sweet X telematics, formell bekannt als Das Wshader Ice von Einem der Unternehmen, das 2020 begann, als die Pandemie begann. Besitzerin und Alleineigentümerin Tierra Mclaurin teilte mit: "Ich wollte schon immer in das italienische Ice-Geschäft einsteigen, und das war der perfekte Zeitpunkt, zu beginnen, seit wir im Lockdown waren."

McLaurin begann mit dem Verkauf von Wshader Ice aus ihrem Auto mit Kühlern. Nach der Öffnung der Stadt wollte sie ihr Unternehmen legitimieren und einen Lkw kaufen. Jetzt verkauft McLaurin ein komplettes Sortiment an Köstlichkeiten, darunter auch ihr originales Wshader Ice.

"Es geht nicht nur um die Qualität des Produkts, sondern um die erfahrungsgemäße Erfahrung", sagt Mclaurin. SweetX ist spezialisiert auf das Mischen von Getreide-Inktoffel-Milks, Sundaes, Wshader-Eis, pflanzlichen Köstlichkeiten und mehr.

Sweet X nun mit dem Leitartikel "The Main Event" ist der Grund, warum Mclaurin den Onan SD20-Generator von Cummins gekauft hat. "Wir benötigten einen Generator mit Leistung und groß genug, um unsere Maschine zu betreiben, die mit 16.000 kW läuft. Cummins hat genau das geliefert, was wir benötigten."

Als Mclaurin begann, sich nach Generatoren zu erkundigen, schlug ihr Eisdielenhersteller den Onan SD20 vor und teilte mit, dass sie 16.000 Kilowatt benötigt, um ihr Unternehmen anzutreiben. Nachdem sie die Möglichkeit hatte, den Generator in einem Demo-Truck im Einsatz zu sehen, wurde sie verkauft und begeistert bei der Gelegenheit, ihren Traum zu verwirklichen und ein einzigartiges Unternehmen in ihre Stadt zu bringen.

Nachdem sie gedacht hatte, dass sie eine Schnur ziehen würde, um den Generator zu kurbeln, war Mclaurin überrascht, wie einfach der Onan SD20 zu bedienen war. "Der SD20 ist sehr einfach zu bedienen. Sie müssen nur die Schalter einschalten. Danach wird man aufgefordert, auf welche Tasten man drücken muss, um es zum Laufen zu bringen", erklärt sie. "Sobald Sie mit dem System verbunden sind, müssen Sie nicht mehr außerhalb des Fahrzeugs fahren, um es zu starten. Es ist nur der Umschalter und der Generator läuft."

Mclaurin sitzt neben dem Onan SD20-Generator, der im mobilen Geschäft platziert ist

Mit dem Onan SD20 kann Mclaurin ein ultimatives Erlebnis mit Soft Serve Eis-Eiseis bieten. "Mit dem SD20 kann ich mehrere Kegel produzieren. Das ist das Ziel, meinen Kunden den Dienst zu liefern."

Die Saison von Sweet X nun im Sommer läuft nur zum Aufwärmen. "Mit einem zuverlässigen Generator werden wir es nicht um längen kommen. Stellen Sie sich vor, Sie haben einen Eiskonus mit Schaumstoff und Einem eisgeeisten Kegel? Dank Cummins haben wir es bei The Sweet X gleichzeitig. Dieser Generator war gut zusammengestellt, einfach zu bedienen, leise und erstklassiger."

Wenn Sie einen Schwerlast-Generator benötigen, sollten Sie sich nicht den Onan SD20 ansehen."
 

Schilder
Bürogebäude von Cummins

Cummins Inc.

Cummins, ein weltweit führendes Unternehmen in der Energietechnik, ist ein Unternehmen mit sich ergänzenden Geschäftsbereichen, die ein breites Portfolio an Stromversorgungslösungen entwickeln, herstellen, vertreiben und warten. Die Produktpalette des Unternehmens reicht von Verbrennungs-, Elektro- und Hybrid-Integrated-Power-Lösungen und -Komponenten wie Filtration, Abgasnachbehandlung, Turbolader, Kraftstoffsysteme, Steuerungssysteme, Luftbehandlungssysteme, automatisierte Getriebe, elektrische Stromerzeugungssysteme, Mikronetz-Steuerungen, Batterien, Elektrolyseure und Brennstoffzellenprodukte.

Weiterleitung zu
cummins.com

Die von Ihnen gesuchten Informationen befinden sich auf
cummins.com

Wir öffnen nun diese Website für Sie.

Vielen Dank.