电力城市:转向电气化运输的未来

康明斯-大蓝巴士-电动运输
在8月2017日,圣莫尼卡市体验到了康明斯提供的第一台 GILLIG 电池电动巴士的清洁动力和潜力。

When it comes to adopting electrified power solutions for transportation, these four cities are leading the way. 

Cities all throughout the world are embracing an electrified future — leading to cleaner air, quieter communities, and more efficient transportation everywhere. 

While electrification is a growing trend just about everywhere, there are a handful of standout cities across the world that have been adopting electrification in breakthrough ways, on a major scale. Let’s celebrate these electric cities for their innovative spirit — and for showing us all what the future of electrified transportation may look like.

Oslo, Norway

Norway has the highest rate of electric car ownership in the world. As of March 2019, electric vehicles (EVs) or hybrids accounted for half of all vehicle sales in Norway, and 57% of all vehicles in the city of Oslo. Norway has a variety of incentives including lower taxes and fees for those driving EVs or hybrids. These regulations make going electric financially feasible for many Oslo residents.

By 2023, Oslo plans to have a city-wide zero-emission taxi system up and running, and they’re already making it simple to charge taxis in the city. To do this, Oslo is installing the world’s first wireless charging system through induction plates. This way, taxis can charge while waiting in a slow-moving line to pick up passengers — making for a much more efficient taxi system, with a greater daily range.  

Shenzhen, China

Every single city bus in Shenzhen is fully electric. That’s 16,000 buses. More than 400,000 electric buses are currently in operation throughout China, and the country is planning to add at least 200,000 more by 2025. 

In China, the government supports electrification enthusiastically through policy and funding. Public transport companies using electric vehicles receive significant subsidies, which makes electrification more accessible for cities of all sizes. With continued government support of electrification, it’s very possible that many other Chinese cities will soon follow Shenzhen’s lead and convert to 100% transit electrification.

San Francisco, United States of America 

Most of the United States has been slower to adopt electrification than the rest of the world. But the state of California is one of America’s leading electric states, and has recently mandated that from 2029 forward, mass transit agencies will only be able to buy electric buses.

While 2029 may seem far away, it’s important to give transit agencies the time they need to adopt fully-electric fleets with the right planning in place. The ten-year mandate will allow these agencies to find and order reliable electric buses and implement necessary infrastructure to ensure they run smoothly in their unique city environments. 

The city of San Francisco is one of the top electrified cities in America. According to the International Council on Clean Transportation, San Francisco has more electric vehicles than anywhere else in the country and more electric vehicle promotion efforts, like policies and subsidies, than any other U.S. city.

Santiago, Chile

To install a city-wide electric bus fleet, there’s a lot more to do than just order a fleet of buses. Charging infrastructure is a key part of the electrification equation. In Santiago, Chile, planners tested charging technology and adjusted the electrical grid long before any buses came to town to create the best possible transport strategy for the city. 

The ultimate plan for Santiago’s transport sector is to have a low-emission system with 6,000 electric buses up and running by 2040.

In Chile, you might say that electric vehicle infrastructure is growing from the ground up. Chile is the world’s largest producer of copper and the world’s second-largest producer of lithium, which are both essential materials used in electric vehicle batteries. 

With an abundance of important battery materials, public policy encouraging EV adoption, and a robust public transit plan for 2040, the city of Santiago and the nation of Chile are helping lead the global electrification movement. 

For many urban transportation systems worldwide, the future is electric. Cities across the world are leading the way in electrified transportation, powering a greener, more efficient tomorrow.

Cummins - Electric Cities - Infographic
Click the image to view a hi-res version of our Electric Cities infographic.


 

康明斯办公大楼

康明斯公司

Cummins is a global power leader that designs, manufactures, sells and services diesel and alternative fuel engines from 2.8 to 95 liters, diesel and alternative-fueled electrical generator sets from 2.5 to 3,500 kW, as well as related components and technology. Cummins serves its customers through its network of 600 company-owned and independent distributor facilities and more than 7,200 dealer locations in over 190 countries and territories.

由康明斯提供动力:徐工电动挖掘机打造其美丽的亮相

康明斯电动挖掘机

在寻找描述我们的电力应用的时候,很多形容词都在脑海中出现,包括耐用、可靠、安全和.....。美丽?这是一个新的(和不寻常的)一个添加到列表中,但今年春天,由康明斯提供动力的新推出的徐工电动挖掘机在其属性列表中添加了 "最美丽"。请继续阅读以了解更多。电动挖掘机

Cummins collaborated with XCMG, the 4th largest construction machinery company in the world, to design and build the 3.5 ton electric excavator, which will serve as a technology demonstrator. Often operating on work sites in densely populated towns and cities around the globe, construction equipment must meet stringent emissions requirements and keep noise and disruption to a minimum while getting the job done. The new electric excavator is suitable for working conditions that require more stringent environmental standards and noise reductions.

该挖掘机由康明斯 BM5.7E 电池模块提供动力,拥有45千瓦时的电池功率。每个电池模块均设计为极高的冲击和振动能力,可承受恶劣的建筑环境条件。电机与液压系统之间的精确匹配创造了高效、可靠、安静的驱动系统,使其成为城市和郊区建设的理想选择。

在单次充电不到六小时的情况下,挖掘机可满足整个8小时轮班的运行需求。短充电时间意味着设备可以在一夜之间充电,从而消除停机时间并充分利用非峰值能量节省的优势。

建筑与合作

去年10月,康明斯和徐工通过签署一项战略合作协议,巩固了他们的长期关系。该协议确保在开发和集成全面的产品系列、价值链和全球运营、创建新的应用、探索新市场并分享有关研发的资源以持续改进方面开展密切合作。

徐工协议
在2019月10日,康明斯和徐工巩固了长期的合作关系。

镜子,墙上的镜子..。

徐工挖掘机由康明斯提供动力的徐工电动挖掘机在今年的 ConExpo 上首次亮相,这是北美最大的建筑展,在内华达州拉斯维加斯举行。挖掘机赢得了它的描述符为 "美丽",因为它赢得了 ConExpo 最美丽的机器奖!将一些强硬的竞争者打到最高档的地方,挖掘机被评为最公平的人选,我们完全同意。

在拉斯维加斯取得胜利后,挖掘机现在又回到了中国,将在康明斯和徐工的一系列性能和客户测试中使用,以证明演示者的能力,并为市场改进稳健的解决方案。

康明斯办公大楼

康明斯公司

Cummins is a global power leader that designs, manufactures, sells and services diesel and alternative fuel engines from 2.8 to 95 liters, diesel and alternative-fueled electrical generator sets from 2.5 to 3,500 kW, as well as related components and technology. Cummins serves its customers through its network of 600 company-owned and independent distributor facilities and more than 7,200 dealer locations in over 190 countries and territories.

受信任,因为它经过测试:康明斯动力 GILLIG 电池电动巴士

康明斯动力 GILLIG 电池电动巴士

值得信赖,因为它已经过测试。

沙子袋、山、无人机和电影摄制组的共同点是什么?嗯,不多,只是他们都是 GILLIG 的重要组成部分,而且康明斯致力于说明康明斯动力 GILLIG 电池电动巴士的测试和验证流程的范围。

自 2017 当康明斯和 GILLIG 宣布合作伙伴关系 共同致力于开发行业领先的全电动动力系统时,这两个组织都在努力地进行设计、测试和验证我们的产品。这并非易事,而是帮助我们区别于竞争对手的一项壮举。在我们推出新技术的同时,我们也以同样的承诺来保证客户对质量的期望。但如何?

I have not failed. I’ve just found 10,000 ways that won’t work.”  - Thomas Edison

测试和验证

康明斯致力于测试和验证我们的产品,以满足客户的需求,这是带来一流解决方案的关键部分。对于我们的电池电气系统(BP74E),这意味着在组件级(例如康明斯专有的电池)上验证产品,实现动力总成水平,甚至更广泛地使用 GILLIG 来测试整体总线的性能。

最终,与大多数学生一样,我们希望通过考试。但正如托马斯. 爱迪生所指出的那样,创新能力不会在没有小故障的情况下完成。测试,而不是成功对流程也是至关重要的。故障测试提供了对产品当前限制的洞察力,以便能够调整设计,并优化性能,以满足客户在日常工作中看到的许多不同情形。我们的客户将会失败,一路上不会发生一些故障。

现实世界条件

GILLIG 和康明斯也自豪地在现实世界中验证我们的产品,而不仅仅是理想条件。为此,最近在 GILLIG 巴士的爬坡测试中进行了说明,在巴士上运行了各种测试,因为它装有沙袋来模拟乘客的重量。能够高效运行但只能如此空洞的动力传动系统对每天都在寻找交通人员的社区来说毫无价值。

同样,我们与现场测试客户密切合作,以细化解决方案并提供值得信赖且可靠的产品。在7月2019日获得第一台现场测试巴士的圣莫尼卡的大蓝巴士在使用实际路线和日常运营场景提供反馈方面一直是至关重要的合作伙伴。与有价值的客户和终端用户合作,确定可提高的机会至关重要。现场测试客户提供的合作与合作伙伴关系使我们能够提供满足和超越客户期望的产品。值得庆幸的是,现场测试已顺利进行,并证明了 大蓝巴士宣布将购买18台额外的电动巴士

信任:我们认真承担的承诺

因此,下次您开车上山或简单地在您的城市旅行,并看到康明斯动力的 GILLIG 电池电动巴士,请放心,它已通过广泛的测试过程,以确保安全和可靠性。我们的客户和社区都信任我们,这是我们不掉以轻心的事情。

康明斯办公大楼

康明斯公司

Cummins is a global power leader that designs, manufactures, sells and services diesel and alternative fuel engines from 2.8 to 95 liters, diesel and alternative-fueled electrical generator sets from 2.5 to 3,500 kW, as well as related components and technology. Cummins serves its customers through its network of 600 company-owned and independent distributor facilities and more than 7,200 dealer locations in over 190 countries and territories.

车队的未来:电气化的四个关键-第4部分

车队零排放的未来

在电池电动车辆方面,商用车部门有四个关键的应用。在 四部分博客系列 的4部分中,我们着眼于新技术必须克服的最后一个障碍:政策和法规。

在这第四个预览博客中,我们将探讨如何在与行业和机构的合作中仔细开发商用电动车的政策和法规。毕竟,可持续发展并非仅限于任何一个部门,而且只有借助电动汽车技术、基础设施和经济专家的洞察力,以及终端用户和其他政策制定者,才能成功地制定出通过的激励措施。

如果您首次阅读此系列,您可以在此处找到 第一个零件 此处的第二部分 三部分.

监管担保人

找到正确的重点将需要在整个移动空间内与利益相关方进行持续的对话、咨询和协作。这里的航线范围广泛:长期的零污染目标将为行业的总体发展方向设定条件;跨行业工作小组将制定成熟的技术标准;为基础设施的推出而提供资金并消除障碍的政策将在可用性方面取得进展;投标合同中的可持续发展规定将展示经济可行性,并为可持续车辆创造市场;数据共享方面的协作性工作将提高监测和效率;将税率与排放挂钩将有助于提高投资回报率。

尽管选择的范围令人望而生畏,但世界各地已经出现了一些最佳实践的例子。例如,来自环境研究小组白罗纳的一份 最新报告 详细说明了一些政策举措的性质,这些措施已经在建设中看到了积极成果,目前占全球二氧化碳(CO2)排放的23%。

例如,在挪威首都奥斯陆,该市的市政开发人员采取了一系列举措,旨在为投标人订立投标合同的最低标准。开发人员采取了 "可以在电动上运行的电力" 的政策,为电气化建筑设备的市场创造了潜力。展望未来,该市预计,到2025,所有公共建筑工地都将运营无排放机械和运输。

奥斯陆倡议的成功的一部分,除了利益相关方决心使其发挥作用之外,还可能采用其政策的措辞。通过使用 "可以在电动上运行的" 这一措辞,城市避免迫使建筑公司采取不恰当的方式(例如电气化不适合电气化的产品),并与他们展开对话,讨论哪些可以和不能通电,携手合作,实现可持续性方面的进展。

将其汇集在一起

在世界各地,通过辛勤工作,将电动汽车的技术能力提升到符合商业应用要求的水平,取得了长足的进步。

这要求我们了解他们的基础设施要求,并明确采取措施,将其总拥有成本降至与传统车辆竞争和超过常规车型的水平,并制定就驱使其通过的政策。

对于康明斯来说,找到正确解决方案的过程始终是一项合作性工作。正确理解意味着在行业和政策的利益相关方以及终端用户之间进行对话,以便深入了解问题并确保成功推出。

如需了解更多详情,请访问我们的 车队的未来白皮书 ,其中介绍了电气化的四个关键要素,其中包括 艾迪生 Lee dg:城市 Nuvve.
 

下载 "车队的未来" 报告(PDF)

康明斯办公大楼

康明斯公司

Cummins is a global power leader that designs, manufactures, sells and services diesel and alternative fuel engines from 2.8 to 95 liters, diesel and alternative-fueled electrical generator sets from 2.5 to 3,500 kW, as well as related components and technology. Cummins serves its customers through its network of 600 company-owned and independent distributor facilities and more than 7,200 dealer locations in over 190 countries and territories.

车队的未来:电气化的四个关键-第3部分

电气化电力-车队的未来-经济现实 BP 3

在电池电动车辆方面,商用车部门有四个关键的应用。在我们的 四部分博客系列 的3部分中,我们研究了新技术必须克服的第三个障碍:经济可行性。

 

目前,EVs 通常比传统动力当量更昂贵。造成这种情况的一个原因是固有的材料成本,电池制造需要大量的锂。然而,随着工艺的改进、效率的提高和结垢的增加,锂离子(Li)电池的制造成本有望减少,而此成本的降低将成为早期商用电动车(EVs)采用的主要推动力。

在 " 车队未来的 " 白皮书预览系列的第三部分中,我们将研究电气化的经济考虑。如果您首次阅读此系列,您可以在此处找到 第一个零件 第二部分.

经济现实

如今,参与车队管理的任何人都熟悉购买商用车所涉及的经济决策。它可以大致分为资本支出(车辆和基础设施的前置成本)、运营费用和运行车辆的日常成本,例如燃料和维护要求。

EV 的采用可能涉及大量支出,这取决于应用的不同而有所不同。虽然可以为某些商用车车队(例如最后一英里的送货车)提供更多的路边充电点,但对于巴士等其他应用,则需要拥有基础设施。事实上,新的电力车队可能需要全新的建筑物配置。不过,可以共享充电点,这意味着可降低前期成本。通过这种方式,大型电气化项目可以比较小的项目提供更好的投资回报。

从运营的角度来看,两个主要的成本领域是能源和维护。电动汽车的能源成本取决于电力价格,因为如今的燃料成本最终取决于石油价格。通过使用远程信息处理来监测磨损并准确预测何时需要维修,维护成本可能会降至最低。

虽然主要的资本支出显然涉及,但通过将价格随着时间的推移而降低,以及通过共享充电点的车辆节省效率,电动车可以--而且在运输卡车方面已经与柴油选择具有经济竞争力。

政策和法规对商用车的电气化有何影响?在下周的 "车队的未来" 博客系列中找到。

下载 "车队的未来" 报告(PDF)

康明斯办公大楼

康明斯公司

Cummins is a global power leader that designs, manufactures, sells and services diesel and alternative fuel engines from 2.8 to 95 liters, diesel and alternative-fueled electrical generator sets from 2.5 to 3,500 kW, as well as related components and technology. Cummins serves its customers through its network of 600 company-owned and independent distributor facilities and more than 7,200 dealer locations in over 190 countries and territories.

正在重定向到
cummins.com

您正在查找的信息位于
cummins.com

我们正在为您启动该网站。

谢谢。