康明斯如何在未来100年蓬勃发展

康明斯董事长兼首席执行官Tom Linebarger在周二的年会上发言。
康明斯董事长兼首席执行官Tom Linebarger在周二的年会上发言。

Chairman and CEO Tom Linebarger celebrated Cummins' 100th anniversary and a successful 2018 at the company's Annual Meeting Tuesday, but he said Cummins must push to meet significant challenges ahead to thrive for the next hundred years.

“It’s worth celebrating. It’s worth stopping and wondering what got us here,” Linebarger said of the 100-year milestone the company reached in February. “…But we must also look forward. We need to ask ourselves, ‘What do we need to bring with us and what do we need to change and improve upon, in order to compete for the next 100 years?’”

He said Cummins anniversary theme, Challenge the Impossible, should help ensure the company doesn’t simply look backwards in 2019.

A SIGNIFICANT ACCOMPLISHMENT

The company’s Annual Meeting is an opportunity for Cummins' leaders to talk about the company’s past year and the future to come. The meeting was held at the Columbus Engine Plant in the company’s headquarters city of Columbus, Indiana (U.S.).

Linebarger did not want to diminish the significance of the anniversary.

“An anniversary is an anniversary, but 100 years as an independent company is not easy to achieve,” he said. “It’s a really important milestone for our company and, frankly, given the change in industry and technology and competitive environment, it’s just getting harder and harder to last 100 years. The odds are pretty strongly against you and here we are 100 years later, still fighting, still succeeding.”

Tom Linebarger speaking at 2019 Annual Meeting
Cummins Chairman and CEO Tom Linebarger lays out the key steps the company must take to thrive in the next 100 years.

He said 2018 was a very strong year, with a company record of $23.8 billion in sales, a 16 percent increase over 2017, which was also a strong year. In the first quarter of 2019, the company had the most profitable quarter in its history.  

INNOVATION IS KEY

Linebarger said to thrive like that in the next 100 years, during good economic times and bad, Cummins must continue to be a leader not just in diesel platforms, but also natural gas, hybrids, electrified power and fuel cells, if that’s where the technology develops.

“Diesel engines have been a leader in our industry for 100 years, but if we look out 100 years they will not be the product of choice in all of our markets,” Linebarger said.

In addition to technology leadership, he said the company must continue to build strong partnerships around the world. Some of the company’s partnerships go back as many as 80 years and have been critical to Cummins’ success.

Linebarger said the company must also continue to help build stronger communities, praising the company’s Cummins Powers Women program launched in 2018. The program is the company’s commitment to the advancement of women and girls around the world by working with nonprofits with proven programs in place to advance gender equity.

DOING MORE TO USE LESS

Finally, he said environmental sustainability will be increasingly important in the future.

“I think all of us know that in order to continue, in order to thrive a hundred years from now, there will be significant challenges to all industrial companies, and certainly a company in the power business, about what impact we’re having on the environment,” Linebarger said. “We will have to produce wealth for all stakeholders while using less, and it’s just that simple.”
 

布莱尔克拉夫林可持续发展通信总监

布莱尔克拉夫林

布莱尔. 克拉夫林是康明斯公司可持续发展通信署署长,于2008年加入了该公司,成为多元化通信总监。布莱尔出身于报纸背景。此前,他曾为印第安纳波利斯球星(2002-2008)和得梅因注册(1997-2002)工作。[电子邮件受保护]

 

高科技工具使康明斯能够在大流行期间为客户提供安全支持

康明斯销售与服务技师可以使用 RemoteConnect 与许多英里以外的专家合作。
康明斯销售与服务技师可以使用 RemoteConnect 与许多英里以外的专家合作。

一组称为 RemoteConnect 的高科技工具使康明斯能够为客户提供支持,同时保持在 COVID-19 危机期间实施的社会疏远和旅行限制。

COVID-19 危机发生之前,康明斯客户关怀团队在2017年创建了这些工具,使专家能够远程查看技术人员所看到的领域,旨在为难以到达的地区的客户提供支持。现在,由于不鼓励旅行来防止病毒的传播,RemoteConnect 的使用急剧增加,使工具比以往更加重要。

康明斯客户关怀经理 Joe 布鲁克斯表示: "在康明斯主题专家无法现场活动的情况下,RemoteConnect 被创造成为替代解决方案." 自2017年以来一直领先于该计划的康明斯医疗管理人员乔. 布鲁克。"这已迅速成为唯一的解决方案,在某些情况下为客户提供服务,原因是 COVID-19。在这些空前的时期,RemoteConnect 一直是一个真正的游戏更换商。

工具的工作原理

这些工具套件配备了一个套件,外观类似于手提箱,包括配备了小型照相机的安全眼镜,技师可以使用这些相机与被称为 "Cfse" 的公司专家合作,以诊断和解决问题。Cfse 可以从字面上看出技师所看到的情况,即使它们相距很远。

RemoteConnect 迅速展示了其提高维修质量的能力,同时减少了误诊、不可恢复的人工费用,以及最重要的是客户的痛苦和痛苦。这些套件已被放置在140多个康明斯网点,主要在美国和加拿大,但康明斯客户关怀也致力于在其他地方部署这些产品。

在 COVID-19 之前,Cfse 在道路上度过了重要的一段时间,与康明斯的特定销售与服务地点的技术人员合作,共同完成艰难的服务工作。此外,他们还将通过 RemoteConnect 与技师合作。

当 COVID-19 被宣布为大流行时,突然一项简单的飞行、培训,甚至是为客户服务的车辆不再是例行选择。很多 Cfse 发现,RemoteConnect 是接下来的最佳之处。

令人印象深刻的数字

虽然配备了摄像头的安全眼镜直播流双向音频和视觉通信可能是最大的魔兽世界因素,但套件还包括:

• LogMeIn 援救:一种工具,为 CFSE 提供远程与现场技术人员合作的能力,并通过控制其台式机。
• 网络桥:一种工具,使 Cfse 能够远程工作,以连接到发动机的电子控制模块(ECM),这是控制其运行的发动机的 command 中心。

As of April, over 5,402 remote support cases had been completed since November of 2018, including 621 that would have required travel, and 3,488 days of downtime were saved. The kit was used 166 times just between February and April.

布鲁克斯和康明斯的其他人士预计,这些数字将在未来数日和数月内增加。RemoteConnect 是康明斯为客户提供技术和创新服务的另一途径。
 

康明斯办公大楼

康明斯公司

Cummins is a global power leader that designs, manufactures, sells and services diesel and alternative fuel engines from 2.8 to 95 liters, diesel and alternative-fueled electrical generator sets from 2.5 to 3,500 kW, as well as related components and technology. Cummins serves its customers through its network of 600 company-owned and independent distributor facilities and more than 7,200 dealer locations in over 190 countries and territories.

康明斯首席执行官在年会上强调员工的安全、独创性

首席执行官 Tom Linebarger 在 COVID-19 危机之前在过去的一次活动中发表讲话。2020年的年会几乎是为了防止病毒的传播而举行的。
首席执行官 Tom Linebarger 在 COVID-19 危机之前在过去的一次活动中发表讲话。2020年的年会几乎是为了防止病毒的传播而举行的。

康明斯正在采取许多步骤,以保护 COVID-19 的员工,董事长兼首席执行官 Tom Linebarger 在星期二的公司年会上表示。

Linebarger 说,该公司为进入工厂的人实施了健康筛查和温度检查,增加了清洁规程,并设立了一个响应中心,由医务人员提供支持,每天24小时回答员工问题,每周七天。

他告诉股东,公司还成立了一个领导委员会来应对报告中的问题和规划团队,专注于未来发展的规划。Linebarger 表示,康明斯运营的员工和社区的健康与安全是公司在这些不确定时刻向前迈进的第一要务。

"康明斯世界各地的大多数办公室员工都是在家工作,我们遵守家庭订单以减少病毒的传播," Linebarger 说。"在本次会议上,我们的一些工厂经历了关闭或减少容量的时期,许多地点现在正在恢复运营,尽管水平非常低。...现在的情况与我们在 COVID-19 之前的操作方式截然不同. "

在工作中的西摩发动机工厂员工
自大流行以来,位于印第安纳州西摩的西摩发动机工厂员工在新的工厂规则下工作。

Linebarger 表示,与大多数办公室员工呆在家里一样,该公司能够将清洁资源转移到员工每天上班的设施中,从而显著提高清洁和消毒规程。对于在工厂工作的员工,除了放映和温度检查外,对于任何显示 COVID-19 症状的人,都可立即提供护理。

对于其工作需要与他人保持密切关系的员工,公司还有额外的个人防护设备供他们佩戴。

不同的工作方式

康明斯还重新设计了某些流程和设施布局,使员工能够安全、有效地运行、重新配置装配线和出入口,以促进社会疏远,并确保公共表面定期清洁。除了回答问题外,响应中心还可进行联系跟踪,以确定可能接触过 COVID-19 的人。

该公司正在使用位于印第安纳州哥伦布市的康明斯 LiveWell 健康中心的医务人员来支持 COVID-19 响应。中心。

Linebarger 表示,自1月首次在中国发现病毒以来,该公司已从处理危机中受益。康明斯在中国武汉拥有多个设施,被认为是此次疫情的震中。由于公司客户对被压抑的需求做出回应,中国的所有康明斯工厂现在都恢复运营,业务活跃。

一名员工在印第安纳州的西摩工作。
除了口罩,任何进入西摩工厂的人都必须通过健康检查来获得体温。

乐观迹象

That is only one hopeful sign. Linebarger said Cummins is also in a strong financial position. At the end of the first quarter of 2020, the company had cash and cash equivalents of $2 billion, strong credit ratings and Cummins’ pension plans are fully funded. Linebarger said aggressive action to cut costs such as reducing pay and hours for some employees, while painful, will serve the company well during this unprecedented downturn.

即使在危机发生期间,康明斯仍然继续投资于诸如氢燃料电池和电池电力平台这样的低和无碳技术,在更正常的条件和需求恢复的情况下,将为公司的未来提供良好的定位。

"在我们100年的历史中,我们遇到了一些不可预见的危机和经济挑战," Linebarger 在虚拟会议上说,这是此次大流行的另一项原因。"我深信,我们将成功地实现这一目标,正如我们之前所做的那样,并在公司中变得更强大."

他还对公司的历史表示了同样的了解,康明斯员工已经应对 COVID-19 提出的挑战,以新的和创造性的方式响应,以帮助公司和他们生活和工作的社区。

员工参与了一系列活动,从 帮助日托中心 和医院计划为 COVID-19,为世界各地的急救医疗中心提供重要的食品和药品运输服务,建造和维修发电机,以及 与其他公司合作 ,以增加个人防护设备的生产。

"我们的世界各地的员工都以创新的方式加强并响应社区的需求,这对您来说不足为奇." Linebarger 表示。"...一如既往,我们的员工和我们的公司正在竭尽所能,以新的和创新的方式解决这场危机,我们将继续致力于为更繁荣的世界提供动力. "
 

布莱尔克拉夫林可持续发展通信总监

布莱尔克拉夫林

布莱尔. 克拉夫林是康明斯公司可持续发展通信署署长,于2008年加入了该公司,成为多元化通信总监。布莱尔出身于报纸背景。此前,他曾为印第安纳波利斯球星(2002-2008)和得梅因注册(1997-2002)工作。[电子邮件受保护].com

 

团队通过康明斯的独创性来保存测试

康明斯团队必须快速了解如何在实践所有 COVID-19 保障措施的同时保持测试的顺利进行。
康明斯团队必须快速了解如何在实践所有 COVID-19 保障措施的同时保持测试的顺利进行。

车载诊断性失火测试的复杂性正如其名称所暗示的那样复杂。保持最近的测试进展可能更加复杂。

劳动密集型测试需要驾驶员和技师并排坐在 "现实生活" 环境下测试发动机,以向监管机构证明其车载诊断能够检测到因组件故障而产生的过量排放而导致的失火。测试对于保持监管流程在2021年的发动机型号上向前迈进至关重要。

测试在几个小时后在一所大学进行,在关键时刻,学校突然不得不关闭实验室,作为对 COVID-19 危机的回应的一部分。由于康明斯团队迅速制定了将测试转移回印第安纳州哥伦布市的计划,测试团队组长亚历克斯. 马林. 克鲁兹也正在制订计划,以便在奥林匹亚大厦(OLY)完成关键测试-这一次,同时保持所有建议的 COVID-19 保障措施,包括六英尺的社会疏远规则。

寻找他们的内在马盖先

在全球快速流行的大流行病引起的所有其他个人和专业压力中,来自 OLY 和康明斯技术中心(反恐委员会)的工程师和技师团队迅速集思广益了安全解决方案。

他们从在反恐委员会和 OLY 的很少使用的储藏柜中提取了超过50英尺的以太网和专用电缆。在一段时间内未使用的双程收音机被掸去。测试稍有重新配置,因此驾驶员和技师不必再坐在一起,但仍然可以使用无线电进行通信。

该团队仅在48小时内输掉,但测试已准备好继续进行。

测试的视图。
该团队发现了电缆和双向收音机,但在一段时间内并没有使用,以保持测试的顺利进行。

毫不怀疑

"我们从来没有任何疑问," 马林克鲁斯说,当被问及他是否曾认为,测试将不得不推迟。"我们只是专注于安全,并让我们相距六英尺."

他们现已走上正轨,在监管机构的最后期限内向加州空气资源委员会(CARB)提交数据,作为认证计划的一部分。他们为保持发动机在轨道上的测试而做出的非凡努力可能对保持项目向前迈进至关重要。

除了克鲁兹之外,团队成员还包括谢莉 Knust、生硬 Barnhart、贾斯汀. 欧文、Ansh 夏尔马、Michael、Shashank 夏尔马、内斯·阿莫林戈麦斯、David L 亚当斯、阿伦法则 D Sundaravel、丹尼尔赫勒和罗伯特. 琼斯。

他们再次展示了公司的团队合作价值以及其为客户进行创新的愿景,无论在康明斯还是在他们身上都是鲜活而出色的。即使是在全球大流行期间
 

康明斯办公大楼

康明斯公司

Cummins is a global power leader that designs, manufactures, sells and services diesel and alternative fuel engines from 2.8 to 95 liters, diesel and alternative-fueled electrical generator sets from 2.5 to 3,500 kW, as well as related components and technology. Cummins serves its customers through its network of 600 company-owned and independent distributor facilities and more than 7,200 dealer locations in over 190 countries and territories.

三项荣誉体现了康明斯对可持续发展的承诺

长期以来,康明斯一直认为,各种因素决定了公司的可持续性。
长期以来,康明斯一直认为,各种因素决定了公司的可持续性。

康明斯在道德、环境弹性和供应商多元化方面的工作最近获得了三年的荣誉。

The recognition reflects the company’s broad approach to sustainability, including everything from Cummins’ efforts to shrink its environmental impact to corporate responsibility, health and safety, diversity and inclusion, financial success, innovation and governance and ethics. The company, which celebrated its 100th anniversary in 2019, is committed to staying in business for the next 100 years.

“When we initiated the World’s Most Ethical Companies recognition in 2007, the concept of companies proactively aligning profits and purpose seemed unlikely,” said Ethisphere CEO Timothy Erblich, upon announcing the group’s list, which Cummins made for a 13th consecutive year. “However, leading CEOs and organizations continue to prove our long-held hypothesis that conducting ethnical business is the key to maximizing profits.”

世界上最具道德的公司

Ethisphere is  the global leader in defining and advancing standards of ethical business practices. It said 132 honorees representing 51 countries and 21 industries were included in the group’s 14th annual recognition. There were 14 newcomers to the 2020 World’s Most Ethical Companies list, while seven companies have received the designation every year since the list was first announced in 2007.

为了获得指定资格,公司必须填写有关其业务实践的全面调查。大多数调查问题涉及道德和合规性,但也有关于公司的环境性能、社区参与以及供应链参与和监督的问题。

共有历来在财务上表现出其他公司的业绩,展示了在市场上备受重视的良好道德实践与绩效之间的联系。2020榜单上的其他公司包括埃森哲、通用汽车、微软和废物管理。

印第安纳州韧性英雄徽标
贯穿复原研究所已准备了 视频 ,以庆祝2020英雄。

印第安纳州韧性英雄

康明斯已被任命为环境复原研究所的 印第安纳州复原英雄 列表,该名单表彰印第安纳州各地的个人和团体为应对气候变化和促进安全、健康社区而做出的努力。该研究所隶属于印第安纳州立大学。

"我们影响我们的环境,我们的环境影响我们," 研究所的主任珍妮特麦凯布说。"无论是冠状病毒、气候变化还是玉米产量,我们都生活在互联系统中。我们对这些联系的了解越多,我们就越能适应保护我们的健康、社区和经济的能力。

总部位于印第安纳州的康明斯因其 PLANET2050 环境可持续性战略 而获得认可,旨在降低公司对环境的影响。该战略于2019年发布,包括以科学为基础的目标,时间为2030,期望达到2050。康明斯是2020个英雄中唯一的一家公司。

这是学院第二年发布的一份名单。该研究所的使命是通过准确预测影响并有效地与社区合作以实施 "可行、公平和研究信息的解决方案",提高印第安纳州和中西部环境变化的适应能力。

供应商多元化与包容性

康明斯被评为 " 全球供应商多元化与 包容性国际冠军" ,该产品旨在表彰领导全球范围内的采购工作的公司。这一认可来自三个团体:美国泛亚商会、全国同性恋商会、残疾人士: in、全球领先的商业残疾资源的非营利组织和 WEConnect 国际,这是一个将女性拥有的企业与世界各地的合格买家联系在一起的全球性网络。

康明斯仅在凯利服务、奔驰和 IBM 的合作伙伴名单上完成了4号。

WEConnect 国际首席执行官兼创始人伊丽莎白. 巴斯克斯表示: "如果您在任何业务领域都不提供资源,那么您就无法充分获得关键的创新和最佳的总价值选择,从而帮助您满足和预测客户的需求.""这一排名展示了对供应商多元化和包容性的真正全球运动的加速."
 

布莱尔克拉夫林可持续发展通信总监

布莱尔克拉夫林

布莱尔. 克拉夫林是康明斯公司可持续发展通信署署长,于2008年加入了该公司,成为多元化通信总监。布莱尔出身于报纸背景。此前,他曾为印第安纳波利斯球星(2002-2008)和得梅因注册(1997-2002)工作。[电子邮件受保护]

 

正在重定向到
cummins.com

您正在查找的信息位于
cummins.com

我们正在为您启动该网站。

谢谢。