Versatile Yard: Versatile Boats

by

Cummins Vessel Reference #645

Ready for work.

 

The marine works and dredging company LMD recently took delivery of a general cargo and heavy lift vessel from the prolific and versatile Italian shipyard Vittoria di Adria. At 60 meters in length with a 16-meter beam and a weight of 2300 gross tons the Alfredo is a hefty vessel designed for maximum productivity. As a bulk cargo vessel she can pack up to 1600 tons in her large 36X16-meter hold. She can load and off-load with her deck-mounted Sennebogen 6180 crane capable of lifting 200 tonnes with its 33 metre jib.

 

 

 

Cummins KTA50 M2

 

A big complex working vessel such as this needs big power and the Alfredo has it. A pair of Cummins KTA50 M2 engines each delivering 1600 HP at 1800 RPM provides the main propulsion. The two engines have separate engine rooms separated by a watertight bulkhead for safety. In addition to the two main engines, the Alfredo has six additional Cummins engines. These include two 6CTA8.3 generator set engines, two QSM11 DM to provide power for the vessel’s bow and stern thrusters, one 6BT DM for the emergency gen set and, for power in the crane, a Cummins QSK23 C. All engines, except that of the crane, were supplied by Sea Italia.

 

Images courtesy of Cummins Marine

 

For further information:

Fabio Duo
Managing Director
Shipyard Vittoria
Via L. Da Vinci, 47
45011 Adria (Rovigo)
Phone: 39 0426 900467
Fax: 39 0426 41741
E-mail: [email protected]
Web: www.vittoria.biz

Sjoerd Spronck
Communications & Media Coordinator – Europe
Cummins Distribution Europe
Cummins Holland B.V.
Olivijn 800m 3316 AM Dordrecht
Netherlands
Phone: 31 0 78 653 0927
Cell: 31 0 6 110 11 075
Email: [email protected]

Alan Haig-Brown

Alan Haig-Brown

Over 30 years as an author for global commercial marine and fishing publications backed with hands-on experience on commercial fishing boats and coastal freighters makes Alan Haig-Brown uniquely qualified to provide vessel reference articles for Cummins Marine. You can find him in shipyards around the world, and on his own website, www.haigbrown.com.

Redirecting to
cummins.com

The information you are looking for is on
cummins.com

We are launching that site for you now.

Thank you.