Survey Vessel from Sibu Malaysia Yard

by

Cummins Vessel Reference #615

Sea trials

A recent delivery from the yard of Eastern Marine Shipbuilding in Sibu, East Malaysia is a further indication of the growing technical sophistication of the Sarawak yards. The 60 by 16-meter Offshore Surveyor is designed by Wartsila Ship Design of Singapore. To do her survey work the Malaysian-registered vessel is fitted with 2.4-meter-square moon pool as well as a deck crane from Marine Equipment of Singapore. The crane has a telescoping boom that can lift up to five tons when extended eight meters. The same supplier also provided the anchor and mooring winch as well as a six-ton capstan. www.mequip.biz/



Main engines are a pair of Cummins QSK60M diesels generation 2200 HP each at 1800 RPM and turning into Hitachi Nico Model MCR1727VC(CPP gears) with 7.5:1 ratios. The controllable pitch propellers are a pair of Berg BCP HDX690. Side thrusters on the dynamic positioning vessel is also CPP and they are supplied by the Japanese firm Kamome. The steering system is by the Singapore firm Palmarine, model PEH5202. www.palmarine.com

To meet the advanced electrical demands of such a vessel the main shafts are fitted with 700 kW Stamford generators. Additional electrical supply is derived from a pair of Cummins QSK11-DM powered 250 kW gensets. The 80kW emergency genset is powered by a Cummins 6BT engine.

The Offshore Surveyor, with a 1,672 GRT and a 501 NRT, has tankage equal to 441 cubic meters for ballast water, 505 m3 of fresh water, 422 m3 of fuel, 387 m3 of drilling mud and 142 m3 base oil. Accommodation is provided for up to 46 people.

Photos courtesy of Eastern Marine Shipbuilding

For more information:

Ngieng Ping Huo
Eastern Marine Shipbuilding Sdn. Bhd.
No. 20, Ground Floor
Lorong Wong Ting Hock 1,
9600 Sibu,
Sarawak, Malaysia
Phone: 084 21 8866
E-mail: [email protected]

Steven Yii Chuk Lik
Scott & English (Malaysia)
Sdn. Bhd. No. 6A, Long 39
Jalan King Kik Kwong
96000 Sibu, Sarawak
Phone: 084 31 8107
Fax: 084 33 6001
E-mail: [email protected]
Web: www.sne.com.my/contactsibu.asp

Alan Haig-Brown

Alan Haig-Brown

Over 30 years as an author for global commercial marine and fishing publications backed with hands-on experience on commercial fishing boats and coastal freighters makes Alan Haig-Brown uniquely qualified to provide vessel reference articles for Cummins Marine. You can find him in shipyards around the world, and on his own website, www.haigbrown.com.

Redirecting to
cummins.com

The information you are looking for is on
cummins.com

We are launching that site for you now.

Thank you.