Powerful Shallow-Draft Paraguay Towboat

by
The Navesur

Paraguay’s Tsuneishi Shipyard, a subsidiary of the Japanese firm of the same name, recently delivered the powerful towboat Tebicuary 3 to her owners Navegación del Sur S.A. (Navesur) in June of 2018.

The new vessel is a near sister-ship to the 2015-delivered Ceasar Primo for a different owner. The newer vessel will also work on the Paraguay-Paraná River system that provides marine access to large parts of central South America. "The Paraguay-Paraná Waterway is a regional agreement between Argentina, Bolivia, Brazil, Paraguay, and Uruguay with the aim of facilitating navigation and thus regional and international trade.

Comprising the Paraguay, Paraná, and Uruguay Rivers, at 3,442 kilometers it is one of the longest natural waterways in the world, extending from Puerto Cáceres, Brazil to Nueva Palmira, Uruguay and Buenos Aires, Argentina. Its area of influence encompasses a direct surface area of 720,000 km² and an indirect surface area of 3,500,000 km². It is one of the most essential transport routes for the geographical integration of regional trade between Mercosur and the rest of the world." [From http://navesur.com.py/en/#hidrovias]

Navesur Engine Room

At 6,400 hp, the Tebicuary 3 is more powerful than most of the towboats currently working on the river system. The power derives from four Cummins KTA50 engines, each developing 1600 hp at 1800 RPM. The boat is 43 by 18-meters with an operating draft of only 1.83 meters allowing it to push barges into most areas of the inland waterway.

In addition to the Cummins propulsion engines, the Tebicuary 3 is fitted with two Cummins Marine NTA855-powered 240 kVA / 50 hz (Total Power: 480 kVA) generator sets.  There is also a Cummins 6B CS 93 kVa / 50 Hz emergency generator set. All the engines and gen sets have Japanese NK class certificates.

With Cummins C Command electronic controls the engines will be able to maximize fuel efficiency and savings. All of this adds to the significant environmental savings by moving cargos from trucks to barges.

 

For further information:

Navesur

See also from 2015: Ceasar Primo: Global Design and Supply

Photos courtesy of Cummins Argentina, Bolivia, Paraguay y Uruguay

Gathered in the Tebicuary 3 engine room are (l to r) -Victor Vacelar, Application Analyst at Cummins, Armando Tavarozzi, HHP Sales Leader at Cummins, Marcial Yoshizaki, Commercial Manager at Tsuneishi, Claudia Kowalczuk, Marketing & Communication Leader at Cummins, Modesto Benitez, Mechanical Technician at Cummins.

María Inés Andrés
Marketing & Communication Specialist
Cummins Argentina, Bolivia, Paraguay y Uruguay
Ruta Panamericana Km. 32,5
El Talar, Buenos Aires, Argentina
Tel.: +54 11 4736 6404
Cel.: +549 11 5597 3752
cummins.com.ar
e-mail: [email protected]
www.facebook.com/CumminsPowerOficial
 
Armando Tavarozzi
HHP Sales Engines Leader
Cummins Argentina, Bolivia, Paraguay y Uruguay Ruta Panamericana Km.
32,5 El Talar, Buenos Aires, Argentina
Tel.: +54 11 4736-6428
Cel.: +54 11 3280-8713
e-mail: [email protected]
www.cummins.com.ar
marine.cummins.com
www.facebook.com/CumminsPowerOficial
 
Astillero Tsuneishi Paraguay SA
Ruta Viulleta Alberdi km 9,
Villeta, Deparamento Centra,
Paraguary
Phone: +595 21 238 1265
 
Navesur
Alkan Headquarters
Terminal occidental
Ruta 12 Km 3,5
+595(220) 758-1000
Villa Hayes, Paraguay

Featured Products
Alan Haig-Brown

Alan Haig-Brown

Over 30 years as an author for global commercial marine and fishing publications backed with hands-on experience on commercial fishing boats and coastal freighters makes Alan Haig-Brown uniquely qualified to provide vessel reference articles for Cummins Marine. You can find him in shipyards around the world, and on his own website, www.haigbrown.com.

Redirecting to
cummins.com

The information you are looking for is on
cummins.com

We are launching that site for you now.

Thank you.