Kara-Matt: Repower After Big Hours

by
kara-matt

Cummins Vessel Reference #832

 

After 60,000 hours of service, crab fisherman Robert Ross decided that his 19-liter Cummins 1150M had earned a rest. The 500 HP engine had been a perfect match for his 72 by 26-foot aluminum boat so he ordered up a new Cummins KTA19-M3 at 500 HP, continuous duty, from his local supplier Cummins Sales and Service in Fredericton, New Brunswick, in eastern Canada.

 

Ross had his well-maintained 39-year-old boat, the Kara-Matt, hauled out at a shipyard and Dugas Equipment Ltd. of Caraquet, New Brunswick took on the repower. Once on the hard, they removed the old engine through a hold cut in the port side. The old engine turned a 52X48-inch propeller on a 5.5-inch shaft through a Capital gear. The new engine turns the same size prop on the same size shaft but it is linked through a ZF W350-1 gear with a 4.536:1 ratio.

 

 

In addition to the new KTA19 main engine, he installed a pair of 65 kW Cummins-powered generators. One of these has a power takeoff for hydraulics and the other also drives the vessel’s refrigeration system.

Built in British Columbia in 1979, the aluminum boat was brought around to the east coast and is currently outfitted for the Gulf of St. Lawrence snow crab fishery. There is a crab pot hauler and a deck crane. The hold keeps the catch chilled in RSW tanks.

The repowered and refurbished boat went back in the water in December 2017 in good time for the 2018 snow crab season. The Kara-Matt is now good for another 40 years with an engine to match.

Photos courtesy of Deon Strickland/Cummins

 

For further information:

Deon Strickland
OEM Account Manager, Maritimes
Cummins Sales and Service
Frederickton, New Brunswick
Canada,
Mobile: 902 717 2647
E-Mail: [email protected]

Dugas Equipment Ltd.
80, St-Pierre Blvd. East
Caraquet, NB,
Canada, E1W 1B6
Phone: 506 727 0952
E-mail: [email protected]

Alan Haig-Brown

Alan Haig-Brown

Over 30 years as an author for global commercial marine and fishing publications backed with hands-on experience on commercial fishing boats and coastal freighters makes Alan Haig-Brown uniquely qualified to provide vessel reference articles for Cummins Marine. You can find him in shipyards around the world, and on his own website, www.haigbrown.com.

Redirecting to
cummins.com

The information you are looking for is on
cummins.com

We are launching that site for you now.

Thank you.