Cummins helps expand a major water treatment plant

by
Water treatment facility

Overview

Challenge: Provide an emergency standby power system solution that would support the expansion of the water treatment plant in Oman approximately doubling capacity from 57,000 to 125,000 m3/ day for the treatment plant and from 130,000 to 260,000 m3/day for the pumping station using a “single-window system” capability.
Cummins Solution: Cummins delivered a 14.5 MVA emergency standby power solution based around five new generator sets – including the first in the country to be powered by the QSK95 Series engine. The Treated Effluent Substation has a C2500 D5A, 6.6 kV generator set. Two C3500 D5, 6.6 kV units serve the biological treatment plant, and the central pumping station is equipped with two C2500 D5A, 415 V units.
Result: All products had to be delivered in approximately six months after approvals, to support the customers’ deployment schedule for the Haya Water plant. The Cummins units were delivered to site, according to the committed schedule, in 2016. Global presence, single-source supply, ability to meet the delivery timeframe, and a single-window capability all proved crucial in placing responsibility for the project with Cummins.

Major sewage treatment center poised for upgrade, doubling capacity

Haya Water is the organization responsible for the implementation and operation of sewage treatment facilities throughout the state of Oman. Amongst these is a major site at Al Ansab near the capital Muscat. The expansion of the site would approximately double capacity from 57,000 to 125,000 m3/ day for the treatment plant and from 130,000 to 260,000 m3/day for the pumping station.

On completion, Al Ansab would become one of the largest facilities in the world to use the flat-sheet-membrane bioreactor process, which produces high-quality reclaimed water and minimises environmental footprint. It would become the biggest water treatment plant in Muscat, capable of producing more than 100,000 m3 of high purity reusable water per day, and it would provide Oman’s capital with one third of its total irrigation requirements for landscaping and beautification up to the year 2025.

Five new generator sets, one impressive 14.5 MVA emergency standby power solution

Oman Color Generator.PNG

To cope with the expansion, Cummins distributor Universal Engineering Services LLC delivered a 14.5 MVA emergency standby power solution based around five new generator sets – including the first in the country to be powered by the QSK95 Series engine. The Treated Effluent Substation has a C2500 D5A, 6.6 kV generator set. Two C3500 D5, 6.6 kV units serve the biological treatment plant, and the central pumping station is equipped with two C2500 D5A, 415 V units. Universal Engineering Services also supplied attenuators, bulk fuel tanks, piping, ventilation system and Neutral Grounding Resistors (NGRs).

Cummins was the right partner to support international requirements

Cummins won the contract thanks to a wide range of factors, including relevant prior experience in Oman and a strong presence in Korea, home of main contractor Doosan Heavy Industries & Construction.

One of the main contractor’s fundamental requirements was the use of a “single-window system”, an internationally recognized trade facilitation concept. Under a single-window system, everyone involved in an international project is required to file standardized information and documents at a single point, to streamline all of the project’s import, export and transit related regulatory requirements. Universal Engineering Services (UES) with the support of Cummins Project Design & Implementation (PD&I) team was able to meet this requirement better than the competition.

Global support, reputation and footprint paved the way to Cummins success

The PD&I team provided expertise throughout the project on several issues: remote radiators for the generators, exhaust silencers, flexible ducting, battery charger selection and supply for the QSK95 units and neutral grounding panels for the medium voltage generators.

Oman Color Generator 2.PNG

Cummins took advantage of its global capabilities, reputation and footprint to deliver the winning solution. UES took the leading role by virtue of its local presence in Oman, its track record of similar projects in the country, and its demonstrated turnkey project capability. The Cummins PD&I team provided technical support, and Cummins in the UK ensured good price support and assistance with deliveries.

After AECOM was selected as design consultant in 2013, the Al Ansab expansion project was a four-year journey. Doosan Heavy Industries & Construction won their contract in June 2015 and in December 2015 they awarded the generator set order to Universal Engineering Services. Cummins was able to meet the aggressive project delivery timeline. All the products had to be delivered in approximately six months after approvals, to support the customers’ deployment schedule for the Haya Water plant. The Cummins units were delivered to site, according to the committed schedule, in 2016. Global presence, single-source supply, ability to meet the delivery timeframe, and a single-window capability all proved crucial in placing responsibility for the project with Cummins.

For more information about critical protection/standby power systems or other energy solutions, contact your local Cummins distributor or visit power.cummins.com.

Cummins Office Building

Cummins Inc.

Cummins, a global power technology leader, is a corporation of complementary business segments that design, manufacture, distribute and service a broad portfolio of power solutions. The company’s products range from internal combustion, electric and hybrid integrated power solutions and components including filtration, aftertreatment, turbochargers, fuel systems, controls systems, air handling systems, automated transmissions, electric power generation systems, microgrid controls, batteries, electrolyzers and fuel cell products.

Redirecting to
cummins.com

The information you are looking for is on
cummins.com

We are launching that site for you now.

Thank you.