Bahtera Bahari Shipyard: The Next Generation

by

Cummins Vessel Reference #621

New tug and barge at the Bahtera Bahari Shipyard.

As with many businesses in Southeast Asia, the Bahtera Bahari Shipyard on Indonesia’s Batam Island is a family business. Although the present company was founded only recently, in 2005, the family’s association with the marine world of Indonesia extends back several decades.

One of four children Ms. Tresya, the oldest of two sisters, has completed her training in project management in Australia. She is now a director of the company and involved in marketing and bringing modern management models to the shipyard as well as an extensive network of inter-related companies. She recently gave a very brief account of the company’s history.


Ms. Tresya and Mr. Rudiyanto with a new-build from the Bahtera Bahari Shipyard.

Her father, Hengky Suryawan, who was born in 1949, began a small ferry company on Bintan Island in the 1980s. As this expanded he learned that transporting inanimate cargo such as logs and coal was a more profitable and much more straight forward. The logistics of arranging cargos let to the development of a shipping company of tugs and barges. This, in turn, led to the acquisition of a quarry and then coal and iron oar mining properties. What began as a company repair yard has morphed into a full shipyard doing new construction of landing craft, tugs and barges.

Now as the four children come of age they are moving into the management of the group of companies. Having grown up around boats and shipyards they are able to apply their overseas educations in a pragmatic fashion that is leading to a stronger fusion of traditional and modern technologies and management. Both Ms. Tresya’s brothers, Selamat Budiman and Selamet Widodo, are directors of the shipping building yard and the shipping arm while a brother-in-law, Mr. Rudiyanto, is the President Director of the Shipyard.

On a recent visit to the yard on Batam Island, Ms. Tresya showed visitors around the yard and toured a recently launched tug, one of three 29 by 8-meter boats moored to a cluster of new barges. The Marina 30 identifies as one of the boats belonging to the family’s extensive fleet all of which are named Marina.

The clean and simple navigation console on the Marina 30.

This class of vessel is a good-sized 29 by 8-meter tug with a 3.7-meter molded depth. The functional and roomy wheelhouse has dual sets of engine controls, one each of the port and starboard main engines. The uncluttered control panel included remote starts for the generator sets, a rudder indicator, compass, VHF and SSB radios, a radar, a GPS and echo sounder.


The port side Cummins KTA38-M2 with the Masson Marine gear.

Two decks down, the functionality is repeated in the engine room. The two big Cummins KTA38-M2 diesels, each generating 1200 HP at 1800 RPM, turn into Masson Marine W5200 gears with 5.955:1 reductions. Electrical services are met with a single Cummins 4BT3.9-GI powered 50 kW generator.

The air-conditioned accommodation area includes a comfortable lounge/mess area with a separate compact galley on the port side. On the tug’s bow an electric-powered anchor winch provides a maximum torque of two tons. On the after deck a 40-ton towing hook is mounted just aft of the main cabin.

The Marina 30 has joined the company fleet providing charter services but also moving coal, iron oar and aggregate from the family’s other operations.

Haig-Brown photos courtesy of Cummins Marine

For further information:

Selamat Budiman (Group Director)or Ms. Tresya (Director)
Bahtera Bahari Shipyard
200 Jalan Sultan
#15-06 Textile Centre
Singapore, 199018
Phone: 65 6296 2292
Singapore Mobile: 65 9639 1050
Indonesia Mobile: 62 855 655 0000
E-mail: [email protected]

Mr. Budiyanto
Branch Manager
PT. Altrack 1978
Kompek Inti Batam Business & Industrail Park
Blok A No. 3A
Sei Panas
Batam
Phone: 0778 432412
Mobile: 62 812 7024 795
E-mail: [email protected] 1978.co.id

Alan Haig-Brown

Alan Haig-Brown

Over 30 years as an author for global commercial marine and fishing publications backed with hands-on experience on commercial fishing boats and coastal freighters makes Alan Haig-Brown uniquely qualified to provide vessel reference articles for Cummins Marine. You can find him in shipyards around the world, and on his own website, www.haigbrown.com.

Redirecting to
cummins.com

The information you are looking for is on
cummins.com

We are launching that site for you now.

Thank you.