Chat with Support

INSITE™ is a Microsoft Windows based electronic service diagnostic program that allows you to troubleshoot Cummins electronic engines.

Software Downloads

The latest version of INSITE is version 8.4.0

Compatible with Windows 7, Windows 8.X, Windows 10

Release Information

PC System Requirements

 

Software Installation: Where to Start Instructions (Size: 5 MB)

Software Update: Where to Start Instructions (Size: 5 MB)

Please note: These instructions are the same for any version of INSITE 8.X and greater. The screenshots are just examples of the software used to build these instructions.

DOWNLOAD  (Size: 1.9 GB)

This file can be downloaded to create a copy of the INSITE DVD and requires DVD creator software or a utility that supports .iso images.

Installation Instructions:

  1. Click the Download button above.
  2. On the next File Download window that appears, click Save and choose a location to save the download.
  3. At this point, you can either burn the ISO to a DVD with Windows 7/8 or some other ISO burning software. (Roxio, Burn-it, etc.)

Note: If you are running Windows 8 or greater you can mount the ISO as a virtual DVD player by right clicking on the file and choosing "Mount" or "Open With..." and choosing "Windows Explorer."

How to Create DVD from ISO Instructions

This Image Contains:

DOWNLOAD  (Size: 1.9 Gb)

Installation Instructions:

Note: Once extracted into C:\Temp, INSITE software requires administrative rights to install. Right-click on BAT File and choose Run as Admin. Alternatively, to install via Update Manager, once extracted into C:\Temp, choose Source > Browse and select the folder where you extracted the Update Manager.

Installation Demonstration Videos:

This ZIP Contains:

  • INSITE™ 8.4.0
  • Cummins Update Manager 6.2
  • License Configuration Tool 1.10.2
  • INSITE Guidanz Service

Release Notes

DOWNLOAD  (Size: 1.7 GB)

Installation Instructions:

This software is not available on mobile. To download for your office or home computer, please return to this page from that device.

Software Licensing

Some Cummins software and mobile applications – including INSITE™, Guidanz™, PowerSpec and QuickCheck – require unique software licenses for use. Licenses are available through a Cummins-authorized distributor or dealer. Please provide us a few details to find your local representative.

Issues and Solutions

Cause:

Malwarebytes or other Anti-Malware software has flagged LCT.exe and other related files or registry keys as malware.

Tools Affected:

  • INSITE 8.X.X and above

Operating Systems Affected:

  • Microsoft Windows 7
  • Microsoft Windows 8.X

How to Fix:

Malwarebytes has been found to cause this problem most often if out of date. So we provided the steps for how to correct this problem based off of this. Other software should have similar steps to create exclusions. See the respective software’s help for more details.

  1. Open MalwareBytes Anti-Malware. If Malwarebytes isn’t installed, please contact INSITE Help Desk.
  2. Click on History at top (A), then ensure you are in the Quarantine (B).
  3.  Locate entry for LCT.exe (C). Please search for any other entries that have “Cummins”.
    • 32-bit Windows – “C:\Program Files\Cummins Inc”
    • 64-bit Windows – “C:\Program Files (x86)\Cummins Inc”
  4. Select any checkbox for entries (D). If there are no entries, please contact INSITE Help Desk.
  5. Click Restore (E).
  6. Click on Settings (F).
  7. Select Malware Exclusions (G).
  8. Click to Add Folder (H).
  9. Locate the Cummins Inc folder and click on “Select Folder”.
    • 32-bit Windows - “C:\Program Files\Cummins Inc”
    • 64-bit Windows – “C:\Program Files (x86)\Cummins Inc”
  10. Click on Dashboard (J).

  11. Update Database (K). Once everything is updated, you should see “Your system is fully protected” and the green check showing your database is up to date (L).
  12. You should now be able to open INSITE. Please ensure your Cummins INSITE software is up to date (currentversion information is below) and run Update Manager as necessary.

Current versions:

  • INSITE: 8.0.2.148
  • License Configuration Tool (LCT): 1.8
  • Tool Licensing Service: 11.12.0.2

Cause:

Licenses are missing because INSITE and/or the Cummins Inc. License Configuration Tool and are not up to date.

How to Fix:

To resolve the issue 3009 error, run the Cummins Inc. Update Manager while connected to the internet. Run Update Manager shortcut, click the green buttons with the arrows which is Refresh Updates then click the blue button which is Install Updates. (If there is a message asking to update the Update Manager, click OK.) Install all INSITE and License Configuration Tool updates until INSITE is at least at 8.0.2 and the License Configuration Tool is at least at 1.3.0.5

If Cummins Inc. Update Manager is not installed, it can be downloaded from the INSITE website (https://insite.cummins.com/insite/info/updatemanagerdl.html)

The License Configuration Tool needs to be able to access the license server which is located at oms.cummins.com via port 443. If that server is inaccessible, then the INSITE license(s) cannot be activated or transferred.

If there is not a shortcut to Cummins Inc. Update Manager on the desktop then go to the following location right click on the UpdateManger.exe file and click Send to Desktop (create shortcut).

C:\Windows\Programs Files(x86)\Cummins Inc\UpdateManager\UpdateManager.exe

If the problem is still present after this, please call your local INSITE help desk or email [email protected] for remote assistance to resolve this issue.

Tools Affected:

  • INSITE 8.X.X and above
  • License Configuration Tool
  • Cummins Inc. Update Manager

Operating Systems Affected:

  • Microsoft Windows 7
  • Microsoft Windows 8.X

Cause:

Corrupted Microsoft Access Database Engine 2007, OR a corrupted INSITE datapack.

How to Fix:

If Microsoft Access Database Engine 2007 is already corrupted, install the 32-bit or 64-bit version, depending on the version of Office you are running, of the Microsoft Access Database Engine 2010 which you can download from the web. Make sure the 32-bit version is installed regardless whether customer has a 32-bit or 64-bit operating system. There is no requirement to uninstall the 2007 Database Engine, as the two can co-exist without issue.

Microsoft Access Database Engine 2007 install file can be found on the INSITE 8.0 DVD in the following folder:

\UpdateManager\INSITE\ISSetupPrerequisites\{D5B36ED1-A330-46D8-9F0A-73EA86CEB71A}

Note: Is replaced with the drive letter (D: E:, F: etc) that represents your DVD-rom drive that the INSITE 8.0.0 DVD is located

If substituting the Microsoft Access Database Engine 2010 does not correct the issue, then the issue is caused by a corrupt datapack, which will need to be replaced. Uninstall the existing datapack via add/remove programs, then transfer a copy of the datapack setup file to the customer’s pc. The setup file is in the prerequisites folder:

- INSITE

ISSetupPrerequisites

{E8EA9808-4F2D-4C28-A517-C12569C12D6D}

INSITE Data Pack

Tools Affected:

• INSITE 8.X.X and above

Operating Systems Affected:

  • Microsoft Windows 7
  • Microsoft Windows 8.X
  • Windows 10

Cause:

Missing or Corrupt Microsoft Access Database Engine 2007 install.

How to Fix:

To resolve the issue 50616/50628 error:

Verify if Microsoft Access Database Engine 2007 or 2010 is installed on PC.

If neither is installed, install the Microsoft Access Database Engine 2007 from the INSITE 8.0 DVD (3rd package) or download it from the web.

If Microsoft Access Database Engine 2007 is already installed, install the 32-bit version of the Microsoft Access Database Engine 2010 which you can download from the web.

Make sure the 32-bit version is installed regardless whether customer has a 32-bit or 64-bit operating system.

Microsoft Access Database Engine:

MS Access Engine 2007

32-Bit & 64-Bit Version (x86) & (x64)

MS Access Engine 2010

32-Bit Version (x86)

64-Bit Version (x64)

MS Access Engine 2013

32-Bit Version (x86)

64-Bit Version (x64)

Cause:

Cummins Update Manager doesn't install both required parts of a INSITE install. This is most commonly caused by a install error 1603 for the INSITE Base install. INSITE Base Install and INSITE Datapack must both be alligned to the proper versions for normal INSITE operation.

How to Fix:

NOTE: Administrative rights are required to perform this fix.

  1. Open Control Panel in Windows
  2. Select "Programs and Features"
  3. Select "View Installed Updates"
  4. Find INSITE and INSITE Datapack
  5. Uninstall the mismatched version of the file. (e.g. The install with the highest version. For the example above you would uninstall INSITE 8.0.2 DP1 as it's higher than INSITE 8.0.1.291)
  6. Close the Control Panel
  7. Open Cummins Update Manager
  8. Select the visible version of INSITE and reinstall the update.
  9. Monitor the update to make sure both the Datapack and Base build installs with no errors. (If the INSITE and/or the Datapack errors again on the update.. Please uninstall INSITE and the Datapack and install it fresh to clear errors.)
  10. Launch INSITE to confirm error has been cleared.

Manual Installs for Missing Datapacks:

 

INSITE 8.2.X

INSITE 8.2.0 Datapack Size: 26 Mb

INSITE 8.2.0 Datapack 1 Size: 23 Mb

INSITE 8.2.1 Datapack Size: 27 Mb

INSITE 8.2.2 Datapack Size: 27 Mb

 

INSITE 8.3.X

INSITE 8.3.0 Datapack Size: 27 Mb

INSITE 8.3.1 Datapack Size: 27.7 Mb

 

INSITE 8.4.X

INSITE 8.4.0 Datapack Size: 28 Mb

Questions and Answers

INSITE is a Microsoft Windows based electronic service diagnostic program that allows you to troubleshoot Cummins electronic engines.

Visit https://insite.cummins.com or contact your local Cummins Distributor or Cummins Authorized Dealer for more information about INSITE.

Please contact your local Cummins distributor or Cummins authorized dealer to find out which product best suits your application and for INSITE pricing.

Visit the downloads section of this website for the latest release information or contact your local Cummins distributor or Cummins authorized dealer.

To find out what version you are currently using open INSITE and go to Help > About INSITE.

Additional functionality, which could include support for newer engines and/or general software updates.

Please review the INSITE Release Notes and the New INSITE Features documents from the installation CD or on the web site.

There is a Virtual College CD developed by Cummins for INSITE. This CD contains Virtual Classroom Training, Written Assessment and Virtual Hands-On Assessment. Please contact your local Cummins Distributor or Cummins Authorized Dealer for more information. An INSITE Overview Presentation is also available on INSITE CD.

Training Videos

Training Materials

Contact Cummins Care

For general inquiries or questions regarding your Cummins product, please use the form below, or call us anytime.

Reach Us By Phone

USA: 1-800-CUMMINS™ (1-800-286-6467)
USA: 1-800-CUMMINS™ (1-800-286-6467)
Albania: +44 (0) 1327 886464
Andorra: +44 (0) 1327 886464
Argentina: 0800 12 26 467
Armenia: +44 (0) 1327 886464
Australia: 1-300-CUMMINS (1 300 2866467)
Austria: +44 (0) 1327 886464
Azerbaijan: +44 (0) 1327 886464
Belarus: +44 (0) 1327 886464
Belgium: +44 (0) 1327 886464
Bolivia: 800 10 18 73
Bosnia and Herzegovina: +44 (0) 1327 886464
Brazil: 0-800-CUMMINS (0 800 2866467)
Bulgaria: +44 (0) 1327 886464
Canada: 1-800-CUMMINS™ (1-800-286-6467)
China: (+86) 400 810 5252
Colombia: 01 800 75 22 501
Costa Rica: 41003-1600, option 6
Croatia: +44 (0) 1327 886464
Czech Republic: +44 (0) 1327 886464
Denmark: +44 (0) 1327 886464
El Salvador: 2555-4000, option 6
Estonia: +44 (0) 1327 886464
Finland: +44 (0) 1327 886464
France: 00-8000-CUMMINS (00 8000 286 6467)
Georgia: +44 (0) 1327 886464
Germany: 00-8000-CUMMINS (00 8000 286 6467)
Greece: +44 (0) 1327 886464
Honduras: 2202–5600, option 6
Hungary: +44 (0) 1327 886464
Iceland: +8000-CUMMINS (+8000 286 6467)
India: 1 800 210 2525
Ireland: 00-8000-CUMMINS (00 8000 286 6467)
Italy: +44 (0) 1327 886464
Kazakhstan: +44 (0) 1327 886464
Latvia: +44 (0) 1327 886464
Liechtenstein: +44 (0) 1327 886464
Lithuania: +44 (0) 1327 886464
Luxembourg: +44 (0) 1327 886464
Macedonia: +44 (0) 1327 886464
Malta: +44 (0) 1327 886464
Mexico: 01-800-CUMMINS (01 800 286 6467)
Moldova: +44 (0) 1327 886464
Monaco: +44 (0) 1327 886464
Montenegro: +44 (0) 1327 886464
Netherlands: 00-8000-CUMMINS (00 8000 286 6467)
New Zealand: 0-800-CUMMINS (0 800 286 6467)
Norway: +8000-CUMMINS (+8000 286 6467)
Panama: 377–9000, option 6
Paraguay: 009 800 521 0101
Poland: +44 (0) 1327 886464
Portugal: +44 (0) 1327 886464
Romania: +44 (0) 1327 886464
Russia: +44 (0) 1327 886464
San Marino: +44 (0) 1327 886464
Serbia: +44 (0) 1327 886464
Slovakia: +44 (0) 1327 886464
Slovenia: +44 (0) 1327 886464
Spain: +44 (0) 1327 886464
Sweden: +8000-CUMMINS (+8000 286 6467)
Switzerland: +44 (0) 1327 886464
Turkey: +44 (0) 1327 886464
United Kingdom: 00-8000-CUMMINS (00 8000 286 6467)
Uruguay: 00 04 05 29 66 23
Vatican City: +44 (0) 1327 886464
If your country is not listed, please contact us using the “Send Us Your Request” form.
Cummins Care representative

Send Us Your Request

A Cummins Care team member will respond to your request within 48 hours.

I am a
I am a *
Need help finding a Cummins Certified Service Provider or Parts Support? Click here
Redirecting to
cummins.com

The information you are looking for is on
cummins.com

We are launching that site for you now.

Thank you.