Chat with Support

Our datalink adapters are designed for use with GuidanzTM and allow communication with the on-board Electronic Control Module (ECM) for vehicle subsystems (e.g. Engine, Transmission, Brake Systems).

For more information, or to purchase Cummins datalink adapters, visit CumminsEngines.com/INLINE, contact your local Cummins Distributor or call 1-800-646-5609.

Software Downloads

INLINE 5 (32-bit) Download
File Name: I5DriverSetup321.zip (Size: 15.0 MB)
DOWNLOAD

INLINE 5 (64-bit) Download
File Name: I5DriverSetup641.zip (Size: 19.7 MB)
DOWNLOAD

Note that if you have an INLINE 5 or INLINE 4 adapter, you must install the proper INLINE 5 PC Driver that is included in this software. The INLINE 5 Software installation is a typical Windows-based, self-executing installation. Version 5.6.5.4 of the executable setup file installs the latest released INLINE 5 PC Driver, which allows RP1210-compatible software applications to communicate with the INLINE 5 adapter. The latest version of the reflash utility and version 5.46 of the firmware are also included in this download and will be installed automatically in their proper folders in your PC when you run the install program, as described below. Note that if you have issues with a DEF gauge, you should use Driver Version 5.7.0.1, which has version 5.47 of the firmware.

Installation Instructions:

  1. Download the appropriate INLINE 5 zip file by clicking on a link above (note that unless you have a 64-bit Operating System, you should use the 32-bit file).
  2. Unzip and extract the executable file using zip/unzip software.
  3. Click on the Windows Start menu and click Run.
  4. Click on the Browse button and locate the files you have downloaded. (Use version 5.6.5.4, unless you have DEF gauge problems, in which case you should use 5.7.0.1).
  5. Click the OK button to install the correct INLINE 5 Driver, reflash utility, and firmware on your PC.
  6. Follow the onscreen instructions to complete the installation.
  7. Connect +8 V to +50 V power to your INLINE 5 adapter through the DB25 cable you have.
  8. Use your DB9F to DB9M serial cable or USB cable to connect the INLINE 5 adapter to the proper PC communication port.
  9. Follow the Driver Installation and other instructions located on the On-line Manuals page.

Additional Resources:

INLINE 6 (Part Number 2892092)

INLINE 6 (32-bit) Download
File Name: inline-6-9-00-32bit.zip (Size: 64.8 MB)
DOWNLOAD

INLINE 6 (64-bit) Download
File Name: inline-6-9-0-0-64bit.zip (Size: 64.8 MB)
DOWNLOAD

Note that if you have an INLINE 6 adapter, you must install the INLINE 6 PC Driver that is included in this software. The INLINE 6 Software installation is a typical Windows-based, self-executing installation. The executable setup file (listed below) installs the latest INLINE 6 PC Driver, which allows RP1210-compatible software applications to communicate with the INLINE 6 adapter. The latest version of the reflash utility and latest version’s firmware are also included in this download and will be installed automatically in their proper folders in your PC when you run the install program, as described below.

Reflash Instructions:

  1. Download the appropriate INLINE 6 zip file by clicking on a link above (note that unless you have a 64-bit Operating System, you should use the 32-bit file).
  2. Unzip and extract the executable file using zip/unzip software.
  3. Click on the Windows Start menu and click Run.
  4. Click on the Browse button and locate the file you have downloaded.
  5. Click the OK button to install the latest INLINE 6 Driver, reflash utility, and firmware on your PC.
  6. Follow the onscreen instructions to complete the installation.
  7. Connect +8 V to +50 V power to your INLINE 6 adapter through the DB25 cable you have.
  8. Use your DB9F to DB9M serial cable or USB cable to connect the INLINE 6 adapter to the proper PC communication port.
  9. Follow the Driver Installation and other instructions located on the On-line Manuals page.

Additional Resources:

INLINE 7 Download (Part Number 5299899)
File Name: INLINE7_2300_Setup.zip (Size: 10.9 MB)
DOWNLOAD

Additional Resources:

This software is not available on mobile. To download for your office or home computer, please return to this page from that device.

Issues and Solutions

Please use a shorter USB cable to see if this resolves your issue.

Questions and Answers

INLINE Warranty Repair Process and Information
Snap-on / Nexiq is a Cummins Inc. authorized repair center for the INLINE 7 and the INLINE mini. The information below will describe things to expect when using this process.
 
INLINE 7
Warranty Period: 1 year from Purchase Date
Cost for Warranty Repair: $310.00 hold will be placed on credit card till the device is received by Snap-On / Nexiq and warranty status can be confirmed. If device sent is under warranty then the money being held will be released and no charge will occur.
Cost for Non-Warranty Repair: If the Device is not under warranty the price to get this repaired will cost $310.00
Repair Turn-around Time: 2-3 Business Days (Plus Return shipping time) from date of receiving the adapter. 
 
INLINE 7 mini
Warranty Period: 1 year from Purchase Date
Cost for Warranty Repair: $0.00
Cost for Non-Warranty Repair: Device is not repaired after the warranty expires. Purchasing a new adapter is cheaper than paying for repair of this device.
Repair Turn-around Time: 2-3 Business Days (Plus Return shipping time) from date of receiving the adapter. 
 
To start the repair process go to https://service.nexiq.com/Login.aspx and register with the Snap-On / Nexiq repair website. 

Before requesting support, please experiment a bit to reproduce and isolate the problem. When you do contact support, please be ready to provide the following information:

  • The model and firmware version of the INLINE adapter you have
  • The version of the Windows operating system you are using on your PC
  • The actual error message or state that you are experiencing
  • The steps you take to reproduce the problem
  • The version of INSITE or other application software you are using

 
To find Windows operating system version information:

  • Click the Start menu in the Windows system tray on the bottom left side of your computer screen in the Taskbar.
  • Click Control Panel (in Settings in older Windows versions).
  • Double-Click System.

 
To find the software application version:

  • Click the Help menu.  
  • Select the About option.

The INLINE 6 and INLINE 5 PC drivers support Windows™ 7, Vista, and XP.

This indicates that the adapter is probably not receiving power. Verify that the data link cable is securely connected to both the adapter and the data link connector and that there are no bent pins in the connectors.

This indicates that the adapter's power voltage is out of its normal operating range. Make sure that the power source voltage is connected and in the normal 8 V to 50 V range.

Contact Cummins Care

For general inquiries or questions regarding your Cummins product, please use the form below, or call us anytime.

Reach Us By Phone

USA: 1-800-CUMMINS™ (1-800-286-6467)
USA: 1-800-CUMMINS™ (1-800-286-6467)
Albania: +44 (0) 1327 886464
Andorra: +44 (0) 1327 886464
Argentina: 0800 12 26 467
Armenia: +44 (0) 1327 886464
Australia: 1-300-CUMMINS (1 300 2866467)
Austria: +44 (0) 1327 886464
Azerbaijan: +44 (0) 1327 886464
Belarus: +44 (0) 1327 886464
Belgium: +44 (0) 1327 886464
Bolivia: 800 10 18 73
Bosnia and Herzegovina: +44 (0) 1327 886464
Brazil: 0-800-CUMMINS (0 800 2866467)
Bulgaria: +44 (0) 1327 886464
Canada: 1-800-CUMMINS™ (1-800-286-6467)
China: (+86) 400 810 5252
Colombia: 01 800 75 22 501
Costa Rica: 41003-1600, option 6
Croatia: +44 (0) 1327 886464
Czech Republic: +44 (0) 1327 886464
Denmark: +44 (0) 1327 886464
El Salvador: 2555-4000, option 6
Estonia: +44 (0) 1327 886464
Finland: +44 (0) 1327 886464
France: 00-8000-CUMMINS (00 8000 286 6467)
Georgia: +44 (0) 1327 886464
Germany: 00-8000-CUMMINS (00 8000 286 6467)
Greece: +44 (0) 1327 886464
Honduras: 2202–5600, option 6
Hungary: +44 (0) 1327 886464
Iceland: +8000-CUMMINS (+8000 286 6467)
India: 1 800 210 2525
Ireland: 00-8000-CUMMINS (00 8000 286 6467)
Italy: +44 (0) 1327 886464
Kazakhstan: +44 (0) 1327 886464
Latvia: +44 (0) 1327 886464
Liechtenstein: +44 (0) 1327 886464
Lithuania: +44 (0) 1327 886464
Luxembourg: +44 (0) 1327 886464
Macedonia: +44 (0) 1327 886464
Malta: +44 (0) 1327 886464
Mexico: 01-800-CUMMINS (01 800 286 6467)
Moldova: +44 (0) 1327 886464
Monaco: +44 (0) 1327 886464
Montenegro: +44 (0) 1327 886464
Netherlands: 00-8000-CUMMINS (00 8000 286 6467)
New Zealand: 0-800-CUMMINS (0 800 286 6467)
Norway: +8000-CUMMINS (+8000 286 6467)
Panama: 377–9000, option 6
Paraguay: 009 800 521 0101
Poland: +44 (0) 1327 886464
Portugal: +44 (0) 1327 886464
Romania: +44 (0) 1327 886464
Russia: +44 (0) 1327 886464
San Marino: +44 (0) 1327 886464
Serbia: +44 (0) 1327 886464
Slovakia: +44 (0) 1327 886464
Slovenia: +44 (0) 1327 886464
Spain: +44 (0) 1327 886464
Sweden: +8000-CUMMINS (+8000 286 6467)
Switzerland: +44 (0) 1327 886464
Turkey: +44 (0) 1327 886464
United Kingdom: 00-8000-CUMMINS (00 8000 286 6467)
Uruguay: 00 04 05 29 66 23
Vatican City: +44 (0) 1327 886464
If your country is not listed, please contact us using the “Send Us Your Request” form.
Cummins Care representative

Send Us Your Request

A Cummins Care team member will respond to your request within 48 hours.

I am a
I am a *
Need help finding a Cummins Certified Service Provider or Parts Support? Click here
Redirecting to
cummins.com

The information you are looking for is on
cummins.com

We are launching that site for you now.

Thank you.