Cummins Stage V B6.7 and L9 Certified and in Production

Paris, France

Cummins announced that is latest B6.7 and L9 Stage V engines are now fully certified and in production at its Darlington UK plant. 

“These engines do more with less, offering higher power output and torque for improved machine capability in a smaller, lighter package that is cheaper to run. Simpler architecture with fewer parts means they are more reliable, and more productive,” said Eric Neal, Executive Director, Cummins Off-Highway business.

Top-rated power for the Stage V B6.7 moves up to 243 kW (326 hp) with a peak torque of 1375 Nm – a 30 percent increase over that of Stage IV. The L9 top rating increases from 298 kW (400 hp) up to 321 kW (430 hp) at Stage V, together with a 13 percent increase in peak torque to 1846 Nm.  The higher capability of these engines is delivering down-sizing opportunities for our equipment manufacturers.  The increase in power and torque means that they are replacing engines of higher displacement with no impact on equipment operation, and providing installation cost savings for OEMs. 

“Cummins capability to tailor engine power and torque curves to the specific operational needs of key installations such as wheeled loaders, excavators and material handling equipment using our in-house technologies, like turbocharging and exhaust aftertreatment, is also enabling OEMs to be more competitive,” added Neal.  
Cummins engineers have completed over 100 Stage V customer installations to date, with more planned.  30% of these installations are for new equipment with current and new customers.   These include air compressors, back-hoe loaders, dump trucks, fork lift trucks, container handlers, drills, pavers, cranes, excavators, wheeled loaders and snow groomers. 

 

L9 Stage V Engine

Note to editor: A version of this press release was issued at Pre-Intermat.

 

About Cummins Inc.

Cummins Inc., a global power leader, is a corporation of complementary business segments that design, manufacture, distribute and service a broad portfolio of power solutions. The company’s products range from diesel and natural gas engines to hybrid and electric platforms, as well as related technologies, including battery systems, fuel systems, controls, air handling, filtration, emission solutions and electrical power generation systems. Headquartered in Columbus, Indiana (U.S.A.), since its founding in 1919, Cummins currently employs approximately 58,600 people committed to powering a more prosperous world. Cummins serves customers in about 190 countries and territories through a network of some 500 company-owned and independent distributor locations and approximately 7,500 dealer locations. Cummins earned $1 billion on sales of $20.4 billion in 2017. Press releases can be found on the Web at www.cummins.com. Follow Cummins on Twitter at www.twitter.com/cummins and on YouTube at www.youtube.com/cumminsinc

Cummins Information

 

 

Media Contact
Redirecting to
cummins.com

The information you are looking for is on
cummins.com

We are launching that site for you now.

Thank you.