About Us Products Investors And Media Corporate Responsibility Careers Customer Assistance Distributor Network
USA & Canada  
Change Region    
CumminsHeader
Sustainability  |   Power Store  |   Service Locator  |   Product Registration  |   Suppliers  |   Online Parts and Service   
Home   >   Sustainability   >   Environment   >   Living Our Values   >   SuperTruck Update
SuperTruck yields exciting fuel mileage numbers during testing
SuperTruck yields exciting fuel mileage numbers during testing Print Print Share Share

March 27, 2013


Cummins and Peterbilt Motors Company announced impressive fuel mileage gains in their concept SuperTruck which is testing a number of possible future innovations.

Cummins and Peterbilt Motors Company say a demonstration tractor-trailer they partnered on achieved a 54 percent increase in fuel economy during testing in the fall of 2012, averaging nearly 10 miles per gallon (mpg) under real world driving conditions.

The “SuperTruck” developed by the two companies features a higher-efficiency engine and an aerodynamic tractor-trailer that significantly reduces drag. The truck also includes a system that converts exhaust heat into power delivered to the crankshaft, electronic controls that use route information to optimize fuel use, tires with lower rolling resistence and lighter-weight material throughout.

The Class 8 Peterbilt 587 powered by a Cummins ISX15 engine averaged 9.9 mpg during testing on U.S. Route 287 between Fort Worth and Vernon, Texas. The testing was conducted over 11 runs meeting SAE International test standards along a 312-mile route.  The tractor-trailer had a combined gross weight of 65,000 lbs.

Today’s long-haul trucks typically achieve between 5.5 and 6.5 mpg. The 54 percent increase in fuel economy would save about $25,000 annually based on today’s diesel fuel prices for a long-haul truck  traveling 120,000 miles per year. It would also translate into a 35 percent reduction in annual greenhouse gases per truck.

The potential savings in fuel and greenhouse gases are enormous, with about 2 million registered tractor-trailers on U.S. roads today, according to The American Trucking Association.

In addition to the fuel economy improvements, the truck also demonstrated a 61 percent improvement in freight efficiency during testing compared to a baseline truck driving the same route. That significantly exceeded the 50 percent SuperTruck program goal set by the U.S. Department of Energy. Freight efficiency is an important metric in the transportation industry that is based on payload weight and fuel efficiency expressed in ton-miles per gallon.

“Many of the technologies we are testing on the engine and truck will be integral parts of the trucks of tomorrow,” said David Koeberlein, Principal Investigator for the SuperTruck program at Cummins. “We are focused on developing innovations that meet and exceed the needs of our customers, while helping to create a cleaner, healthier and safer environment.”

Cummins personnel have been focused on the engine and its integration with the powertrain. They have been working with several other companies and research institutions to develop numerous changes in the combustion system as well as advances to reduce internal friction and so-called “parasitic power” – excess power the engine needs to run such things as lube and coolant pumps and air compressors.

In addition to the truck’s exterior, Peterbilt, a division of PACCAR, and its partners have been working on improvements in the drivetrain, the idle management system, weight reduction and vehicle climate control. Eaton's advanced transmission facilitates further engine downspeeding for additional fuel economy benefits.

“Aerodynamics has been a significant contributor to the efficiency gains,” said Scott Newhouse, Senior Assistant Chief Engineer of Product Development at Peterbilt, . “We are very pleased with what our team has been able to accomplish using a comprehensive tractor-trailer approach.”

Cummins is a prime contractor leading one of four teams under the Department of Energy’s SuperTruck project. SuperTruck is one of several initiatives under the 21st Century Truck Partnership, which is a public-private partnership founded to further stimulate innovation in the trucking industry.

Cummins, Peterbilt and their program partners will have invested $38.8 million in private funds over the four-year life of their SuperTruck program, which started in 2010, with critical support coming through awarded matching grants from the Department of Energy’s Vehicle Technologies Program.

Testing will continue in 2013 on a new Peterbilt 579 that Cummins and Peterbilt are confident will take what has been achieved so far to even higher levels. The testing will address use of the tractor-trailer over a 24-hour period; including periods when drivers are at rest but still need power for such things as air conditioning and small appliances.